Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is it safe to power a raspberry pi from battery's?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 715 subscribers
  • Views 5385 views
  • Users 0 members are here
  • raspberry
  • pi
  • raspberry_pi
Related

Is it safe to power a raspberry pi from battery's?

e14 Contributor
e14 Contributor over 10 years ago

I want to make my raspberry pi portable, is  it safe to run it from battery's?

  • Sign in to reply
  • Cancel
Parents
  • tonyboubady
    tonyboubady over 10 years ago

    Consider power as water, current as speed of flowing water and battery as a container...

     

    What we really need to power anything is amount of the water(voltage) and throttle of the water(current)...

     

    If the water container(battery) is not providing enough amount of water(voltage), add more containers(batteries) in series...

     

    If the container(battery) is not providing enough throttle of water(current), add more containers(batteries) in parallel...

     

    So, yes we can power anything with this logic image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to tonyboubady

    Have raspberry pi 3 w/7inch monitor. Need more voltage. Raspberry pi 3 needs exactly 5 volts or it will throttle. That's why PSU with starter kit is 5.25 volts. I tried my 15.000 m Amp hour battery. It doesn't

    drain fast, but it does not supply enough voltage for Pi3 not to throttle.

     

    Can pi 3 over volt. How far is safe if it can.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Eric Kazer

    I believe the problem is the current not the voltage. 15,000 mAh is a measure of current over time. I bet it delivers only 1.0 Amp. A Pi 3 needs more especially with a 7 inch display! If you have two usb connections, each is 1.0 Amp. Then drive one for the Pi 3 and separately drive the 7 inch display.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Battery pack has 2 1 amp outs, and 1 2.1 amp out. The pi3 is in the 2.1 amp out on the battery pack. When I was running pi2 it was ok. I should try putting the monitor and the audio amplifiers on their own 1 amp usb power outputs. The battery it's self might not be enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Battery pack has 2 1 amp outs, and 1 2.1 amp out. The pi3 is in the 2.1 amp out on the battery pack. When I was running pi2 it was ok. I should try putting the monitor and the audio amplifiers on their own 1 amp usb power outputs. The battery it's self might not be enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank You.

     

    It was amperage. I connected the Raspberry Pi3 to the 2.1 amp USB by its self & the monitor to one of the 1 amp USB, then the 2 amplifiers to the last 1 amp USB. The volt drop stopped. No more colored box. No more CPU speed drop which was awful. I'm surprised at how critical .1 volt drop is to pi 3. That's all it was dropping. Now I can run games like Street Fighter movie, Metal Slug 4, Metal Slug X,3, etc..

     

    Thanks again,

    Eric