Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What Will You Do With Your New Raspberry Pi 3?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 65 replies
  • Subscribers 718 subscribers
  • Views 5974 views
  • Users 0 members are here
  • projects
  • pi3
  • raspberry_pi_space
  • raspberry pi 3
Related

What Will You Do With Your New Raspberry Pi 3?

spannerspencer
spannerspencer over 10 years ago
imageNEW! Raspberry Pi 3 Model B
Frequently Asked QuestionsComparison ChartTechnical Specifications
40 Pin OutPi3 Video Arcade ProjectRaspberry Pi 3 RoadTest

So, now that the Raspberry Pi 3 is live and among us, the most obvious question is what are you going to do with it?image


Got any cool project ideas that tie in neatly with its new connectivity functions? Or maybe all those extra horses beneath its silicon hood are what you need?

 

Tell us all about your plans for the Raspberry Pi 3!

 

And if you're looking for inspiration...

PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table

  • Sign in to reply
  • Cancel
Parents
  • mconners
    mconners over 10 years ago

    I've got a bluetooth ODBII adapter for my truck. I've been toying with the idea of hooking up a small device to get real time readings and displaying them in my overhead console. The built in BT may come in handy for that.

     

    Mike

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mconners

    Nifty idea. If you want, the information is available for the protocol of the messages from Society of Automotive Engineers (SAE), and the document is J1978 or J1979 (old brain cells) one is the messages, the other is the scan tool, and I forget which one is which (I was on the committees back in the early 90s when they were being developed, fun times).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mconners

    Nifty idea. If you want, the information is available for the protocol of the messages from Society of Automotive Engineers (SAE), and the document is J1978 or J1979 (old brain cells) one is the messages, the other is the scan tool, and I forget which one is which (I was on the committees back in the early 90s when they were being developed, fun times).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mconners
    mconners over 10 years ago in reply to jack.chaney56

    I was actually serious about it enough once to download all those docs and look into it. I was gonna use an arduino, but this might be a better option.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mconners

    You should be able to get enough information to make a kind of performance recorder as well. All sorts of engine information is available like Air/Fuel levels, O2 and knock sensor, as well as engine speed and general sensor readings.  The information is not real-real time (can't use it to run the motor), but the data would be current with all the status (including any error conditions or emissions data).

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 10 years ago in reply to jack.chaney56

    I've got an android app that monitors all that stuff (Torque Lite) , so I've got a good idea what is available.

     

    Thanks for the suggestions,

     

    Mike