Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What Will You Do With Your New Raspberry Pi 3?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 65 replies
  • Subscribers 718 subscribers
  • Views 6085 views
  • Users 0 members are here
  • projects
  • pi3
  • raspberry_pi_space
  • raspberry pi 3
Related

What Will You Do With Your New Raspberry Pi 3?

spannerspencer
spannerspencer over 10 years ago
imageNEW! Raspberry Pi 3 Model B
Frequently Asked QuestionsComparison ChartTechnical Specifications
40 Pin OutPi3 Video Arcade ProjectRaspberry Pi 3 RoadTest

So, now that the Raspberry Pi 3 is live and among us, the most obvious question is what are you going to do with it?image


Got any cool project ideas that tie in neatly with its new connectivity functions? Or maybe all those extra horses beneath its silicon hood are what you need?

 

Tell us all about your plans for the Raspberry Pi 3!

 

And if you're looking for inspiration...

PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table

  • Sign in to reply
  • Cancel
  • artful_bodger
    artful_bodger over 10 years ago

    I'm going to do something that a lot will consider mainstream.  A full blown media player.  I never managed to get really good, smooth video streaming off the original Pi.  I'm going to take the opportunity to build it into a 5 channel audio amp I have and make a media centre, with multiple input and output sources. If there is enough grunt, it'll also be a mini-NAS. The bluetooth will be really handy for a dedicated remote control modified from infra-red.

    The power consumption & speed figures posted by Christopher Stanton https://www.element14.com/community/community/raspberry-pi/blog/2016/02/29/the-most-comprehensive-raspberry-pi-comparison-benchmark-ever are very encouraging.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ipv1
    ipv1 over 10 years ago

    The RPI 2 was good but it lacked BLE and I am hoping to add the TI BLE lights in direct connection to the RPI in my Home automation system. The extra horsepower will be useful when using Open to take in Visual stimulus. Consider this...

    Use OpenCV to track a particular object and use TI BLE LEDs to generate colors correspondingly.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago

    I'm looking forward to getting familiar with the WiFi/BLE capabilities to better support the flood of support queries that are sure to follow. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago

    First comment... I have now sworn off PCs for home use.  I have been using Pi B, B+ and B2, and just ordered my B3.  If the upgrade is as good as predicted, I am kissing PCs good bye.  image

    Second, for work, I am going to start porting our monitor application to propose a low cost solution for emerging countries. The GPIO and touch screen should handle all the communication needed, and make it a credible solution.

     

    Thank you for the new toy,

    Jack

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to gadget.iom

    This sounds like the best platform yet to build a car stereo out of. with the bluetooth built in, pairing a cell phone should be easier.  Thats where I would like to take my raspberry pi 3 project. Developing an inexpensive car stereo probably running KODI

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 10 years ago

    I've got a bluetooth ODBII adapter for my truck. I've been toying with the idea of hooking up a small device to get real time readings and displaying them in my overhead console. The built in BT may come in handy for that.

     

    Mike

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mconners

    Nifty idea. If you want, the information is available for the protocol of the messages from Society of Automotive Engineers (SAE), and the document is J1978 or J1979 (old brain cells) one is the messages, the other is the scan tool, and I forget which one is which (I was on the committees back in the early 90s when they were being developed, fun times).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 10 years ago in reply to jack.chaney56

    I was actually serious about it enough once to download all those docs and look into it. I was gonna use an arduino, but this might be a better option.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • CrazyFace
    CrazyFace over 10 years ago

    I haven't even taken it out of the box yet let alone got over the fact I was lucky enough to win one on release day.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mconners

    You should be able to get enough information to make a kind of performance recorder as well. All sorts of engine information is available like Air/Fuel levels, O2 and knock sensor, as well as engine speed and general sensor readings.  The information is not real-real time (can't use it to run the motor), but the data would be current with all the status (including any error conditions or emissions data).

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>