Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Model B Cases?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 180 replies
  • Subscribers 727 subscribers
  • Views 20190 views
  • Users 0 members are here
  • raspberry
  • help
  • pi
  • b
  • raspberry_pi
  • 3d_printing
  • model
  • case
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Raspberry Pi Model B Cases?

Wwessex
Wwessex over 14 years ago

Hi,

I was wondering if anyone knows of a case for the Model B?

  • Cancel
  • Catwell
    Catwell over 14 years ago

    William,

     

    I am not sure of an official case or not, but I plan on making enclosures myself.

     

    What would you like to see in a case?

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Catwell

    The forum at the maker's site is currently out of service due to high volume, but I remember there being talk about a case being at least in the design stage. They are also working on expensions, so who knows what's really in store?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Wwessex
    Wwessex over 14 years ago in reply to Catwell

    I would like the case to include both a top and bottom (sometimes cases don't include a bottom to save money), holes for all the ports and SD card slot.

    Also it should have ventilation and the Raspberry Pi logo on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • fustini
    fustini over 14 years ago

    That's a good question also I think a great business opportunity for those with laser cutters or 3d printers like hackerspaces.  I would definately pay some money for a nice case/enclosure.

     

    Looks like there's already a few designs on Thingiverse:

     

    http://www.thingiverse.com/search?q=raspberry&sa=Search

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to fustini

    Drew,

     

    Thanks for the link. I can use board model there to design a case.

     

    So far, the ones I have seen are not exactly blowing my hair back.

    I plan on designing something smaller and more rugged. Too back the board does not have any mounting holes. Just one would have helped.

     

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Take a look at the Raspberry Pi orgs forum when it comes back up. There is a long thread about user designed cases, even one that is made from Lego bricks complete with a bill of materials.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    I have put a RepRap design on thingiverse : http://www.thingiverse.com/thing:16104

     

    Also put a version  on shapeways.   http://www.shapeways.com/shops/picase

    I have 4 versions there.

    With 1mm walls - open bottom and closed bottom

    With 1.4mm walls - open bottom and closed bottom

    I would advise the 1.4mm walls version, because it is much much stronger. Bad side it is a bit more expensive because it uses more material

     

    There is a big difference between a RepRap version and the one on shapeways.

    For RepRap printing everything needs to be supported, so there is a strange case split needed to get this working.

    The 2 case halfs stick together by friction....

     

    Downside of Shapeway is the price... but it is very very well made, very fine detail and the 2 halfs click together.

    This weekend I will put up a version with an open top and possible an open bottom with 1.4mm walls, but with room to put a transparent perspex sheet (5x8 cm) instead. So that will save a lot of material costs.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Case will be supplied when it ships. It will apparently be transparent. I like the idea of this.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I would like to see a few case options:

     

    1) Simple case to put thing in and expose sockets

     

    2) A bigger case that could hold a 2.5 drive that could be connected via usb.

     

    3) a PC type case so you can add CD rom, 2.5 Drive, have additional USB sockets, power switch, etc. Think Blu-ray player sized.

     

    4) What about a case thats a keyboard? That the thing can slide into and make into the good old 80's type home computer. With all the connection on the back and usb ports etc..

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hmm,

     

    Methinks that I will be modding a mini pelican personnaly.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
>