Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Model B Cases?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 180 replies
  • Subscribers 727 subscribers
  • Views 20234 views
  • Users 0 members are here
  • raspberry
  • help
  • pi
  • b
  • raspberry_pi
  • 3d_printing
  • model
  • case
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Raspberry Pi Model B Cases?

Wwessex
Wwessex over 14 years ago

Hi,

I was wondering if anyone knows of a case for the Model B?

  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    We have seen a vast amount of interest in cases for the RPi.

     

    As the foundation we focused on the PCB rather than the case as that is very much first base. Many of our developers can manage without but now it needs to be done.  I have to agree that having the  RPi floating around on the desk is not cool and no good for our schools projects - although someone pointed out that using a P clip on the HDMI cable held a Pi in place quite well !

     

    Material - any 'Official' case is likely to be plastic - we can cope with the tooling costs (to a point) but not the reaction to a $20+ case for a RPi.  I hear that some guys are planning a $20 + gamer case made out of metal but I don't have link for that at the moment.

     

    Mounting Holes - OK I hold my hands up - (sorry folks) should have dealt with that better - just really under pressure to get the design out - ho hum.  Don't forget that a 2.5mm screw with clearance will cost about 7mm in diameter on the PCB itself - crushing and shorting inner layers of PCBs under screws has always been a debugging nightmare so they need to be moated out and tracks removed / routed round. So finding space on the board for these would be challenging.

     

    I had always envisaged that the board could clip into a plastic base - cheap and quick.

     

    My real embarrassment is that fact that the Ethernet and USB ports don't line up.  It makes life to say the least 'interesting' for a case designer. We have a couple of options on a board spin but Eben may just keep buying me beers until I agree to move the USB back 6mm or so which means the SMSC needs to move!

     

    I'll keep you in the all in the loop as casework progresses - comments and suggestions always appreciated.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    We have seen a vast amount of interest in cases for the RPi.

     

    As the foundation we focused on the PCB rather than the case as that is very much first base. Many of our developers can manage without but now it needs to be done.  I have to agree that having the  RPi floating around on the desk is not cool and no good for our schools projects - although someone pointed out that using a P clip on the HDMI cable held a Pi in place quite well !

     

    Material - any 'Official' case is likely to be plastic - we can cope with the tooling costs (to a point) but not the reaction to a $20+ case for a RPi.  I hear that some guys are planning a $20 + gamer case made out of metal but I don't have link for that at the moment.

     

    Mounting Holes - OK I hold my hands up - (sorry folks) should have dealt with that better - just really under pressure to get the design out - ho hum.  Don't forget that a 2.5mm screw with clearance will cost about 7mm in diameter on the PCB itself - crushing and shorting inner layers of PCBs under screws has always been a debugging nightmare so they need to be moated out and tracks removed / routed round. So finding space on the board for these would be challenging.

     

    I had always envisaged that the board could clip into a plastic base - cheap and quick.

     

    My real embarrassment is that fact that the Ethernet and USB ports don't line up.  It makes life to say the least 'interesting' for a case designer. We have a couple of options on a board spin but Eben may just keep buying me beers until I agree to move the USB back 6mm or so which means the SMSC needs to move!

     

    I'll keep you in the all in the loop as casework progresses - comments and suggestions always appreciated.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • GreenYamo
    GreenYamo over 14 years ago in reply to e14 Contributor

    Pete, thanks for such an interesting reply.

     

    I am a bit of a case freak and always want cases for my tech, from the Pi (on order) to mobile, camera etc so I'm watching this eagerly.

     

    I think until the dust settles on the cases, I'm going to get this from from eBay :-)

     

    http://www.ebay.co.uk/itm/Genuine-Raspberry-pi-all-models-B-DIY-Casing-/300673071877?pt=LH_DefaultDomain_3&hash=item460182fb05

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Brilliant device. If persons have nothing better to complain about than the position of ports, and a lack of mounting holes then you've out-performed more or less every other device ever released to consumers! Nothing more needs to be said.