• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Model B Cases?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 180 replies
  • Subscribers 727 subscribers
  • Views 20371 views
  • Users 0 members are here
  • raspberry
  • help
  • pi
  • b
  • raspberry_pi
  • 3d_printing
  • model
  • case
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Raspberry Pi Model B Cases?

Wwessex
Wwessex over 14 years ago

Hi,

I was wondering if anyone knows of a case for the Model B?

  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I was wondering if the Pi can be used with it simply standing on the anti-static bag in which it was packed .

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Montala
    Montala over 14 years ago in reply to e14 Contributor

    This is not really advisable, as the outside of an anti-static bag is NOT actually anti-static!

    You would actually be better off placing it on a piece of cardboard, or buying one of these fairly cheap so called 'cases' which are basically two pieces of 'perspex' held apart with some spacing screws.

    There is probably a bit more to it than that, but you get the idea!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Montala

    Thanks for the information.  Then if the anti-static bag was turned inside out and used to cover the cardboard on which the Raspberry Pi is placed, this would give it protection from ESD.  Is that a good or acceptable result?

    It would be most appreciated and helpful if you would kindly advise further regarding protection from ESD with the acrylic or plastic commercially available cases.

     

    Thanks for your most kind help.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Montala

    Thanks for the information.  Then if the anti-static bag was turned inside out and used to cover the cardboard on which the Raspberry Pi is placed, this would give it protection from ESD.  Is that a good or acceptable result?

    It would be most appreciated and helpful if you would kindly advise further regarding protection from ESD with the acrylic or plastic commercially available cases.

     

    Thanks for your most kind help.