Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Doing more with less: Raspberry Pi & Software Engineering
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 709 subscribers
  • Views 2928 views
  • Users 0 members are here
  • raspberry
  • pi
  • raspberry_pi
  • raspberrypi
Related

Doing more with less: Raspberry Pi & Software Engineering

morgaine
morgaine over 14 years ago

Minimalism is a concept which hardware engineers embrace almost instinctively, but sadly in the world of software it's rarely even present in the vocabulary.

 

The emphasis in practical computing today is to ride upon the shoulders of giants by reusing the work of others, which is a terrific idea in principle but can be a disaster when applied without checks and balances.  It almost always results in cancerous growth of colossal monolithic applications, which is why so many software systems today are bloated beyond belief and become ever more flaky in proportion to their size, not to mention suffering from dependency hell.

 

We used to call this nightmare "The Software Crisis", the reason why "software bridges" collapse millions of times a day across the world, in contrast to the products of other branches of engineering where reliability is required, expected and achieved as a matter of course every day, not as the exception.  The Software Crisis is rarely mentioned anymore, because we have lost the war, surrendered to complexity, and have no solution in sight.  Software bridges continue to fall, ever faster.

 

How does this relate to Raspberry Pi?  Not very strongly, except in the sense that in software, "smaller is better".  256MB is such a huge amount of memory that if any significant part of it is used to hold the program code of a monolithic application then that application is in crisis, whether it's admitted or not.

 

There isn't really any solution to this problem available at the present time.  It would require a breakthrough in computing science to come up with a way of doing more with less, and then to force it upon a world which doesn't even realize that its pride and joy is actually an engineering disaster.  That's not going to happen any time soon.

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    Excellent post, Morgaine.  The only part I disagree with is your assertion that there isn't a solution at this time.  Sure, it's a hard sell since so many people believe that "more features" means better, and "more apps" means better, and "more complex" means better.  But I do read articles occasionally about "good enough computing" and how most people can easily get by with RasPi-like machine capabilities.

     

    I like to make an analogy with the RISC versus CISC argument of the 1980s.  (One of my favorite article titles of the time is from Electronics (5 May 1986): “RISC: Is it a Good Idea, or just another Hype?”)  In the 1980s transistors became so cheap you could afford to design computers with every instruction you always wanted.  However, those instructions were useless if the compiler couldn't take advantage of them, and their presence slowed down the performance of the instructions you really needed.

     

    I say software is similar: useless features clog the software with complexity, making the features you really need harder to use and learn.  I have a longer essay on the subject at http://code.google.com/p/xxicc/wiki/RSCwiki if you're interested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    I liked your linked article a lot, John.  I can't find fault with any of it, and since I started my Unix days on a PDP-11/34, I both agree with your premises and also found your writeup very nostalgic.

     

    With regard to solutions for the Software Crisis, I guess it comes down to where one draws the finish line.  You've pointed out some directions that help reduce the speed of headlong rush towards the precipice, and I agree with them, but in the end the velocity vector is still towards it, just a little less quickly.

     

    And sadly there is no existing solution that could sway the current high priests of the software fraternity, who totally believe that they are on the true path of enlightment already.  To make matters even worse, there is no shortage of programmers who do what they do because it's fun and COOL, rather than for engineering reasons.  You can't argue against COOL, engineering disaster be damned.  It's one of the biggest problems of computing today --- programming is fun and creative, and as a result, serious engineering is almost entirely ignored.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine - your a mind reader (was travelling today and following the conversation and thought the same thing) - interesting discussion - but as you say we have gone a bit off topic and therefore a shame its buried in something that is titled differently.

     

    I would like to suggest that we try to keep this thread to things that people have found wrong with the Pi rather that the philosophy of programming. What the Pi could have been, rather than what actually would also be better in another thread but these work so well together I would leave them together if that is OK?  So I would cut earlier and title something like "Lack of Memory on the Pi?" and it would hopefully encourage people to read and comment.

     

    Never annoyed - it's a community thread - it is Drew's and the Admin's job to keep us in some sort of order.  image

     

    Off to eat some humble Raspberry Pi whilst I fix up the daft mistakes on the schematics, good job they are not on the board - V1.1 soon.

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustiniadmin
    fustiniadmin over 14 years ago in reply to morgaine

    I went ahead and branched after seeing what Pete wrote, too.  I've manually set the language setting again to English to avoid that visibility problem which happened last time I branched a thread.  But the issue with the subject of individual replies not changing hasn't been fixed yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    @Pete: Haha, don't kick yourself, things of this complexity are improved iteratively, they're not born magically perfect.  Well at least mine aren't.  image

     

    @Drew: Many thanks for doing the deed.  Of course, now that it's split, the discussion is guaranteed to dry up. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine,

       Why aren't your complex products born magically perfect?

     

    In message 12 of thread:

    http://www.raspberrypi.org/forum/features-and-requests/interfaces-case-package-requestsuggestion

     

    Liz wrote:

     

    "I can absolutely assure you that we won't be shipping a product that still requires beta testing! What you'll see at the end of the year will be the finished, polished product. The reasons we"re having a hobbyist release first are basically dull old business reasons – we need some income to get the larger release of boards made, which we mean to raise by selling the first batch to…you lot, because we know the demand is there!"

     

    If the RPi can do it, you should be able too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine,

     

    You wrote:

    "If the space shuttle had been built as a monolithic unit, it would never have got off the ground because of complexity meltdown."

     

    Interestingly, the shuttle's solid rocket boosters perhaps should have been built as a monolithic unit, but instead were built in segments to facilitate transport.  But the poorly-designed segment joints caused the Challenger tragedy. Sometimes, the overhead involved in splitting up a monolithic design is not repaid in improved reliability.

     

    you wrote:

    "hardware "units" continue to be independent even when put together into a whole, they don't lose their independence and observability when they are linked together."

     

    I think you are referring to something like hardware chips on a pcb board not losing their independence.  But in other cases, like a SoC, the hardware components do essentially lose their independence, much like software components.

     

    While it is generally true both in hardware and software that cost and complexity grows exponentially with the size of a project,  this is largely due to increased interconnections between the parts.  It isn't necessarily true when simply aggregating together components that have well-defined interfaces, as is done with a SoC. 

     

    It used to be that Fortran programs had all their global variables declared in common statements, and complexity therefore grew exponentially with size.  But modern software can be designed in layers and modules with restricted visibility to other layers and modules, so complexity grows more linearly with size.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I've learned to ignore most of what comes from that particular source.  It's mostly highly decorative and self-congratulatory PR, regularly spinning the truth and faithful to the teachings of mushroom management.  But the straw that broke the camel's back for me was incitement of the fanbois against participants who ask inconvenient questions or voice any criticism.  What little credibility remained was destroyed utterly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    @coder27: It's partly true what you say about the components within SoCs losing their independence as hardware units.  This is what happens when hardware is "programmed" into shape rather than assembled from actual physically independent devices.

     

    However, it's not nearly as bad as what happens in software systems assembled out of classes and functions, because the  units in hardware are always static components with narrow interfaces, whereas software units are generally dynamic (even recursive) and very commonly have disastrously wide interfaces.  That results in a combinatorial explosion of complexity.

     

    Curiously, software should be easier to nail down tightly and monitor to any desired degree of granularity than hardware, because software is not bound by debug limitations such as pinout counts and limited cell numbers that restrict the ability of deeply embedded components in SoCs to be monitored effectively.  What's curious is that the relative ease of doing this monitoring in software does not lead to it actually being done, at least not as a matter of course.  Right across the industry, software validation is extraordinarily minimal.  As a freelance contractor I've seen the insides of a lot of companies, and this problem is universal.

     

    It truly is a crisis, and the fact that people consider it NORMAL nowadays that software will fail shows just how deep a crisis it has become.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    As Morgaine points out, hardware generally has well-defined interfaces.  Provided that power and clocks are reliable, timing requirements are met, and signals are sound the modules only interact through their interfaces.  In hardware there are no global variables or pointers to create unexpected interactions between modules you thought were independent.

     

    Also, hardware modules tend to have simpler functionality because you want to move complex behavior to software whenever possible because it's cheaper and more flexible to implement there.

     

    Software modules should also have well-defined interfaces, and well-designed modules do.  For example, the OSI model for data commucations works extremely well, allowing you to have TCP/IP communication over whatever underlying link and physical layers are available.

     

    But a well-defined software interface only goes so far.  The biggest problem I have in software design is that there are so many different combinations of data that it's impossible to test more than a few of them.  For example, a document editor may have a data structure which retains the information needed to implement UNDO operations and perhaps change management, given both text and formatting changes.  It's really hard to get these right with efficient code and data structures.  Occasionally you get a sequence of insert, delete, and reformat operations that exposes a bug in the program.  Often it's really hard to reproduce that sequence and the bug remains until a someone is able to reproduce it on demand and is generous enough to report how to do it.

     

    Once you have a reproducible bug it's usually straightforward to track it down.  "A reproducible bug is half fixed."  But until you have a way to reproduce it it's a mystery, and occasionally you get a "Heisenbug" which goes away when you try to instrument it.

     

    I like this quote from CAR Hoare: "There are two ways of constructing a software design: One way is to make it so simple that there are obviously no deficiencies, and the other way is to make it so complicated that there are no obvious deficiencies.  The first method is far more difficult."  The modern approach of slapping together modules without really designing anything is easy in the short run, but creates a maintenance time bomb.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    +1 John, very nicely put.

     

    And Tony Hoare is one of my heroes, he used to come around to our research group and wax lyrical about CSP and how we would soon be painting our walls with 2D arrays of transputers.  He was so ahead of his time, and so very right about the only sane way to scale up computational machinery.

     

    Morgaine.

     

    /sigh ... forgot to reply to original post

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to e14 Contributor

    coder27 wrote:

    Interestingly, the shuttle's solid rocket boosters perhaps should have been built as a monolithic unit, but instead were built in segments to facilitate transport.  But the poorly-designed segment joints caused the Challenger tragedy. Sometimes, the overhead involved in splitting up a monolithic design is not repaid in improved reliability.

    No, the joints were designed pretty good. Just not perfect. An effect that they claim was unknown caused the rubber to be less flexible when cold. No problem. Because of good design, there were two rubber seals that function as a backup for each other. That is how they were designed. In practise they noticed the backup being used, when it shouldn't have. They should have investigated why the backup seal was getting loaded/used, and figured out the correlation with launch temperature. Then they should've postponed the Jan 28 1986 launch.

     

    As Feynmann wrote: It is NOT a technical problem that brought challenger down. It is the organizational problems at NASA that bring spaceshuttles down.

     

    They repeated the display of organizational mismanagement on the columbia disaster. They had two weeks to take a look at the damage of the wing, but waived it away. They should've taken a look, said: "Whoa, that looks larger than we expected" and then scrambled for a solution. Launching an unplanned rescue mission is one, plugging the hole with tools and water-ice was another. Deciding not to take a look is the biggest blunder.

     

    (When a spaceshuttle crashes, an investigation is launched. So at two points in time we have the evidence that NASA is being mismanaged. Do you think NASA functions correctly when we're not looking? Ha!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 14 years ago in reply to e14 Contributor

    coder27 wrote:

    Interestingly, the shuttle's solid rocket boosters perhaps should have been built as a monolithic unit, but instead were built in segments to facilitate transport.  But the poorly-designed segment joints caused the Challenger tragedy. Sometimes, the overhead involved in splitting up a monolithic design is not repaid in improved reliability.

    No, the joints were designed pretty good. Just not perfect. An effect that they claim was unknown caused the rubber to be less flexible when cold. No problem. Because of good design, there were two rubber seals that function as a backup for each other. That is how they were designed. In practise they noticed the backup being used, when it shouldn't have. They should have investigated why the backup seal was getting loaded/used, and figured out the correlation with launch temperature. Then they should've postponed the Jan 28 1986 launch.

     

    As Feynmann wrote: It is NOT a technical problem that brought challenger down. It is the organizational problems at NASA that bring spaceshuttles down.

     

    They repeated the display of organizational mismanagement on the columbia disaster. They had two weeks to take a look at the damage of the wing, but waived it away. They should've taken a look, said: "Whoa, that looks larger than we expected" and then scrambled for a solution. Launching an unplanned rescue mission is one, plugging the hole with tools and water-ice was another. Deciding not to take a look is the biggest blunder.

     

    (When a spaceshuttle crashes, an investigation is launched. So at two points in time we have the evidence that NASA is being mismanaged. Do you think NASA functions correctly when we're not looking? Ha!)