Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Ethernet port turned off after few minutes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 713 subscribers
  • Views 4489 views
  • Users 0 members are here
  • raspberry
  • help
  • helpme
  • ethernet
  • port
  • raspberry_pi
  • raspberrypi
  • off
  • turned
Related

Ethernet port turned off after few minutes

e14 Contributor
e14 Contributor over 14 years ago

I am using 5V 1300mA adapter (http://www.skross.com/product/en/15/USB-Charger/56/World-USB-Charger.html) to power my Pi and another cheaper adapter that gives 5V 800mA.

 

The SD card is KINGSTON 16GB 100X SD10-HC.

 

I plugged in my Ethernet cable into the port and booted off Debian image from http://downloads.raspberrypi.org/images/debian/6/debian6-19-04-2012/debian6-19-04-2012.zip (SSH enabled). I am able to SSH into the Pi remotely and run basic commands, top, ps, ping. After about 15 minutes, the Ethernet LEDs just went off and my SSH session is gone too.

 

Checking the voltage at TP1 with my DMM it reads between 4.75 to 4.8V when the Ethernet is up and 4.9V when the Ethernet is down, i.e. the 3 LEDs marked FDX, LNK and 10M are off.

 

The same symptom is happening with both adapters. I have nothing else plugged into the Pi except the power and Ethernet cable.

 

Could this be another power problem? Anyone else seeing similar issue?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Mine should be the second batch then since it's using HanRun HR901110A and the manufacturing date on the board says 1213.  I will have to find the HTC charger to try it out and will report back if that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    So I tried HTC One X charger rated at 5V 1A but the Ethernet still shuts down after less than 5 minutes. I was able to SSH in before it went down though. I have sent RMA to element14 and they will be picking my unit up tomorrow for inspection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Nate1616

    Most of the problems I've seen have been from the cheap parts that the user supplies (bad power supply, bad SD card). Or perhaps not necessarily "bad" but "incompatible with the R-Pi requirements" which you could argue is a design problem, in that it apparently is more picky about USB supply voltage and SD card timing(?) than most other devices that use them.  I've seen relatively few reports of boards being returned due to apparent failures of the hardware itself. Apparently there are 10k+ units out in the field now. If there was a 1% field failure rate (not too bad for first run of a brand-new board), that would be 100 units. I suspect we don't hear about most of the ones that are working fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to Nate1616

    I would like to know what fraction of the 10K or so units out there came up with no problems.  It does sound like there are lots of problems, but maybe that's just because there are lots of units.  Personally, I would not blame bad design.  However, RasPi does seem to be sensitive to power supply voltage and it may be that expecting any correctly-labeled USB power supply to work with any correctly-labeled micro USB cable was too optimistic.  Perhaps RasPi will need to ship with a qualified power supply and cable.  I don't have much personal experience with polyfuses but if RasPi's troubles with them are typical then I'm not impressed with them.

     

    Along with quality of parts, another unknown is quality of manufacturing.  For example, are some of the heat-related issues people are reporting caused by poor solder joints?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to e14 Contributor

    it does seem that its picking in what card and power supply is used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    I work for a company that does consumer electronics. Some time ago we used some "PTC Resettable Fuses" (generic term for PolySwitch(tm), Polyfuse(tm), Multifuse(tm) etc) and I recall hearing they were one among a few troublesome components we had on the board. That design was before my time though; our current products use only the conventional type of non-resettable fuse. It might have been a specific vendor, or a design tolerance issue, I don't know.

     

    "Since a PPTC device has an inherently higher resistance than a metallic fuse or circuit breaker at ambient temperature, it may be difficult or impossible to use in circuits that cannot tolerate significant reductions in operating voltage, forcing the engineer to choose the latter in a design."

    ...from http://en.wikipedia.org/wiki/Resettable_fuse

     

    The Arduino 2009 contained a 500 mA polyfuse on the USB +5V input, and I haven't heard about many problems with that. Of course the Arduino itself only uses around 30 mA and I measure a fairly negligible 11.4 mV across its polyfuse.   http://arduino.cc/en/Main/ArduinoBoardDuemilanove

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Looks like the SD card problem may have just got a bit better now-  new firmware & kernel has apparently fixed some things:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=2&t=6093

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    However, RasPi does seem to be sensitive to power supply voltage and it may be that expecting any correctly-labeled USB power supply to work with any correctly-labeled micro USB cable was too optimistic.

     

    In addition to that, I think there may be a rather important practical difference between "USB power supply" and "USB cellphone charger".

     

    While they may be one and the same thing in the eyes of the USB spec, in practice the cellphone charger is made for the sole purpose of charging the cellphone with which it is bundled, and given the nature of the cellphone market, that charger will be made to the lowest cost possible.  It wouldn't surprise me at all to discover that it's only in-spec when charging the phone, and at no other current draw.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to morgaine

    You make a good point Margaine in that most phone chargers are made with the cheapest parts possible and are typicaly junk.  these probably wouldnt be the best for anything but charging your phone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Nate1616

    Old news?

    I have several mains power (110VAC) to USB power sources. The one that came with my HTC phone is marked 2Amps and works well. Others that have no marked spec. or say 1A or so, just won't charge the HTC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I have just received a replacement unit from element14 to replace my older unit that had the Ethernet issue. It took 2 weeks for the replacement to arrive though but I have no complain there! :)

     

    The new unit appears to work normally for now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • M0DCD
    M0DCD over 14 years ago in reply to e14 Contributor

    There has been mentioned on other Pi forums an issue with the LAN9512 IC that controls the USB and Ethernet. It is to do with intermittant operation of the 25MHz clock around the device. Seems if it's touched with a scope probe it may spark into life, it's possibly one of these things you can't pick up until you've built thousands of them.

     

    I have noted that some have added a stick on heatsink to the LAN7512 - but have had no report about if this does actually work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • M0DCD
    M0DCD over 14 years ago in reply to e14 Contributor

    There has been mentioned on other Pi forums an issue with the LAN9512 IC that controls the USB and Ethernet. It is to do with intermittant operation of the 25MHz clock around the device. Seems if it's touched with a scope probe it may spark into life, it's possibly one of these things you can't pick up until you've built thousands of them.

     

    I have noted that some have added a stick on heatsink to the LAN7512 - but have had no report about if this does actually work.