Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Wireless network conectivity
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 75 replies
  • Subscribers 707 subscribers
  • Views 10232 views
  • Users 0 members are here
  • raspberry
  • pi
  • wireless
Related

Wireless network conectivity

wallarug
wallarug over 14 years ago

I bought one of these about 12 mths ago: http://www.jaycar.com.au/productView.asp?ID=YN8306&keywords=high+power+wireless+n&form=KEYWORD

I downloaded the drivers from the link above then installed them on a windows computer.  How do I use these linux drivers/installers on the raspberry pi to get the wireless adaptor to work?

 

Will this work with the Raspberry Pi?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    If your adaptor uses Broadcom chipset you may need to install a piece of firmware to make it work. I had a similar problem with my Linux netbook that had Ralink wifi. It booted up but said that there was no WiFi as no firmware was loaded! After much searching the solution is at http://linuxwireless.org/en/users/Drivers/b43.

     

    The B43 package installs the firmware needed to run the Broadcom chipset. As its not GPL it can't be released with any Linux package, but is able to be extracted from the Windows driver. This package is already to go, just install!

     

    I required the firmware-b43-installer package. Not sure if it's in the RasPi repositories as I haven't got mine to play with yet... :-( But the above site it fairly comprehensive!

     

    Hope it works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    i have had issues with broadcom on various laptops using different distro's of linux, this is the best solution i have found so far. i also cant confirm at the moment if the b43 firmware is in the repositories. i will check tonight and see if it is.

     

    i cant actually try this on the R-Pi as i dont have a USB wifi adapter with the broadcom chipset.

     

    http://ubuntuforums.org/showpost.php?p=10527475&postcount=5

     

    hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    Thats ok.  but I found this site which looks interesting, I am posting it here so I can find it later image

    http://linux.die.net/man/8/iwconfig

     

    For fixing a file I messed up.

    http://elinux.org/RPi_Peripherals#Wireless:_TP-Link_TL-WN722N_USB_wireless_adapter_.28Debian_6.29

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    I bought the Edimax EW-7811Un but I need help setting it up, Steve, could you please help me with this one.  The RPi wiki says that it is verified but there is no guide to set-up this device for Raspbian.  I found this guide: http://www.ctrl-alt-del.cc/2012/05/raspberry-pi-meets-edimax-ew-7811un-wireless-ada.html but it has not worked for my RPi.  I think it has something to do with me not being able to get the rpi-update thing.  I tried to get this but failed.  Everytime I run rpi-update it returns:

     

    /usr/bin/rpi-update: line 1: syntax error near unexpected token `newline'

    /usr/bin/rpi-update: line 1: `<!DOCTYPE html PUBLIC "-//W3C//DTD XHTML 1.0 Trans                                                                             itional//EN" "http://www.w3.org/TR/xhtml1/DTD/xhtml1-transitional.dtd">'

     

     

    Can this be fixed so that I can update the firmware?

     

    Wireless card help would be nice as well image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to wallarug

    I noticed from the link that Edimax uses the rtl8192cu driver.  I have another adapter (Asus USB-N13) which uses that driver and it did not work by default with the current Raspbian Wheezy image.  However, it did work ok with Adafruit's new image as it includes that driver, so you may want to give that a try: http://learn.adafruit.com/adafruit-raspberry-pi-educational-linux-distro/occidentalis-v0-dot-1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to GreenYamo

    With the EDIMAX, it gives me the errors:

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

     

    The "name of the parts" are all different.

     

    What can be done to fix this issue?  This might sovle my problem.

     

    How do you unpack a .ko file?

     

    I didn't unpack mine.  this could be leading to the above issues.








     

    Message was edited by: Fergus Byrne

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to fustini

    Drew Fustini wrote:

     

    I noticed from the link that Edimax uses the rtl8192cu driver.  I have another adapter (Asus USB-N13) which uses that driver and it did not work by default with the current Raspbian Wheezy image.  However, it did work ok with Adafruit's new image as it includes that driver, so you may want to give that a try: http://learn.adafruit.com/adafruit-raspberry-pi-educational-linux-distro/occidentalis-v0-dot-1

    I do not really want to change image (right now).  But I might give it a go in the future.

     

    Right now though, I just want to get this adapter working. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to wallarug

    My guess is that the 8192cu.ko module you have doesn't agree with the version of the kernel your running.  a .ko file is a kernel module file and shouldn't have to unpacked.  the utility "modinfo" will print out information about the module.  could you run that and paste the output?  also, could you paste what "uname -a" outputs?  it might be that the kernel versions don't agree.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to fustini

    will do image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Hey drew,

     

    I installed Occidentalis v10.1 successfully onto my Raspberry Pi's SD card and went to /etc/network/interfaces to add my SSID and password where it wanted me to add it. But for some reason I still can't connect to the Internet wirelessly when my wireless dongle is connected in (I'm using the Zyxel NWD2105 which uses Ralink firmware). When adding my SSID do I keep the quotation marks so it's SSID "xxxx" or do I remove the quotation marks? Is there anything else I must do to get my dongle working?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    Hi Ahmad,

     

    I believe you should keep the quote marks.  An alterative to configuration via /etc/network/interfaces would be to wicd which is a GUI network manager that allows you to configure your wifi adapter.  You should be to install it by entering into the command line: "sudo apt-get install wicd" (while connected to Internet via Ethernet).  I wrote up more detailed instructions in this comment before:

     

    http://www.element14.com/community/docs/DOC-44703/l/raspberry-pi-wifi-adapter-testing#comment-15744

     

    I didn't try to install wicd it on the Adafruit image yet, so I think I'll give it a go this weekend.  I had installed wicd on the "official" Raspbian Wheezy image and it worked well.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to fustini

    Drew Fustini wrote:

     

    My guess is that the 8192cu.ko module you have doesn't agree with the version of the kernel your running.  a .ko file is a kernel module file and shouldn't have to unpacked.  the utility "modinfo" will print out information about the module.  could you run that and paste the output?  also, could you paste what "uname -a" outputs?  it might be that the kernel versions don't agree.

    Here's the output from uname -a:

    Linux raspberrypi 3.1.9+ #168 PREEMPT Sat Jul 14 18:56:31 BST 2012 armv6l GNU/Linux

     

    I also fixed the problem of the :

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

     

    ...by deleting the driver (8192cu.ko file).

     

    Which leads me to suspect that the RPi s/ware didn't like it.

     

    I can now also tell you that the output of lsusb is:

    Bus 001 Device 007: ID 7392:7811 Edimax Technology Co.,Ltd EW-7811Un 802.11n Wireless Adapter [Realtek RTL8188CUS]

     

    I hope this helps you solve my problem.  I also found someone who had the same problem and am reading what they did now: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=6256&hilit=edimax&start=575

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago in reply to fustini

    Drew Fustini wrote:

     

    My guess is that the 8192cu.ko module you have doesn't agree with the version of the kernel your running.  a .ko file is a kernel module file and shouldn't have to unpacked.  the utility "modinfo" will print out information about the module.  could you run that and paste the output?  also, could you paste what "uname -a" outputs?  it might be that the kernel versions don't agree.

    Here's the output from uname -a:

    Linux raspberrypi 3.1.9+ #168 PREEMPT Sat Jul 14 18:56:31 BST 2012 armv6l GNU/Linux

     

    I also fixed the problem of the :

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

     

    ...by deleting the driver (8192cu.ko file).

     

    Which leads me to suspect that the RPi s/ware didn't like it.

     

    I can now also tell you that the output of lsusb is:

    Bus 001 Device 007: ID 7392:7811 Edimax Technology Co.,Ltd EW-7811Un 802.11n Wireless Adapter [Realtek RTL8188CUS]

     

    I hope this helps you solve my problem.  I also found someone who had the same problem and am reading what they did now: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=6256&hilit=edimax&start=575

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wallarug
    wallarug over 14 years ago in reply to wallarug

    THIS IS A MUST ADD TO THE WIKI! (it is already there but is not advertised very well)

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=6256&hilit=edimax&start=600 

     

    http://dl.dropbox.com/u/80256631/install-rtl8188cus.txt

     

    and

     

    http://dl.dropbox.com/u/80256631/install-rtl8188cus-latest.sh

     

    These solved all my problems in less than 15minutes.  Keep in mind that it only works for some adapters, which are listed on the 1st link.

    The script also installs all the latest updates for the RPi (rpi-update) as well as setting up your wireless.

     

    Great job,  MrEngman

     

    I still wonder how to install my other device though.  So if anyone finds this out, please let me know (it is not really that important now).

     

    Fergus.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

     

    ...by deleting the driver (8192cu.ko file).

     

    Which leads me to suspect that the RPi s/ware didn't like it.

    What those messages tell you is that the module you compiled was built against a different kernel than the one you're running. Sometimes this can be as simple as having the exact same kernel source, but just one option has been changed in the .config

     

    To build external modules you need the correct kernel source tree and the .config from the running kernel. You can usually obtain this from the /proc/config.gz file.

     

    It's difficult to cover every possible problem in just a few lines, but here's a basic outline of how it should be done - no idea if this would work for you though

     

    cd /home/pi  - or wherever

    git clone https://github.com/raspberrypi/linux.git - this should leave you with a 'linux' directory eventually, it will take some time

    cd linux

    cp /proc/config.gz .   - copy config of running kernel

    gunzip config.gz       - unpack config

    mv config .config      - move it to (dot)config that leading . is necessary !

    make oldconfig         - this configures the kernel source with the config of your running kernel

     

    if make oldconfig asks lots of confusing questions you don't know how to answer, try make silentoldconfig instead

     

    at this point you can go and build your driver, but you must make sure it uses the kernel source tree you've just configured. You likely need to change two symlinks under /lib/modules/* for this to work properly like this:

     

    rm /lib/modules/`uname -r`/build

    rm /lib/modules/`uname -r`/source

    ln -s /home/pi/linux /lib/modules/`uname -r`/build

    ln -s /home/pi/linux /lib/modules/`uname -r`/source

     

    now build and install your external driver module.

     

    It's sometimes the case that you'll end up with two conflicting versions of a driver, you can search for them like this

     

    find /lib/modules/`uname -r`/ -name 8192cu.ko

     

    if that finds more than one, delete all of them and then re-run the drivers install.

     

    When you're done, run depmod -a hopefully the driver install did it for you, but sometimes they don't.

     

    You should then be able to run modprobe 8192cu to load the module. dmesg will show you any errors.

     

    I hope some of the above helps, but no guarantees - too many assumptions in there for guarantees image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    8192cu: disagrees about version of symbol <name of part>

    8192cu: Unknown symbol <name of part> (err -22)

     

    ...by deleting the driver (8192cu.ko file).

     

    Which leads me to suspect that the RPi s/ware didn't like it.

    What those messages tell you is that the module you compiled was built against a different kernel than the one you're running. Sometimes this can be as simple as having the exact same kernel source, but just one option has been changed in the .config

     

    To build external modules you need the correct kernel source tree and the .config from the running kernel. You can usually obtain this from the /proc/config.gz file.

     

    It's difficult to cover every possible problem in just a few lines, but here's a basic outline of how it should be done - no idea if this would work for you though

     

    cd /home/pi  - or wherever

    git clone https://github.com/raspberrypi/linux.git - this should leave you with a 'linux' directory eventually, it will take some time

    cd linux

    cp /proc/config.gz .   - copy config of running kernel

    gunzip config.gz       - unpack config

    mv config .config      - move it to (dot)config that leading . is necessary !

    make oldconfig         - this configures the kernel source with the config of your running kernel

     

    if make oldconfig asks lots of confusing questions you don't know how to answer, try make silentoldconfig instead

     

    at this point you can go and build your driver, but you must make sure it uses the kernel source tree you've just configured. You likely need to change two symlinks under /lib/modules/* for this to work properly like this:

     

    rm /lib/modules/`uname -r`/build

    rm /lib/modules/`uname -r`/source

    ln -s /home/pi/linux /lib/modules/`uname -r`/build

    ln -s /home/pi/linux /lib/modules/`uname -r`/source

     

    now build and install your external driver module.

     

    It's sometimes the case that you'll end up with two conflicting versions of a driver, you can search for them like this

     

    find /lib/modules/`uname -r`/ -name 8192cu.ko

     

    if that finds more than one, delete all of them and then re-run the drivers install.

     

    When you're done, run depmod -a hopefully the driver install did it for you, but sometimes they don't.

     

    You should then be able to run modprobe 8192cu to load the module. dmesg will show you any errors.

     

    I hope some of the above helps, but no guarantees - too many assumptions in there for guarantees image

     

    I am a linux n00b,  I read something and think that was what the problem could be. Anyway, the problems are all solved for me anyway.

     

    thanks for the help. image

     

    Message was edited by: Fergus Byrne

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    YEPPY!!

     

    I worked it out after 6 months of trouble.

     

    I found these instructions: http://elinux.org/RPi_Ralink_WLAN_devices

    ...Which I then used to install the card as my second Wireless interface.

     

    Install the wpasupplicant and the ralink firmware:

    1) sudo apt-get install wpasupplicant

    2) sudo apt-get install firmware-ralink

    Restrict access to /etc/interfaces so only root can read it (in this method, this file will contain your network password):

    3) sudo chmod 0600 /etc/network/interfaces

    Edit you /etc/network/interfaces:

    4) sudo nano /etc/network/interfaces

    5) The file already contains the configuration for eth0 (your Ethernet port) and looks something like this:

    auto eth0 iface eth0 inet dhcp  

    add the following lines below, enter you network name (ssid) and password:

    iface wlan0 inet dhcp wpa-ssid <your network ssid here>  wpa-psk <your network password>  

    6) save the file.

    The network interface will connect every time the RPi boots up. To connect it now manually, run:

    7) sudo ifup wlan0

     

    I hope someone can now add this to the wiki as a working adapter.

     

    Ralink Technology, Corp. RT2870 Wireless Adapter

    ID: 148f:2870

     

    Must be used with a powered hub and works out-of-the-box with Raspbian (August 16th 2012 --> From Raspberrypi.org Download page)

     

    The only real instructions required are:

    1. Image card and go through normal set-up

    2. Plug in card and confirm that it is what it says it is using "lsusb" command

    3. Type in "sudo nano /etc/network/interfaces"

    4. Add the following lines:

    auto lo

     

    iface lo inet loopback

    iface eth0 inet dhcp

     

    allow-hotplug wlan0

     

    auto wlan0

     

    iface wlan0 dhcp

    wpa-ssid <insert name of your ssid here using inverted commas " ">

    wpa-psk < insert password of access point here using inverted commas " ">

    5. Use the command "sudo ifup wlan0"

    6. Let the device connect

    7. You should be connected.

     

     

    Thanks for all the help.

     

    This problem is now SOLVED.

     

    Fergus.