Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum DC to DC Converter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 707 subscribers
  • Views 5647 views
  • Users 0 members are here
  • raspberry
  • pi
  • converter
  • raspberry_pi
  • battery
  • rpi
  • supply
  • power
Related

DC to DC Converter

e14 Contributor
e14 Contributor over 14 years ago

I want to run my RPi from DC sources.  (1) 12 volt sealed cell battery.  (2) 2 to 4 cell lithium packs, and (3) perhaps even a set of AA batteries.  As we know, the RPi gets glitchy if not running right around 5v, with a load applied.  Therefore I am looking for a converter (or converters, if one is needed for each situation) that will work with the above sources.  With the 12v and lithium batteries I'll need to set a cut-off voltage, so I don't kill the battery.  If the output voltage can't be maintained at 5v when under load then I'll need a method of tweaking the output for a given load situation.  Obviously, since this is for an RPi project, I don't want a converter that is the size of a PC power supply; the smaller the better.

 

Are there such off-the-shelf converters that I could use and if so then can someone point me to them?

 

Thank you in advance,

Andrew

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Andrew and Morgaine,

     

    It is kind of easy, but it all depends on how much electronics you're into. The trickiest part is if you want to be able to charge the batteries while using the R-Pi.

     

    So, let's drill into it! Powering the R-Pi:

     

    (1) 12 volt sealed cell battery.

     

    This is the most easy one: a linear regulator (LM7805) with a heat dissipator and 2 bypass capacitors should do the trick.

     

    (2) 2 to 4 cell lithium packs

     

    It depends... with the packs in series  (2S or 2P2S) you have between 5.6V and 7.3V. In that case, the voltage is too low for a 7805.

    The circuit is almost the same, but using a LP2954-5V or a LM2940CT-5.0, the last one being more common. A 2S2P pack would drain in around 1-2 hours.

     

    (3) perhaps even a set of AA batteries.

     

    I would go for 4 AA batteries and a LM2940CT-5.0. The problem is that they will discharge very quickly and the system will shutdown.

    The most beautiful solution I can think of is a 2AA pack running thru a LT1302 boost converter (see the Minty Boost http://www.adafruit.com/products/14). The main problem is that they would drain in around 1 hour...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Rafael, although I know that sealed lead-acid batteries recombine their H and O  so that outgassing through the pressure release valve should occur only rarely or never, I remember an issue I encountered while researching uninterruptible power supplies.  They're pretty universally spec'd to require ventilation, despite using these "sealed" batteries.  This makes me anxious.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Yes, Morgaine, you are right.

     

    Lead-acid batteries should not be kept on closed places, although just small vents are enough to release the gas in sealed batteries.

     

    Hydrogen is too light, so it dissipates pretty quickly, and there is not enough released gas to make it explosive in a room, maybe just in closed cabinets.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Yes, Morgaine, you are right.

     

    Lead-acid batteries should not be kept on closed places, although just small vents are enough to release the gas in sealed batteries.

     

    Hydrogen is too light, so it dissipates pretty quickly, and there is not enough released gas to make it explosive in a room, maybe just in closed cabinets.