Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum "Best Power Supply for the Raspberry Pi"?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 709 subscribers
  • Views 3439 views
  • Users 0 members are here
  • raspberry_pi
  • raspberrypi
  • rpi
  • adafruit
Related

"Best Power Supply for the Raspberry Pi"?

fustini
fustini over 14 years ago

Hi, I came across this video comparing USB chargers for the Pi today:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I've been using the Adafruit power supply he shows.  Interestingly, it is designed to output 5.25V:

 

http://www.adafruit.com/products/501

This adapter was specifically designed to provide 5.25V not 5V, but we still call it a 5V USB adapter. We did this on purpose to solve a problem that occurs often with USB-powered gadgets: they draw so much current than the resistance of the cable causes a voltage drop, so instead of 5V, the device sees 4.75V or so. To avoid this problem, we made the adapter 5.25V. This is because the USB power specification allows up to 5.25V, and its safe for all 5V electronics, and has the benefit of making up for any loss due to thin USB cables. Basically, you can use it where ever USB 5V power is needed, with no risk of damage, and it will happily work at the full current range, no matter what cable you use!

Is there any downside to having a USB power supply output 5.25V?  If it's within USB spec, then I wonder why all supplies without a built-in cable don't do this.

 

Cheers,

Drew

 

UPDATE: that YouTube user also has an interesting Pi temperature video, too:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    Most chargers I've seen say "5.1V".  This permits a 100mV drop across the Micro USB cable, e.g., 1A across a 0.1 Ohm cable.  To amplify Morgaine's comment, you really don't want to try to manufacture a 5.25V supply, as there needs to be some tolerance.  An excellent regulator will give you 2%, which is 100mV.  5.1V is 3% away from max USB voltage, which gives you a comfy margin.

     

    A potential problem with RasPi is that its 3.3V linear regulator RG2 gets hotter with higher 5V, which could expose a heat-related problem such as an iffy polyfuse F3.  YMMV, but it could affect some RasPis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    This permits a 100mV drop across the Micro USB cable, e.g., 1A across a 0.1 Ohm cable. 

    All of the micro usb cables I was able to get my hands on were about 0.5 ohm in both ground and 5v lines, so lots of voltage drop @ 450-ish mA

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    This permits a 100mV drop across the Micro USB cable, e.g., 1A across a 0.1 Ohm cable. 

    All of the micro usb cables I was able to get my hands on were about 0.5 ohm in both ground and 5v lines, so lots of voltage drop @ 450-ish mA