Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Hardware fixes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 709 subscribers
  • Views 5089 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Hardware fixes

e14 Contributor
e14 Contributor over 14 years ago

So one of the things I plan to do when R-Pi are more available is to butcher a couple of them and incorporate some things I consider to be appropriate hardware fixes. This is my list so far, any feedback or additional suggestions welcome.

 

1. Remove the SD Card slot and replace it with a small adapter pcb containing a micro-sd connector. The full size SD card sticking out the end is ok for development or when you want to swap the card a lot, not so good when you want to build the whole Pi into something else and would like to use some of that dead space for other things. 1764377 micro-sd connector chosen, will be oriented at right angle to the current slot.

 

2. Replace usb polyfuse arrangement. Diodes Inc AP1212 seems to fit the bill. 1825303 33 pence each

 

3. Replace RG1 & RG2. Current plan is to use the TPS54231 1755637 as suggested by jamodio, however it's relatively expensive. Also looking at AP1533, 1825334 which appears similar from an external components point of view, but approx 1/10 the cost.

 

4. Cut the 1.8v from the Lan9512. Could do with the full gerbers to work out if this is possible. C29, C36 & C43 along with pins 15 & 38 just vanish into vias. Ideas welcome.  My other options are to remove the Lan9512 and make myself a model A, or to leave RG1 off and see if we still boot with 1.8v from the lan9512 regulator.

 

5. As I'll be replacing the SD card slot, I'm contemplating if it's possible to add some power switching to allow running the slot at 1.8v to get some of the faster access modes. I think this will probably need some driver work and stealing a gpio from somewhere. I'd be tempted to use GPIO5 or GPIO27 (CAM_CLK, CAM_GPIO), but maybe the GPU will mess with those and GPIO31/CONFIG3 could be a better choice.

 

6. RTC based on MCP79410, 1823155

 

7. Removal of micro-usb power connector as I don't consider it appropriate. 5v and 3.3v can be supplied via P1 instead.

 

If only 1.8v was available on P1, some things could have been easier. So...

 

8. Replace P1 with a 28 pin connector to allow 1.8v to be made available. The extra two pins to extend off the end on the pcb and be wired to RG1's previous position.

 

9. For ease of integration, put P1 on the underside of the board and likely also replace P4 & S7 with headers allowing their connectors to be moved onto the underlying board and aligned better wrt case.

 

Thoughts ?

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 14 years ago

    There is another DC-DC converter I'm testing for another design from Intersil, ISL9104 500mA 4.3MHz high efficiency, very small package and cheap, few external components.

     

    The Alpha board had DC-DC converters and apparently a better power supply design. The micro USB and phone chargers is turning to be a really bad idea, so I agree about changing that, actually I'm powering the board from the P1 header.

     

    Yes without the Gerbers is not easy to envision what kind of "blue wire" fixes can be done.

     

    I'm thinking seriously if after all there is enough interest and momentum to start a true "open source hardware" development.for a Pi like board, with parts that are documented. Even if I understand the reasons I don't like at all that the Pi design was built around a part that has practically no documentation publicly available.

     

    I may be able to get some funding and people interested to support an open project, perhaps I should exchange some lines with Jim Manley that seems interested to the right thing.

     

    I'm really pissed with all the secrecy, conspiracy, mystery, bad vibes and misinformation emanating from RPF.

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    I'm thinking seriously if after all there is enough interest and momentum to start a true "open source hardware" development.for a Pi like board, with parts that are documented.

    I could certainly be interested, but I see two stumbling blocks. First is that anything with a GPU is unlikely to have good enough docs, second is that anything without a GPU seems unlikely to have the sort of mass market appeal to get the cost down to something reasonable.

     

    The rhombus-tech guys seem to be a reasonable way along this road already, with some interesting info like the cpus they've evaluated: http://rhombus-tech.net/evaluated_cpus/

    However they seem to be a long way from an actual released product and I'm not at all convinced of the EOMA-68 form factor. Although I do like the idea of a set of standard interfaces.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Sure, at $89 BeagleBone sounds like a lot of money, but I expect it's quite reasonable given the quantities sold.  If more people get behind BeagleBone, the costs would come down to something closer to RasPi.

    Looking at BeagleBone on uk.farnell.com the other day, out of stock. Approx 300 available for delivery sometime between now and 2nd week in August.

    Compare to the 12000+ available for delivery on 23rd July that the Pi was showing a few days ago and the difference in scale is clear.

     

    You have to give the RPF credit for managing to get the interest and backing to be able to ramp up to where they are in such a short time. They seem to be the only ones to have managed it so far. As everyone keeps pointing out there's plenty of other boards out there, but none seem to be gaining the necessary momentum.

     

    How much of the success of the R-Pi is down to aiming low to begin with and praying that the interest will be there ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    ... As everyone keeps pointing out there's plenty of other boards out there, but none seem to be gaining the necessary momentum.

     

    How much of the success of the R-Pi is down to aiming low to begin with and praying that the interest will be there ?

    I think the success of RasPi is the US$25 price.  "A computer for $25?  You've got to be kidding!"  And yes, they are kidding because you can't get the $25 unit, only the warmer $35 version.  Oh, and that doesn't include a case or compatible power supply or mass storage or monitor or cables or keyboard or mouse or any of the other gewgaws you expect to have with a computer -- but you already had those, right?  So there's a big red asterisk beside that "An ARM GNU/Linux box for $25" slogan.  Must be a new meaning of the word "box" I'm not familiar with.

     

    [I'm not complaining.  I knew exactly what I was getting when I ordered a RasPi and it's a great board for the price.  But having grown up reading MAD Magazine I dislike misleading marketing.  "An ad that's bad gets spoofed in MAD."]

     

    Anyway, the US$25 price point gets you interested.  When BeagleBoard came out in 2008, the US$150 price point was terrific for a tiny GNU/Linux capable development board, especially compared to the US$800 (IIRC) full-size board you could get from TI.  But as Morgaine has pointed out, US$35 buys you a good dinner with shipping paying for the tip.  The risk in buying a RasPi and discovering that it's useless for your needs is pretty low.  And US$35 is usually below the level requiring spousal approval.

     

    I imagine that the RPF is flabbergasted by the level of interest -- in a world where desktops are dominated by Windows and most consumer computers are closed consumption devices, who could imagine that you could sell 1 million uncased boards for which you have to download the operating system yourself and transfer it to an SD card.  I'm flabbergasted by the level of interest as well -- the idea that millions are becoming GNU/Lunix users is terrific and helps the future of computing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    at least you find out that the advertized $25 price isn't real before you

    commit to the purchase.   Only later do you find out that your keyboard

    doesn't work, or your SD card, or your power supply, or your usb hub,

    or your wifi dongle, or your mpeg-2 TV tuner, etc.   And only after getting

    everything to work do you find out the performance issues, that the hyped

    GPU isn't used for X acceleration, that the SD cards run slow, that the

    cpu overhead for USB interrupts is 20% at idle, the L2 cache isn't attached

    to the cpu, etc.  And then you find out about the intermittent problems,

    such as usb packet loss, SD card corruption, audio pops, failure to boot

    after working fine for a week, etc.

     

    All the front-page blog stories are happy stories, the sad stories are

    in the discussion forums, and the media hasn't picked up on them yet.

     

    I think it's interesting that half (10 of 19 by my count) of next month's

    magpi interview questions have to do with hardware fixes.  So that's

    clearly on people's minds.  We'll see if they actually answer those,

    or just dodge them like they've been doing so far.

     

    http://issuu.com/themagpi/docs/the_magpi_issue4_draft

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I think the success of RasPi is the US$25 price.  "A computer for $25?  You've got to be kidding!"  And yes, they are kidding because you can't get the $25 unit, only the warmer $35 version. 

     

    That's the sum total of it, it's all about price perception, and perception management which is a polite way of saying "lying".  RPF are good at it, and this seems to be why they don't like people messing them around with reasoned factual discussions.  It gets in the way of spin.

     

    Any competitor will have to live with the same magic price point though, $25, that's the key to mass adoption.

     

    Oh, and that doesn't include a case or compatible power supply or mass storage or monitor or cables or keyboard or mouse or any of the other gewgaws you expect to have with a computer -- but you already had those, right?

     

    Oh it wouldn't do to point out that after buying an SD card and several USB chargers to find one that works with Pi, your total investment could be higher than for BeagleBone which comes with a 4GB micro-SD card in the box and takes +5V from a generic barrel connector with proper power management so that everything "just works" without needing to play compatibility games.

     

    BeagleBone and Pi aren't directly comparable because each has benefits that the other lacks, but comparing price and nothing else, I spent more to get a basic 4GB system running on Pi than on BeagleBone, so my bank manager could validly claim that the BeagleBone was cheaper.

     

    It depends on what gear you happen to have around of course, but the "$25" tag is creative marketing that verges on deceitful because that expenditure alone doesn't give you a bootable system.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    At least they removed that silly picture on the front cover.

     

    I'll not deny that the R-pi was a good market test that if there is demand for this type of boards, but the success (not sure how to define that) in the rapid volume of units ordered was essentially driven by a misleading amount of hype and confusing messages, most of them emanating from RPF and its minions. Eben still today keeps saying that you can do whatever other computers do with the R-pi, which as we know is not quite true.

     

    When you get the beaglebone you know exactly what you are getting and all the parts used are documented and it is a true open source project, you get full Gebers, etc.

     

    Everything around the R-pi is a mystery cloud, and if you can't ask or comment freely.

     

    I'm almost sure that we'll see a lot of R-pis on eBay in the near future from people that got it because it was cool or some friends told them, etc, etc.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I could certainly be interested, but I see two stumbling blocks. First is that anything with a GPU is unlikely to have good enough docs, second is that anything without a GPU seems unlikely to have the sort of mass market appeal to get the cost down to something reasonable.

     

    The closed nature of GPUs will change one day, and that change may not even be so far away.  Although this is just a gut feeling, it's based on observing the rapid march of progress and the evolution of devices towards ever-greater complexity.

     

    Before long, basic graphic functionality will be taken for granted instead of being regarded as a crown jewel, and given the huge number of players in the ARM scene, I bet that someone will release a device with an openly documented graphics core.  It's almost inevitable as devices evolve and their subsystems turn into commodity functions.

     

    Also, there is steadily growing pressure towards making graphics drivers open-source, and that pressure isn't coming only from inside the FOSS community, but also from device manufacturers themselves because having to maintain closed drivers gets in the way of making profit.  Broadcom and nVidia are in denial about it, but Intel and AMD/ATI certainly aren't.

     

    Things are gonna change.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Things are gonna change.

    When ? 

    You're right that it only takes one to do it and they'll all have to..  To work though it really wants to be a shiny new competition trashing GPU that gets open drivers on the day of release. If it's an older or slower design (like the intel ones) it's not really making the case to the vendors with 10x the performance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    To work though it really wants to be a shiny new competition trashing GPU that gets open drivers on the day of release. If it's an older or slower design (like the intel ones) it's not really making the case to the vendors with 10x the performance.

     

    No no, my point was just the opposite --- that with the march of progress, what is crown-jewel functionality today is implemented as a commodity item tomorrow..  It's then no longer considered worthy of protection because it's completely lacklustre compared to the crown jewels of tomorrow.

     

    FOSS reinforces this still further.  When  beancounters sell product which includes a commodity function that is too basic for a marketing bullet point, they are less likely to want to fund a development team to create and support its software.  Open source gives them a cheap way out, so when selecting that commodity function, they'll pick an implementation that already has software available which costs them nothing.  Their accounting will drive it.

     

    Put both of those factors together and I expect tomorrow's "basic" functionality to include 2D and 3D acceleration and to have become open, despite the new crown jewels of the day still being myopically restricted.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I think we probably agree. We'll get some basic 3D functionality in the FOSS side, and probably sooner than later.

     

    We also seem to agree on the one constant being that progress happens and the world moves on.

     

    So my point is simply that by the time we get that basic 2D/3D FOSS driver will anyone care ?  What's been clear in both the linux world with the likes of KDE4 and in the windows world is that they're not developing for todays GPUs, they're developing for what they hope to have in a year or two.  Performance tends to be crappy on current hardware. So does getting that basic functionality help, or is it just hindering the eventual goal ?  Oh, and I don't pretend to know the answer to that question image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    So my point is simply that by the time we get that basic 2D/3D FOSS driver will anyone care ?  What's been clear in both the linux world with the likes of KDE4 and in the windows world is that they're not developing for todays GPUs, they're developing for what they hope to have in a year or two.  Performance tends to be crappy on current hardware. So does getting that basic functionality help, or is it just hindering the eventual goal ?  Oh, and I don't pretend to know the answer to that question image

     

    There's a directly relevant universal constant that applies here, commonly called "YMMV" and with a value of 'Always True'. image

     

    I know the answer to your question in my specific case:  there is no eventual goal, there is only the current moving target.  What's more, because I try to implement systems that make engineering sense rather than follow the latest fads and trends and eye candy, my machinery typically has almost no bloat, for example no KDE nor Gnome desktops which just get in the way of getting stuff done.

     

    Consequently, I'm totally happy with non-bleeding edge technology, because my lean software systems run like blue light even on older hardware.  For me then, the answer to your question is an unqualified 'Yes', the basic functionality is all important.

     

    I'm sure that others will object violently and demand 32 cores just to make their pointer crawl across their desktop, but that's their problem and I'm not a missionary out to convert them.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    So my point is simply that by the time we get that basic 2D/3D FOSS driver will anyone care ?  What's been clear in both the linux world with the likes of KDE4 and in the windows world is that they're not developing for todays GPUs, they're developing for what they hope to have in a year or two.  Performance tends to be crappy on current hardware. So does getting that basic functionality help, or is it just hindering the eventual goal ?  Oh, and I don't pretend to know the answer to that question image

     

    There's a directly relevant universal constant that applies here, commonly called "YMMV" and with a value of 'Always True'. image

     

    I know the answer to your question in my specific case:  there is no eventual goal, there is only the current moving target.  What's more, because I try to implement systems that make engineering sense rather than follow the latest fads and trends and eye candy, my machinery typically has almost no bloat, for example no KDE nor Gnome desktops which just get in the way of getting stuff done.

     

    Consequently, I'm totally happy with non-bleeding edge technology, because my lean software systems run like blue light even on older hardware.  For me then, the answer to your question is an unqualified 'Yes', the basic functionality is all important.

     

    I'm sure that others will object violently and demand 32 cores just to make their pointer crawl across their desktop, but that's their problem and I'm not a missionary out to convert them.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I can only aspire to that.. I find that those pesky Web2.0 people and their javascript have conspired to make most things unuseable, once you're dragged kicking and screaming onto a browser that finally works dependency hell topples all the other dominoes and you find yourself dragged into 'the future' whether you like it or not. Resistance is futile and all that image  I've come to accept that the rest of the world doesn't care what we want, we're not the target market after all.

     

    The eventual goal for me would be functional FOSS drivers for all current GPUs, you're right that's a moving target. I'm pragmatic enough to realise it's unlikely to happen anytime soon.

     

    OT, but related to those Web2.0 people, uk.farnell.com has recently gained a span that overlays the search box with a higher z order effectively making the site unuseable. It's a silly error in a style sheet, but one of those things that renders differently on different browsers as using it's shiny new eye-candy features. There is no escape image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    You're totally right about webbies and their mindless destruction of a web that used to work just fine.  It's a tautology, but webbies are beyond clueless.  That's not intended as abuse, but as a factual statement:  they manifestly do not have a clue about the broader issues of what they do, and when confronted with it, demonstrate that it is not within their ability to think about such issues.  All that matters is "cool", not engineering.

     

    I do however disagree with "resistance is futile".  A site that webbies have made unusable is one that they have designated not to be used --- 'most obliged for the hint.

     

    That works fine for me. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    I do occasionally consider organizing a NoJS conference though, with the goal of creating an alternative mirror web that complies fully with REST addressibility principles and doesn't make Roy Fielding want to jump off a bridge.

     

    Strictly no webbies invited of course, although there would be no danger of them coming anyway since a web without Javascript would make their single brain cell crash.  Also no Google, as the JS malaise runs deep there.  In contrast, DuckDuckGo have their heart in the right place.

     

    A web that runs 50 times faster, requires 50 times less CPU, and works on all equipment .... what a dream.  And it's totally achievable, because that's what we had before the webbie infestation.

     

    It's almost worth organizing an IETF working group to that end .... image image image