Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible Hardware fixes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 709 subscribers
  • Views 5098 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible Hardware fixes

e14 Contributor
e14 Contributor over 14 years ago

So one of the things I plan to do when R-Pi are more available is to butcher a couple of them and incorporate some things I consider to be appropriate hardware fixes. This is my list so far, any feedback or additional suggestions welcome.

 

1. Remove the SD Card slot and replace it with a small adapter pcb containing a micro-sd connector. The full size SD card sticking out the end is ok for development or when you want to swap the card a lot, not so good when you want to build the whole Pi into something else and would like to use some of that dead space for other things. 1764377 micro-sd connector chosen, will be oriented at right angle to the current slot.

 

2. Replace usb polyfuse arrangement. Diodes Inc AP1212 seems to fit the bill. 1825303 33 pence each

 

3. Replace RG1 & RG2. Current plan is to use the TPS54231 1755637 as suggested by jamodio, however it's relatively expensive. Also looking at AP1533, 1825334 which appears similar from an external components point of view, but approx 1/10 the cost.

 

4. Cut the 1.8v from the Lan9512. Could do with the full gerbers to work out if this is possible. C29, C36 & C43 along with pins 15 & 38 just vanish into vias. Ideas welcome.  My other options are to remove the Lan9512 and make myself a model A, or to leave RG1 off and see if we still boot with 1.8v from the lan9512 regulator.

 

5. As I'll be replacing the SD card slot, I'm contemplating if it's possible to add some power switching to allow running the slot at 1.8v to get some of the faster access modes. I think this will probably need some driver work and stealing a gpio from somewhere. I'd be tempted to use GPIO5 or GPIO27 (CAM_CLK, CAM_GPIO), but maybe the GPU will mess with those and GPIO31/CONFIG3 could be a better choice.

 

6. RTC based on MCP79410, 1823155

 

7. Removal of micro-usb power connector as I don't consider it appropriate. 5v and 3.3v can be supplied via P1 instead.

 

If only 1.8v was available on P1, some things could have been easier. So...

 

8. Replace P1 with a 28 pin connector to allow 1.8v to be made available. The extra two pins to extend off the end on the pcb and be wired to RG1's previous position.

 

9. For ease of integration, put P1 on the underside of the board and likely also replace P4 & S7 with headers allowing their connectors to be moved onto the underlying board and aligned better wrt case.

 

Thoughts ?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I can only aspire to that.. I find that those pesky Web2.0 people and their javascript have conspired to make most things unuseable, once you're dragged kicking and screaming onto a browser that finally works dependency hell topples all the other dominoes and you find yourself dragged into 'the future' whether you like it or not. Resistance is futile and all that image  I've come to accept that the rest of the world doesn't care what we want, we're not the target market after all.

     

    The eventual goal for me would be functional FOSS drivers for all current GPUs, you're right that's a moving target. I'm pragmatic enough to realise it's unlikely to happen anytime soon.

     

    OT, but related to those Web2.0 people, uk.farnell.com has recently gained a span that overlays the search box with a higher z order effectively making the site unuseable. It's a silly error in a style sheet, but one of those things that renders differently on different browsers as using it's shiny new eye-candy features. There is no escape image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    You're totally right about webbies and their mindless destruction of a web that used to work just fine.  It's a tautology, but webbies are beyond clueless.  That's not intended as abuse, but as a factual statement:  they manifestly do not have a clue about the broader issues of what they do, and when confronted with it, demonstrate that it is not within their ability to think about such issues.  All that matters is "cool", not engineering.

     

    I do however disagree with "resistance is futile".  A site that webbies have made unusable is one that they have designated not to be used --- 'most obliged for the hint.

     

    That works fine for me. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    I do occasionally consider organizing a NoJS conference though, with the goal of creating an alternative mirror web that complies fully with REST addressibility principles and doesn't make Roy Fielding want to jump off a bridge.

     

    Strictly no webbies invited of course, although there would be no danger of them coming anyway since a web without Javascript would make their single brain cell crash.  Also no Google, as the JS malaise runs deep there.  In contrast, DuckDuckGo have their heart in the right place.

     

    A web that runs 50 times faster, requires 50 times less CPU, and works on all equipment .... what a dream.  And it's totally achievable, because that's what we had before the webbie infestation.

     

    It's almost worth organizing an IETF working group to that end .... image image image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Dom said today:

     

          I agree that a small resistor is a better solution.  ...    

         The problem was that by the time the first report of the small resistor         

         fixing the reset problem was posted, the rev2 PCB had already been laid out.

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=5249&start=166

     

    I wonder exactly when the rev2 PCB was laid out, especially since PeteL

    was apparently getting up to speed on the 1.8V issue quite recently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    Dom said today:

     

          I agree that a small resistor is a better solution.  ...   

    It's really not. The better solution is to use a proper USB Power Switch IC like a AP1212 or similar that has a slow-start feature and big enough reservoir capacitors.  As Burngate said in the post after the one you linked, v2 is a backward step in this regard as it removes the possibility to do something better yourself.

    I wonder exactly when the rev2 PCB was laid out, especially since PeteL

    was apparently getting up to speed on the 1.8V issue quite recently.

    It was my thought that v2 was probably done in conjunction with the move to UK manufacturing. The chinese factory has built enough without needing holes for the ATE fixture, but a new manufacturer might well demand some improvements to help their process.

    I could obviously be wrong in that assumption, but if I'm right it would likely put it's layout at around the time of Pete's last visit here.  That ties in reasonably well with the 1.8v fix, but I'm also fairly sure the low ohm resistor ideas were being talked about much earlier. 

    But was anyone listening ?  One of the big problems I see with the level of interest in the Pi is that discussions inevitably get drowned out by the noise, especially in the RPF forums, and solutions with solid engineering reasoning often get blown out of the water or simply ignored by the clueless masses flapping around in the dark. Just look at jamoido's post on the RPF forum on the 1.8v thing, as far as I can tell it was completely ignored at the time.

    Not sure there's an easy solution though, the RPF is somewhat a victim of it's success and the way it's forums are run doesn't engourage proper discussion on issues or the engineering reasons why they're an issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I somtimes have the impression they really want to create confusion on the RPF forum.

    Like Jamesh agreeing there is a problem with the usb stack, and a bit later claiming that he fixed his stuck keys by replacing his supply...

    You don't need a 5000 euro usb analyser to test that theory. A simple lab adjustable power supply can do the trick.

    When I told them Element 14 was selling usb hubs for the Pi that apparently provided power on their upstream port, they said it wasn't their problem.

    Every technical question about the current progress on the issues is simply ignored....

    A lot of people have no problems. That sure helps if you go to a forum with a problem.

    But as Jamesh pointed out very accurate yesterday...It's just a waste of time...

    And even better I found ...how much more open can the foundation be?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    I reported the problem as soon as the schematics were released, I've no way of knowing when they realized there was a problem with it since nobody acknowledged or commented about it.

     

    I agree with selsinork that the resistors or even the complete elimination of the polyfuses/resistors on Rev 2.0 are not a solution but a quick "fix."

     

    It will be a solution when they finally accept an understand that the entire power design needs to be redone.

     

    Also promoting this fix saying that it has side benefits like powering the Rpi from a hub via a USB port opens another can of worms. While that approach is interesting for an experiment it is not a very good idea since the Rpi does not behave like a USB device and people with limited knowledge could end damaging the device provide power or even the Rpi.

     

    I really don't know who is leading over there the engineering side of the show, some claim that they work hard and put a lot of effort thinking about how to fix problems and improve the design, but for example the placement of the new P5 tells a different story, something not worth a "knighthood" image

     

    BTW did anybody seen the schematics for the Rev 2 board ?

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to jamodio

    They are on the elinux wiki - so I'm told.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to wallarug

    Fergus Byrne wrote:

     

    They are on the elinux wiki - so I'm told.

     

    The schematics on the Wiki are for the R1.0 board. Nothing yet for R2.0.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to jamodio

    I was told that someone changed them the day of the release of rev2.  They must have been wrong.  Oh well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>