Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Ethernet not working on RPI - my fault or the pi's?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 707 subscribers
  • Views 15962 views
  • Users 0 members are here
  • helpme
  • raspberry_pi
  • rpi
Related

Ethernet not working on RPI - my fault or the pi's?

e14 Contributor
e14 Contributor over 14 years ago

Hi Everyone,

 

I got my RPI yesterday from E14 in Australia.

 

I was really impressed but haven't been able to get ethernet working.

 

I get no link lights (only OK and PWR) on a 5v/1a power supply. I've tried booting with and without keyboard but no luck. I loaded raspbian but couldn't ping anywhere. When I checked my interfaces file I saw that eth0 didn't have an 'auto' step so I added that and tried a static configuration but no luck. From one of the if/lsusb commands I did see that the Ethernet seemed to have a MAC address (which I imagine means the system can at least sense the port) but I just don't know what to do after trying different cables...


I've tried raspbian and xbian but neither seems to work and I'm not sure how I could definatively confirm if my ethernet is the source (and sole) problem...

  • Sign in to reply
  • Cancel
  • wallarug
    wallarug over 14 years ago

    Have you tested the cable/connection with a different computer?  Does that work?

     

    I though I had a problem like this but I found that it was the connection/cable.  I wigglied it about and this got it working.  Maybe try a different cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    I've tried 2 different cables that both worked from my laptop to the router. I tried directly connecting the laptop to the pi with the cables (i read somewhere the port can auto-sense and crossover appropriately) and neither worked...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Ewan Watson wrote:

     

    I've tried 2 different cables that both worked from my laptop to the router. I tried directly connecting the laptop to the pi with the cables (i read somewhere the port can auto-sense and crossover appropriately) and neither worked...

    Are you using a router that is DHCP active?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Yes I am. Though I have tried manually assigning static IPs for the router and (of course) for the direct to laptop connection. I didn't even get a link light though which is why I am concerned that the problem is lower level than IP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Can I just confirm something. 

     

    The RPi is connected to a cable (that works) and the cable is then connected to a socket on your router (that you know works).

     

    Correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Yes. The RPi has been connected using 2 cables (that both work) to each of the 4 ports on the router (that all work). At no time did the raspberry pi show any lights or successfully ping anything (using dhcp or static)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago

    If "ip link ls eth0" displays a MAC address on the second line of output (link/ether) then it's a near certainty that everything is fine at interface link level, and all you need is a proper cable to your Ethernet switch or router for all the link LEDs to light up like a Christmas tree.  It's just a hardware problem so focus on getting those lights to appear before worrying about IP addresses or network configuration.  DHCP, IP addresses, and routing aren't relevant until your link lights are lit.

     

    Your tests so far seem to have eliminated the leads and the other end of the Ethernet connection though, so it rather looks like there could be a physical problem on the board.  Have a very close look at the Pi in the vicinity of the RJ45 looking for anomalies like poor solder joints, and peer inside the connector for any bent pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    It sounds you have network problems.  I can only see three possible issues:

     

    1. Your router is not giving out IP addresses for so reason / does not like the RPi image.

     

    2. One of the files that you modified is not correct (a fresh image would fix this)

     

    3. Your RPi is not functioning correctly (but I don't think this is the problem)

     

     

    Try re-imaging your SD card and start-up with the cable ethernet plugged in.  The other casue could be your power supply. Check: http://elinux.org/RPi_VerifiedPeripherals#Power_adapters to see if you have a problem power supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Thanks for that. I'm pretty sure I saw a mac address somewhere in testing and figured that meant the port was getting power but I just wasn't able to make it happy. I was thinking about making a loopback ethernet adapter but thats about as close as I go to technical. I'll check out the board when i get home (in about an hour) and see if anything is out of whack (but wouldn't know where to begin with fixing it..)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Mrjdy1
    Mrjdy1 over 14 years ago

    The first batch of RPI's that were sent out had faulty Ethernet port and the Foundation has - will replace then if you get in touch with them image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>