Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Ethernet not working on RPI - my fault or the pi's?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 710 subscribers
  • Views 15793 views
  • Users 0 members are here
  • helpme
  • raspberry_pi
  • rpi
Related

Ethernet not working on RPI - my fault or the pi's?

e14 Contributor
e14 Contributor over 14 years ago

Hi Everyone,

 

I got my RPI yesterday from E14 in Australia.

 

I was really impressed but haven't been able to get ethernet working.

 

I get no link lights (only OK and PWR) on a 5v/1a power supply. I've tried booting with and without keyboard but no luck. I loaded raspbian but couldn't ping anywhere. When I checked my interfaces file I saw that eth0 didn't have an 'auto' step so I added that and tried a static configuration but no luck. From one of the if/lsusb commands I did see that the Ethernet seemed to have a MAC address (which I imagine means the system can at least sense the port) but I just don't know what to do after trying different cables...


I've tried raspbian and xbian but neither seems to work and I'm not sure how I could definatively confirm if my ethernet is the source (and sole) problem...

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 14 years ago

    Have you tested the cable/connection with a different computer?  Does that work?

     

    I though I had a problem like this but I found that it was the connection/cable.  I wigglied it about and this got it working.  Maybe try a different cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 14 years ago

    Have you tested the cable/connection with a different computer?  Does that work?

     

    I though I had a problem like this but I found that it was the connection/cable.  I wigglied it about and this got it working.  Maybe try a different cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    I've tried 2 different cables that both worked from my laptop to the router. I tried directly connecting the laptop to the pi with the cables (i read somewhere the port can auto-sense and crossover appropriately) and neither worked...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Ewan Watson wrote:

     

    I've tried 2 different cables that both worked from my laptop to the router. I tried directly connecting the laptop to the pi with the cables (i read somewhere the port can auto-sense and crossover appropriately) and neither worked...

    Are you using a router that is DHCP active?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Yes I am. Though I have tried manually assigning static IPs for the router and (of course) for the direct to laptop connection. I didn't even get a link light though which is why I am concerned that the problem is lower level than IP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    Can I just confirm something. 

     

    The RPi is connected to a cable (that works) and the cable is then connected to a socket on your router (that you know works).

     

    Correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    Yes. The RPi has been connected using 2 cables (that both work) to each of the 4 ports on the router (that all work). At no time did the raspberry pi show any lights or successfully ping anything (using dhcp or static)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    It sounds you have network problems.  I can only see three possible issues:

     

    1. Your router is not giving out IP addresses for so reason / does not like the RPi image.

     

    2. One of the files that you modified is not correct (a fresh image would fix this)

     

    3. Your RPi is not functioning correctly (but I don't think this is the problem)

     

     

    Try re-imaging your SD card and start-up with the cable ethernet plugged in.  The other casue could be your power supply. Check: http://elinux.org/RPi_VerifiedPeripherals#Power_adapters to see if you have a problem power supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Some things to try:

     

    1. type in: ip link set up dev eth0 if this gets some of the remaining three lights to come on, then it's possibly a software issue.

     

    2. ip link ls eth0 gives output similar to the following examples:

     

    2: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc pfifo_fast state UP mode DEFAULT qlen 1000

        link/ether e1:14:51:ff:17:22 brd ff:ff:ff:ff:ff:ff

     

    The important parts are the UP which tells you that the interface has been enabled and LOWER_UP which tells you that there's an active link to the device at the other end of the cable - you should have lights in this case.

     

     

    2: eth0: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc pfifo_fast state DOWN mode DEFAULT qlen 1000

        link/ether e1:14:51:ff:17:22 brd ff:ff:ff:ff:ff:ff

     

    Here, the interface is enabled (UP), but NO-CARRIER tells us the link cannot be established to the other end.

     

     

    2: eth0: <BROADCAST,MULTICAST> mtu 1500 qdisc pfifo_fast state DOWN mode DEFAULT qlen 1000

        link/ether e1:14:51:ff:17:22 brd ff:ff:ff:ff:ff:ff

     

    In this last example, where there's no UP, then the interface is DOWN and will not be attempting to bring the low level link up. Try ip link set up dev eth0 and see what happens.

     

     

    One possible, but unlikely, reason for a NO-CARRIER indication could be that the device at the other end of the cable is configured to only connect at 1gigabit. The Pi can only manage 10/100 so this would cause it not to work. Alternatively, if 'autonegotiation' has been disabled on the switch/router then the connection will not be made unless you force the settings on the Pi to match.

     

    Another good command to debug this is ethtool eth0 you'll get something like this:

    Settings for eth0:

            Supported ports: [ TP MII ]

            Supported link modes:   10baseT/Half 10baseT/Full

                                    100baseT/Half 100baseT/Full

            Supported pause frame use: No

            Supports auto-negotiation: Yes

            Advertised link modes:  10baseT/Half 10baseT/Full

                                    100baseT/Half 100baseT/Full

            Advertised pause frame use: Symmetric Receive-only

            Advertised auto-negotiation: Yes

            Link partner advertised link modes:  10baseT/Half 10baseT/Full

                                                 100baseT/Half 100baseT/Full

            Link partner advertised pause frame use: Symmetric

            Link partner advertised auto-negotiation: Yes

            Speed: 100Mb/s

            Duplex: Full

            Port: MII

            PHYAD: 1

            Transceiver: internal

            Auto-negotiation: on

            Current message level: 0x00000007 (7)

                                   drv probe link

            Link detected: yes

     

    Interesting stuff highlighted.  If there's no matching modes between Advertised link modes & Link partner advertised link modes then you'll have a problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks everyone for your help and particularly selsinork for your comprehensive list of tests.

     

    From memory I had eth0: <NO-CARRIER,BROADCAST,MULTICAST,UP> but I'll need to go back and check.

     

    I tried plugging the pi into another two computers with a third ethernet cable last night and used a 5v1a phone charger to try charging the pi with no luck.

     

    I glanced briefly at the connectors and saw nothing obvious but I wouldn't really know what I was looking for...