Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry PI power socket
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 709 subscribers
  • Views 1615 views
  • Users 0 members are here
Related

Raspberry PI power socket

maudil
maudil over 14 years ago

Hi all,

I've recently received my Raspberry PI B type board and I'm starting working on it.

Since I'd like to use it in some embedded application I'm wandering if it is possible to power it through a different connector than the micro USB one.

Is the 5V present on GPIO connector usable to power the unit?

I tried to have a look at the schematics but, unfortunatelly, the supplied link does not work.

 

Thank you in advance

 

Bye

Maurizio

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 14 years ago

    You're in luck, Maurizio.  The Pi can be powered through pins 2 and 4 on the P1 header, and this provides better voltage regulation than powering through the micro-USB socket with its F3 polyfuse.  Be careful though, since it's so easy to damage the hardware by accidentally touching adjacent 3.3V pins.

     

    You're right that Element 14's link to its own copy of the schematic listed under Design Elements->Schematic on its main Raspberry Pi page is broken --

     

    http://www.element14.com/community/docs/DOC-42993/l/raspberry-pi-single-board-computer?ICID=rasp_group

     

    To Element 14 Support --- a website fix needed here please when you can.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago

    You're in luck, Maurizio.  The Pi can be powered through pins 2 and 4 on the P1 header, and this provides better voltage regulation than powering through the micro-USB socket with its F3 polyfuse.  Be careful though, since it's so easy to damage the hardware by accidentally touching adjacent 3.3V pins.

     

    You're right that Element 14's link to its own copy of the schematic listed under Design Elements->Schematic on its main Raspberry Pi page is broken --

     

    http://www.element14.com/community/docs/DOC-42993/l/raspberry-pi-single-board-computer?ICID=rasp_group

     

    To Element 14 Support --- a website fix needed here please when you can.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    2 & 4 are both 5v currently, but only 2 is officially documented (if you can find Eben's blog post and even that changed a couple of days later), GND goes to pin 6.

     

    I'm using these SSW-115-01-T-DSSW-115-01-T-D with various things soldered on to make it less likely to short flying leads to some other pin.

     

    Something like MULTICOMP - 2226A-03 - CRIMP HOUSING, 1 ROW, 3 WAY MULTICOMP - 2226A-03 - CRIMP HOUSING, 1 ROW, 3 WAY is also suitable, problem is the required crimp tool costs more than the Pi !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    there is a working link to the schematic at the end of the first post

    in this thread:

     

    http://www.element14.com/community/thread/19261?tstart=0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustiniadmin
    fustiniadmin over 14 years ago in reply to morgaine

    You're right that Element 14's link to its own copy of the schematic listed under Design Elements->Schematic on its main Raspberry Pi page is broken --

     

    http://www.element14.com/community/docs/DOC-42993/l/raspberry-pi-single-board-computer?ICID=rasp_group

    Hi, are you still seeing a broken link?   The schematic link takes me to:

     

    http://www.element14.com/community/solutions/5952/l/raspberry-pi-schematic-for-raspberry-pi-model-b-board

     

    where this PDF is available for download, Raspberry-Pi-Schematics-R1.0.pdf , which I'm able to download and view ok.

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to fustiniadmin

    Yep, the chain of links works now, good job. image