I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
Just received via email from element14:
We are thrilled to announce the launch of a new 512MB board version of the Raspberry Pi. Now packed with double the RAM, the new Pi is suited to multimedia, high-memory and mobile applications, including a future version of an Android 4.0 operating system. Order yours here! We're really looking forward to hearing what plans you have for your new Pi. So, we've launched a blogging competition asking what you're going to do with double the memory. Join in and submit an entry on the RPi forum and you could win an awesome prize!
Hello Jamodio. . .
I'm happy to report I've just purchased the new Raspi, model B with 512Mb. Nice that it was $35 (+6 to ship) from the Newark site. Receipt said "1 available to ship today". Great way to start a Monday. . .now if only the line on my order history for the Gertboard would say SHIPPED, we'd have a perfect day!
Best
Peg
I suspect that, currently, over-exuberance is trumping stock levels to fulfill the level of enthusiasm.
Well it seems that newark have/had some boards in stock, got confirmation that it was shipped via UPS, expected delivery on 10/17.
Hi,
I will pass your message to Newark Customer Service so they confirm with you delivery date.
Thanks,
Farnell element14 Raspberry Pi Customer Support
Hmm - will have to wait and see what turns up in your shipping package to be sure. I ordered my Pi from element14 New Zealand - looks like it was fulfilled from Element14 Australia.
When i noticed they had a couple of thousand turn up in stock, i called (yesterday) to ask if they were the new improved spec models - and was assured yes i would revieve one of the newer models.
It turns up by courier today, and disappointed to see that despite being a newer board manufactured in the UK, it seems to have a 256meg chip fitted.
I guess i ordered the 256meg version, so i shouldnt be so disappointed - but actually am rather gutted as i want it to run XBMC - which would certainly benefit from the extra memory...
guess i should just have cancelled and re-ordered. Grrrr.
Hi Pete
Looking at your post I would also think you should have received a 512MB unit
You may have doen this but can you run the following command and check the code number that the board returnsd
cat/proc/cpuinfo
If you’re running revision 1.0 you will see code numbers 2 or 3
If you're running revision 2.0, 256MB you will see code numbers 4 or 6.
If you are running the Raspberry new Pi Model B (512MB) Revision 2.0 you will see code numbers 13 or 14
Thanks
Mike
Mike Buffham wrote:
Hi Pete
Looking at your post I would also think you should have received a 512MB unit
You may have doen this but can you run the following command and check the code number that the board returnsd
cat/proc/cpuinfo
If you’re running revision 1.0 you will see code numbers 2 or 3
If you're running revision 2.0, 256MB you will see code numbers 4 or 6.
If you are running the Raspberry new Pi Model B (512MB) Revision 2.0 you will see code numbers 13 or 14
Thanks
Mike
Will there be a 256 rev2 with code 5? or has this been abandoned?
The Rev 2.0 board just arrived, Samsung part number is K4P4G324EB-AGC1, board says made in UK, no indication on the box about version or memory size. FPC connectors look cheaper than the ones on previous boards.
Good thing, the LDOs are from ON Semi and not from cheap-o-china.
My 512Mb Pi arrived yesterday, will only have a chance to play at the weekend. Will try touching the usb controller and see what happens.
Heck, I like to live dangerously, might touch it with my tongue and see what happens !
Fergus Byrne wrote:
Just noticed on my Rev2 512mb that if you touch the USB controller chip, it shorts out the USB circuit. Is this a flaw? Or is it just it should not be touched?
Sounds like a flaw. As long as you've touched ground somewhere on the board (e.g., the USB or Ethernet shell) before lightly touching a chip package, it shouldn't have any effect other than perhaps a burned finger-tip. If the USB chip fails if you touch it, IMO the most likely cause is a hair-line break in a PCB trace so that if the board flexes the trace opens. It could also be an iffy solder joint, though those are more likely to open when you're not pressing down on the chip.
You could have an effect if you touch the LAN9512 crystal oscillator pins. Also check the solder joints on crystal X1 which is on the back side of the PCB near the LAN9512. Crystals are sensitive to being touched, especially if not well soldered.
Can you be more specific about "shorts out the USB circuit"? What's shorting to what, or are you just saying USB stops working, and if so, for how long?
Oh, and what's under the RasPi? If it's on a mildly conductive surface pressing down could cause mischief.
Fergus Byrne wrote:
Just noticed on my Rev2 512mb that if you touch the USB controller chip, it shorts out the USB circuit. Is this a flaw? Or is it just it should not be touched?
I wonder if there's something squirrely with latest RasPis. There's someone with a similar unexplained USB/Ethernet problem at the RasPi forum. I wonder when the rev 2 schematic is going to get published? Gerbers would be nice too.
John Beetem wrote:
Fergus Byrne wrote:
Just noticed on my Rev2 512mb that if you touch the USB controller chip, it shorts out the USB circuit. Is this a flaw? Or is it just it should not be touched?
I wonder if there's something squirrely with latest RasPis. There's someone with a similar unexplained USB/Ethernet problem at the RasPi forum. I wonder when the rev 2 schematic is going to get published? Gerbers would be nice too.
Same bloke I'm reckoning.
Sorry for double posting. I get different replies from both forums.
Just had some time last night to connect the new Rev 2.0/512MB, didn't find any issues with the USB/Ethernet controller,
didn't try with my tongue but even putting the fingers on the bottom side where the crystal and other components are didn't
produce any effect.
I hope sooner or later they decide to release the schematics for the new board.
One thing that look strange is that when the original images for the 256MB with different memory splits (besides am240)
have the same file size, only two images have the same file size.
-J
I was on the list to be notified when I could order the new 512 RPi, got an email about 2 hours ago to this affect with link to the site, however the site shows all I can do is get on the wait list (which I already was) or call an 1-888 number to make order, but the 1-888 number doesn't seem to match up to anything on the site. Probably legit, but a bad way to do business. 'Here call this number you can't verify and give us your credit card number for something the site says we don't have!'