I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
Just received via email from element14:
We are thrilled to announce the launch of a new 512MB board version of the Raspberry Pi. Now packed with double the RAM, the new Pi is suited to multimedia, high-memory and mobile applications, including a future version of an Android 4.0 operating system. Order yours here! We're really looking forward to hearing what plans you have for your new Pi. So, we've launched a blogging competition asking what you're going to do with double the memory. Join in and submit an entry on the RPi forum and you could win an awesome prize!
Hello Jamodio. . .
I'm happy to report I've just purchased the new Raspi, model B with 512Mb. Nice that it was $35 (+6 to ship) from the Newark site. Receipt said "1 available to ship today". Great way to start a Monday. . .now if only the line on my order history for the Gertboard would say SHIPPED, we'd have a perfect day!
Best
Peg
Hmm - will have to wait and see what turns up in your shipping package to be sure. I ordered my Pi from element14 New Zealand - looks like it was fulfilled from Element14 Australia.
When i noticed they had a couple of thousand turn up in stock, i called (yesterday) to ask if they were the new improved spec models - and was assured yes i would revieve one of the newer models.
It turns up by courier today, and disappointed to see that despite being a newer board manufactured in the UK, it seems to have a 256meg chip fitted.
I guess i ordered the 256meg version, so i shouldnt be so disappointed - but actually am rather gutted as i want it to run XBMC - which would certainly benefit from the extra memory...
guess i should just have cancelled and re-ordered. Grrrr.
Hi Pete
Looking at your post I would also think you should have received a 512MB unit
You may have doen this but can you run the following command and check the code number that the board returnsd
cat/proc/cpuinfo
If you’re running revision 1.0 you will see code numbers 2 or 3
If you're running revision 2.0, 256MB you will see code numbers 4 or 6.
If you are running the Raspberry new Pi Model B (512MB) Revision 2.0 you will see code numbers 13 or 14
Thanks
Mike
Mike Buffham wrote:
Hi Pete
Looking at your post I would also think you should have received a 512MB unit
You may have doen this but can you run the following command and check the code number that the board returnsd
cat/proc/cpuinfo
If you’re running revision 1.0 you will see code numbers 2 or 3
If you're running revision 2.0, 256MB you will see code numbers 4 or 6.
If you are running the Raspberry new Pi Model B (512MB) Revision 2.0 you will see code numbers 13 or 14
Thanks
Mike
Will there be a 256 rev2 with code 5? or has this been abandoned?
The Rev 2.0 board just arrived, Samsung part number is K4P4G324EB-AGC1, board says made in UK, no indication on the box about version or memory size. FPC connectors look cheaper than the ones on previous boards.
Good thing, the LDOs are from ON Semi and not from cheap-o-china.
My 512Mb Pi arrived yesterday, will only have a chance to play at the weekend. Will try touching the usb controller and see what happens.
Heck, I like to live dangerously, might touch it with my tongue and see what happens !