Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Peripheral Devices That I have but Don't know how to use. Help Please.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 710 subscribers
  • Views 4408 views
  • Users 0 members are here
  • raspberry
  • of
  • people
  • the
  • pi
  • gpio
  • touch;
  • useful
  • rasp
  • what
  • display;
  • screen;
  • but
  • above
  • could
  • raspberry_pi
  • raspi;
  • used
  • see
  • thought
  • is
  • know
  • don't
  • rpi
  • with
  • be
  • thought.;
  • if
  • any
  • inch;
  • would
  • i
  • 4
  • pi;
Related

Peripheral Devices That I have but Don't know how to use. Help Please.

wallarug
wallarug over 13 years ago

I took apart a TomTom GPS the other day and stole the 4 Inch Display out of it along with a GPS module and SD card reader.

 

Specs of Dispaly:

     Touch Screen

     480x272 resolution

     NAME: LTE400WQ-E01-005

      50 pin connector (see below)

image

 

Can someone help me find a way that I can use this with my Raspberry Pi?  If someone could please find a datasheet first, that would be much appreciated.

 

Specs of GPS module are not know except for the NAME: Valencia ANT PCB REV:3P1 (see below)

image

Specs of SD card Reader - only pictures. (see below)

Connector:

image

Reader:

image

 

I don't know if any of the above could be used / is useful with the Raspberry Pi but I thought I would see what people thought.

 

The one I really would Like to work with the Raspberry Pi is the touch display.  this would make my RPi somewhat portable and would be cool to have.

 

If the display can work with GPIO, then it would be nice to use with a rev 2 board with mounting holes.

 

Also, If the display works, then I thnk you can by these 4 Inch Touch Displays online from about $30 -$50 Dollars.

 

Thanks for any responces, they will be much apreicated.

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 13 years ago

    Ok,

     

    I have done a bit of research into the touch screen display that I mentioned at the start of this topic, and found this: 

     

    http://beyondinfinite.com/lcd/Library/Samsung/LTE400WQ-F02.pdf

     

    This is the data sheet for the LTE400WQ-F02.  It looks exactly the same as the connector on my one though...  I did a bit of a dumby check.  The GNDs and DNC and VCC all match up which is pritty good.

     

    Can anyone suggest a converter (either home made or other wise) that can turn this into a touch screen that can be written to by serial/UART/SPI  ??

     

    Right now, It seems I would have to connect all the R0 - G7 which I cannot do on the raspberry pi (not enough connectors).

     

    Let me know what you think.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 13 years ago

    Ok,

     

    I have done a bit of research into the touch screen display that I mentioned at the start of this topic, and found this: 

     

    http://beyondinfinite.com/lcd/Library/Samsung/LTE400WQ-F02.pdf

     

    This is the data sheet for the LTE400WQ-F02.  It looks exactly the same as the connector on my one though...  I did a bit of a dumby check.  The GNDs and DNC and VCC all match up which is pritty good.

     

    Can anyone suggest a converter (either home made or other wise) that can turn this into a touch screen that can be written to by serial/UART/SPI  ??

     

    Right now, It seems I would have to connect all the R0 - G7 which I cannot do on the raspberry pi (not enough connectors).

     

    Let me know what you think.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 13 years ago in reply to wallarug

    Hi Cian,

    There are a few ways to use the display, but sadly all are non-trivial or complicated ; -(

    Most of these types of display require an off-board device for refreshing the display repeatedly with

    the right data. Epson make some SMD devices to interface to some LCD displays, but I'm not sure

    if they have a device available in individual quantities to handle this sized display.

    Also, most of these types of display have some slight difference in timing or logic levels from one

    part number to another, so some of Epson's controllers have registers that you can set to interface correctly.

    Another way is to use your own logic and external RAM, and this could be implemented with a

    CPLD and RAM (or FPGA), but it may be a lot of work but rewarding. Also, it is possible to dedicate

    some high-speed microcontroller to this, but it will consume lots of logic pins. It is inefficient, but may be the easiest

    way. Finally, you could also get ideas from here. It is slow loading for me, not sure why, but I think it

    uses one of these methods described.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to shabaz

    Thanks for reply.

     

    Just had a look at the page linked above...

     

    unfortunatly, the display I have has a 50pin connector not a 40 pin... image

     

    I will keep looking into your other suggestions.