Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Issue with graphic output:  stuck with : HPD high|DVI mode|1280x720 @ 60Hz
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 707 subscribers
  • Views 890 views
  • Users 0 members are here
  • graphic
  • raspberry_pi
  • raspberrypi
Related

Issue with graphic output:  stuck with : HPD high|DVI mode|1280x720 @ 60Hz

e14 Contributor
e14 Contributor over 13 years ago

Issue with graphic output
Firstly, I'd like to say that I've waiting Raspberry impatiently and I
not disapointed. This project is really interresting.
But I have an graphic issue (already two months) : I spent lots of time on forums and try
all the options I can in config.txt but I still have a trouble using
the graphic output.
I'm stuck with : state: HPD high|DVI mode|HDCP off|composite off
(0x120016), 1280x720 @ 60Hz, progressive
I tried several screens but always the same problem.
I had the right configuration on other sdcard, but since the problem
occurs, it remains the same. I tried every new releases of Raspbian, etc.
Before the problem occurs, everything was ok using 'overscan_*'
options, but the first boot itself ; I had no screen but sdcard was on
activity.
Now it is the opposite. I had a screen during the first boot but I got
the wrong resolution which is always 1280x720p.
It seems that the problem appears just after a a try of 'Preferences
-- Paramètres de l'écran' which failed and a reboot of the RaspBerry.
When I did :
tvservice -m CEA
Group CEA has 0 modes:
tvservice -m DMT
Group DMT has 0 modes:
No result when trying to fetch the  edid of screen:
tvservice -d edid
Written 0 bytes to edid
With 'framebuffer_*' options and fbset I get broken pixels.
Please help me ! Is it possible the graphic hardware has trouble ?
I read other screen isues but it wasn't the same problem. For them it
was always possible to get edid or a least the CEA/DMT supported
modes.
Best regards.
Ivain.K

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Toujours le même problème et ce alors que j'ai passé des dizaines d'heures à en touver la cquse Ça ne doit pas être Soft mais plutôt hard au niveau du 'bios vidéo...'

    Je crois que je vais le renvoyer en garantie en janvier. J'en ai marre de tester toutes les options du config.txt sans succès, de réinstaller la Raspbian à chaque version. J'aimerai bien l'utiliser normalement,

     

    I.K

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Avez-vous essayé config.txt avec "hdmi_safe=1"?  Ça doit faire résolution VGA = 640x480.  Si la résolution reste 1280x720 je me demande si config.txt est dans la SDcard partition FAT où le BCM2835 le cherche.  Est config.txt visible avec Microsoft Windows?  Le Wiki RasPi a des conseils pour éditer config.txt ici.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to johnbeetem

    Try reading this post and following the instructions there:

    http://www.element14.com/community/thread/18205?tstart=0

     

    Essayez de lire ce post et en suivant les instructions là-bas:

    http://www.element14.com/community/thread/18205?tstart=0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Bonjour John,

     

    Je vous remercie de votre réponse, mais en effet j'avais déjà essayé cette

    option.

    J'ai bien la première partition qui est montée dans /boot qui est de type

    W95 FAT32, le fichier de config étant bien /boot/config.txt. J'ai même

    booté sous windows7 pour rajouter l'option

    "hdmi_safe=1" <http://elinux.org/RPi_config.txt#Video_mode_options>, je

    n'ai pas touché aux autres.

    Si je fais un tvservice -s j'ai bien un mode de 1280x720 @ 60Hz alors que

    je devrais être en 640 x 480 et fbset done un mode de "1184x624".

    Comme je l'ai écrit j'avais bien l'affichage qui s'adaptait automatiquement

    (ça a bien marché pdt 5 ou 10 boot je crois) puis c'est bloqué depuis sans

    aucune modification du config.txt. J'ai vraiment l'impression qu'il y a un

    pb hard.

     

    Cordialement,

     

    Ivain.

    2012/12/19 johnbeetem <messages@element14.com>

     

    **

        image: element14<http://www.element-14.com?CMP=e14notificationemail_header> Re: Issue with graphic output: stuck with : HPD high|DVI mode|1280x720 @

    60Hz  created by John Beetem<http://www.element14.com/community/people/johnbeetem>in

    Raspberry Pi - View the full discussion<http://www.element14.com/community/message/66209#66209/l/re-issue-with-graphic-output-stuck-with-hpd-highdvi-mode1280x720-60hz>

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Très bizarre.  Avez-vous essayé un autre SDcard?  Il y a des classes de SDcard que le RasPi n'aime pas.  C'est guère probable -- si le SoC ne peut pas lire config.txt, c'est improbable qu'il puisse lire les plus grands fichiers sans erreur.  Mais c'est quelque choise à essayer si vous ne l'avez pas déjà fait.

     

    Pouvez-vous nous montrer le contenu de config.txt?  Peut-être quelqu'un ici peut voir une erreur.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Honnêtement le config.txt est bien pris en compte par le SOC car les

    options comme 'l'overscan' font leur effet. J'avais plusieurs carte SD qui

    fonctionnaient très bien, le Raspberry-Pi trouvait très bien la résolution

    d'un 19" et d'un 24" tous deux branchés en DVI, aucun soucis après

    ajustement de l'overscan, et suite au problème ces mêmes cartes étaient

    elles aussi bloquées à une résolution de 1280x720p @60Hz. Par la suite j'ai

    réinstallé les dernières RaspBian sur ces cartes. Ce qui est bizarre c'est

    que le SOC ne me donne plus l'EDID de ces écrans. Ces mêmes écrans n'ont

    aucun pb avec d'autres PC. Sous G/Debian j'arrive bien à récupérer leur

    EDID par exemple. Le tvservice -m DMT/CEA ne donne pas de mode disponible

    (peut-être car se sont des moniteurs et non des TV) j'ai forcé le

    hdmi_group et hdmi_mode mais sans succès. La commande 'hdmi_drive=2' n'a

    pas donné de résultat car elle force un mode de l'HDMI pour TV.

     

    Pour répondre à votre question concernant le config.txt, j'ai essayé avec

    un fichier vide. L'option hdmi_safe n'a pas d’incidence. Actuellement il

    n'y a que 'overscan=1' dans mon fichier de conf et le turbo dynamique placé

    avec les options par défaut de raspi-config.

     

    Voilà, c'est vraiment très bizarre... J'espère que je trouverai une

    solution car je vais bientôt investir dans une TV full HD est là je vais

    voir la différence si je reste bloqué en 1280x720p....

    En tous cas merci pour les réponses.

     

    Cordialement,

     

    Ivain.

     

    2012/12/19 johnbeetem <messages@element14.com>

     

    **

        image: element14<http://www.element-14.com?CMP=e14notificationemail_header> Re: Issue with graphic output: stuck with : HPD high|DVI mode|1280x720 @

    60Hz  created by John Beetem<http://www.element14.com/community/people/johnbeetem>in

    Raspberry Pi - View the full discussion<http://www.element14.com/community/message/66233#66233/l/re-issue-with-graphic-output-stuck-with-hpd-highdvi-mode1280x720-60hz>

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Bonsoir,

     

    J'ai profité d'un séjour chez mes parents pour confirmer avec une TV, le problème que j'ai avec mes deux moniteurs. Donc j'ai connecté le Raspberry-Pi à une TV Sony KDL-40V4000 (full HD 1080p), et j'ai le même problème. Impossible de récupérer les modes CEA (ni DMT mais ça c'est plus normal pr une TV), impossible de 'dumper' l'EDID, sans configuration dans le config.txt ça ne marche pas, je suis en 720p. J'ai rajouté l'overscan qui est bien pris en compte. Puis j'ai forcé les modes CEA (en utilisant la réf. http://elinux.org/RPiconfig) mais je suis toujours en 720p (fbset et tvservice).

    Voici le contenu de mon dernier /boot/config.txt :

         disable_overscan=0

         hdmi_drive=2

         hdmi_group=1

         hdmi_mode=16

         overscan_left=-18

         overscan_right=-15

         overscan_top=-30

         overscan_bottom=-30

    Voilà...

    Je ne sais plus quoi essayer...

    Bonnes fêtes à tous.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Ivain Kesteloot a écrit:

     

    Bonsoir,

     

    Impossible de récupérer les modes CEA (ni DMT mais ça c'est plus normal pr une TV), impossible de 'dumper' l'EDID, sans configuration dans le config.txt ça ne marche pas, je suis en 720p.

    Salut,

     

    Il me semble que vous avez essayé tout ce qu'on peut avec le logiciel.  Peut-être c'est vraiment un problème du matériel.  Si c'est impossible de récupérer les modes CEA ou l'EDID, peut-être le signal HDMI_SCL ou HDMI_SDA est cassé à cause d'un défaut de soudure.   Il arrive q'une soudure faible peut casser après quelques heures d'opération.  Si c'est le cas le meilleur est de renvoyer le RasPi.

     

    C'est aussi possible que le câble HDMI est cassé.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Ivain Kesteloot a écrit:

     

    Bonsoir,

     

    Impossible de récupérer les modes CEA (ni DMT mais ça c'est plus normal pr une TV), impossible de 'dumper' l'EDID, sans configuration dans le config.txt ça ne marche pas, je suis en 720p.

    Salut,

     

    Il me semble que vous avez essayé tout ce qu'on peut avec le logiciel.  Peut-être c'est vraiment un problème du matériel.  Si c'est impossible de récupérer les modes CEA ou l'EDID, peut-être le signal HDMI_SCL ou HDMI_SDA est cassé à cause d'un défaut de soudure.   Il arrive q'une soudure faible peut casser après quelques heures d'opération.  Si c'est le cas le meilleur est de renvoyer le RasPi.

     

    C'est aussi possible que le câble HDMI est cassé.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Merci pour la réponse, je crois réellement que ça doit être ça vu que ça me

    l'a fait assez vite. J'ai essayé plusieurs câbles HDMI avec le même

    résultat. Je vais prendre contact avec le revendeur. Encore merci pour le

    temps passé.

    Ivain.

     

    2012/12/22 johnbeetem <messages@element14.com>

     

    **

        image: element14<http://www.element-14.com?CMP=e14notificationemail_header> Re: Issue with graphic output: stuck with : HPD high|DVI mode|1280x720 @

    60Hz  created by John Beetem<http://www.element14.com/community/people/johnbeetem>in

    Raspberry Pi - View the full discussion<http://www.element14.com/community/message/66348#66348/l/re-issue-with-graphic-output-stuck-with-hpd-highdvi-mode1280x720-60hz>