Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB or SD?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 676 subscribers
  • Views 723 views
  • Users 0 members are here
  • usb
  • learning
  • sd
  • downloading
Related

USB or SD?

Former Member
Former Member over 13 years ago

hi everyone, first post
i would like to run my pi as a linux, everywhere i look i'm being told to download onto an SD card but does anyone know if it would work if i download it straight to USB?

i always thought USB was faster than SD card

thanks in advance

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 13 years ago

    Yes you can run it off USB and yes USB is faster. But then you have a thumb drive sticking out the side of your Pi and taking up one of the USB slots. SD is seen as a more practicle option in this case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago

    RasPi initially boots from the SD card, but after that you should be able to put your file system elsewhere, e.g., a USB Flash drive or a USB hard disk.  I don't know how to do this personally, nor have I read first-hand reports from people doing this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 13 years ago

    Hello Andy,

     

    I think the following post may be helpful ?

     

    http://raspberrypi.org/phpBB3/viewtopic.php?f=63&t=5974

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to Former Member

    I'm getting a pair of these to test, it won't stick out.

     

    http://www.amazon.com/SanDisk-Cruzer-Flash-Drive-SDCZ33-016G-B35/dp/B005FYNSZA

     

    I'll let you know if they work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to jamodio

    The little USB drives arrived yesterday, just had a chance to test one of them (8GB) ...

    image

     

    As you can see it is very small and does not stick out too much.

     

    Here is what is the device info via lsusb

     

    Bus 001 Device 004: ID 0781:5571 SanDisk Corp.

    Device Descriptor:

      bLength                18

      bDescriptorType         1

      bcdUSB               2.00

      bDeviceClass            0 (Defined at Interface level)

      bDeviceSubClass         0

      bDeviceProtocol         0

      bMaxPacketSize0        64

      idVendor           0x0781 SanDisk Corp.

      idProduct          0x5571

      bcdDevice            1.26

      iManufacturer           1 SanDisk

      iProduct                2 Firebird USB Flash Drive

      iSerial                 3 4C532000011021100122

      bNumConfigurations      1

      Configuration Descriptor:

        bLength                 9

        bDescriptorType         2

        wTotalLength           32

        bNumInterfaces          1

        bConfigurationValue     1

        iConfiguration          0

        bmAttributes         0x80

          (Bus Powered)

        MaxPower              200mA

        Interface Descriptor:

          bLength                 9

          bDescriptorType         4

          bInterfaceNumber        0

          bAlternateSetting       0

          bNumEndpoints           2

          bInterfaceClass         8 Mass Storage

          bInterfaceSubClass      6 SCSI

          bInterfaceProtocol     80 Bulk-Only

          iInterface              0

          Endpoint Descriptor:

            bLength                 7

            bDescriptorType         5

            bEndpointAddress     0x81  EP 1 IN

            bmAttributes            2

              Transfer Type            Bulk

              Synch Type               None

              Usage Type               Data

            wMaxPacketSize     0x0200  1x 512 bytes

            bInterval               0

          Endpoint Descriptor:

            bLength                 7

            bDescriptorType         5

            bEndpointAddress     0x02  EP 2 OUT

            bmAttributes            2

              Transfer Type            Bulk

              Synch Type               None

              Usage Type               Data

            wMaxPacketSize     0x0200  1x 512 bytes

            bInterval               1

     

    No problems doing fdisk and creating an ext4 file system, I'll copy the root fs and see what happens ...

    I'll also test the 16GB version later.

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to jamodio

    Everthing seems to be working fine with the SanDisk USB drive (8GB) mounted as root and an old 256MB microSD card I used for just the boot partition.

     

    pete@raspi:~$ df

    Filesystem     1K-blocks    Used Available Use% Mounted on

    rootfs           7692968 1800124   5502060  25% /

    /dev/root        7692968 1800124   5502060  25% /

    devtmpfs           94484       0     94484   0% /dev

    tmpfs              18912     204     18708   2% /run

    tmpfs               5120       0      5120   0% /run/lock

    tmpfs              37800       0     37800   0% /run/shm

    /dev/mmcblk0p1     57288   16928     40360  30% /boot

     

    pete@raspi:~$ mount

    /dev/root on / type ext4 (rw,noatime,user_xattr,barrier=1,data=ordered)

    devtmpfs on /dev type devtmpfs (rw,relatime,size=94484k,nr_inodes=23621,mode=755)

    tmpfs on /run type tmpfs (rw,nosuid,noexec,relatime,size=18912k,mode=755)

    tmpfs on /run/lock type tmpfs (rw,nosuid,nodev,noexec,relatime,size=5120k)

    proc on /proc type proc (rw,nosuid,nodev,noexec,relatime)

    sysfs on /sys type sysfs (rw,nosuid,nodev,noexec,relatime)

    tmpfs on /run/shm type tmpfs (rw,nosuid,nodev,noexec,relatime,size=37800k)

    devpts on /dev/pts type devpts (rw,nosuid,noexec,relatime,gid=5,mode=620)

    /dev/mmcblk0p1 on /boot type vfat (rw,relatime,fmask=0022,dmask=0022,codepage=cp437,iocharset=ascii,shortname=mixed,errors=remount-ro)

     

    I'm expecting some of the microSD-SD adapters from Adafruit, with that one and the boot on the microSD almost nothing will be sticking out on the sides of the board (remember that I'm powering the Rpi directly from the P1 connector.)

     

    -J