Raspberry Pi Forum I've killed my gertboard ! ( and havent even finished it )
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 686 subscribers
  • Views 1438 views
  • Users 0 members are here
  • raspberry_pi
  • gertboard_kit
Related

I've killed my gertboard ! ( and havent even finished it )

Former Member
Former Member over 13 years ago

Well this is amusing.. Whilst attempting to solder one of the grains of sand in the kit,  I've managed to burn a couple of surfacemount pads on the board  image.  It's on one of the resistors,  I think I had the iron way to hot.

 

I was wondering ( hoping )  if anyone could advise on a way to fix it..

 

Thanks in advance.

 

 

Ash.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    image

     

    It's the R1 pads, both of them, rather than the view above,, I have two brown marks where the pads used to be.. 

     

    I have invested in a decent iron since..lol

     

    I'll try and pick up some of the AWG30 and have a go at a repair.

     

    https://community.element14.com/resized-image/__size/1200x900/__key/communityserver-discussions-components-files/91/3821.contentimage_5F00_175229.html

     

     

    Ash.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to Former Member

    According to the Gertboard schematic from rev 1.0 of the Gertboard User Manual, R1 and R2 are both pull-ups to +3.3V.  So I think you can just connect the labeled ends of R1 and R2 using a short non-insulated jumper wire.  For the other end of R1, you could scrape the solder resist off the diagonal trace and solder a short bare wire to the exposed trace.  You'll need a sharp X-acto knife or equivalent and stop scraping as soon as you see metal.  Then pre-tin the trace by heating it up with your soldering iron while melting solder onto the trace.  This makes it much easier to solder the actual wire to R1.  Be careful not to short to the copper fill beside the trace.

     

    You could also make the repair on the back side of the board, soldering one end of R1 to the through-hole pin it's supposed to pull up (J11 pin 4) and solder an insulated wire to +3.3V (J7 pin 2) from the other end of R1.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to johnbeetem

    Brilliant, thanks :-)  I dont feel quite so sad now, I was thinking of the bin for it ....

     

    I'll have a stab and post back..

     

    The new iron is much better, so hopefully I can finish the board without any further problems

     

     

    Ash>

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago in reply to johnbeetem

    Brilliant, thanks :-)  I dont feel quite so sad now, I was thinking of the bin for it ....

     

    I'll have a stab and post back..

     

    The new iron is much better, so hopefully I can finish the board without any further problems

     

     

    Ash>