Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 1080p on 23 inch monitor but text is blurry
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 707 subscribers
  • Views 2988 views
  • Users 0 members are here
  • raspberry_pi
  • rpi
Related

1080p on 23 inch monitor but text is blurry

e14 Contributor
e14 Contributor over 13 years ago

Dear raspberry pi gurus, recently I have just purchased a spanking new raspberry pi. I am tried to set the resolution to full hd which is 1080p 60 Hz. The config.txt that I had enabled was:

hdmi_drive = 2

hdmi_group = 1

hdmi_mode = 16 (1080p 60Hz)

hdmi_boost = 4

disable_overscan = 1

The monitor that I am using is 23 inch Dell Ultrasharp U2312HM. The pi is connected via HDMI to VGA converter (PI-VIEW) sold by element14. I have a steady 5V 1 amp PSU and I don't believe that the PSU is problematic.

 

I did the /opt/vc/bin/tvservice -s and it shows that my current resolution is 1920x1080, progressive. The only issue that I had is that the texts are blurry. Its kinda hard to read them, and is there any idea on how to make them sharp? I mean when I connect my PC via VGA mode, it still looks sharp on 1920x1080p. Please advice thank you 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hey guys thanks for the feedback. I have switched to DVI the text is crisp and clear. Thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hey guys thanks for the feedback. I have switched to DVI the text is crisp and clear. Thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Lewiste Johannes wrote:

     

    I have switched to DVI the text is crisp and clear. Thanks image

     

    Win ! image

     

    Not sure what it is about HDMI, but for every board / receiver / gadget I have, using an HDMI-DVI adapter into a DVI port reduces the hassle / breakage of one kind or another versus using an HDMI port directly.  My monitors are Dell too (the awesome 24" Dell 2408), which may or may not have a bearing on it.  As a result, I try to avoid plugging anything into the HDMI port except when it's the only way of getting audio out.

     

    Anyway, after telling the HDMI port to take a hike on most boards, all is happiness and light. image