Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pidora 18 (Raspberry Pi Fedora Remix) Released!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 706 subscribers
  • Views 5053 views
  • Users 0 members are here
  • raspberry_pi
Related

Pidora 18 (Raspberry Pi Fedora Remix) Released!

e14 Contributor
e14 Contributor over 13 years ago

Pidora 18 (Raspberry Pi Fedora Remix) Release

 

We're excited to announce the release of Pidora 18 --

an optimized Fedora Remix for the Raspberry Pi.

It is based on a brand new build of Fedora for the ARMv6

architecture with greater speed and includes packages

from the Fedora 18 package set.

 

* * *

 

There are some interesting new features we'd like to highlight:

* Almost all of the Fedora 18 package set available via yum

    (thousands of packages were built from the official Fedora

    repository and made available online)

* Compiled specifically to take advantage of the hardware already

    built into the Raspberry Pi

* Graphical firstboot configuration (with additional modules

    specifically made for the Raspberry Pi)

* Compact initial image size (for fast downloads) and auto-resize

    (for maximum storage afterwards)

* Auto swap creation available to allow for larger memory usage

* C, Python, & Perl programming languages available & included

    in the SD card image

* Initial release of headless mode can be used with setups

    lacking a monitor or display

* IP address information can be read over the speakers and

    flashed with the LED light

* For graphical operation, Gedit text editor can be used with

    plugins (python console, file manager, syntax highlighting)

    to serve as a mini-graphical IDE

* For console operation, easy-to-use text editors are included

    (nled, nano, vi) plus Midnight Commander for file management

* Includes libraries capable of supporting external hardware

    such as motors and robotics (via GPIO, I2C, SPI)

 

* * *

 

For further documentation, downloads, faq's, read-me's,

    how-to's, tutorials, or videos:

        http://pidora.ca/

 

* * *

 

Pidora 18 is a Fedora Remix -- a combination of software packages

from the Fedora Project with other software.

 

The Fedora Project is a global community of contributors working

to advance open source software. For more information or to join

the Fedora Project, see http://fedoraproject.org

 

Pidora is a project of the Seneca Centre for Development of Open

Technology (CDOT). To connect with CDOT, please visit

http://cdot.senecacollege.ca

 

The Raspberry Pi is a small, inexpensive computer board designed

to provoke curiosity and experimentation in programming and

computer electronics. For more information, see the Raspberry

Pi Foundation website at http://raspberrypi.org

 

* * *

 

 

- - -

The CDOT team at Seneca College

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Andrew,

       Thanks for showing up in this forum to make the announcement!

     

       Can you tell us if this release fixes the firmware problem that

    prevented the previous F18 release from working with Hynix memory?

    http://trac.proximity.on.ca/projects/rpfr/ticket/161

    https://fedorahosted.org/arm/ticket/65

     

      Will there be release notes showing what problem reports have been closed?

     

       Can you tell us if there are any plans to maintain this release,

    unlike the F14, F17, and F18 releases?

     

       Can you tell us if there are any plans to consolidate your two

    bug tracking systems into a single system (and remove the spam)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    The current firmware we are using is Version 20130415git1c339b1, this is the firmware that was last committed on May 14th.

     

    More information will be posted on pidora.ca or the pidora wiki when available. We will be maintaining this release.

     

    Bug tracking should be done with, as stated by the pidora wiki: http://trac.proximity.on.ca/projects/rpfr/

     

    The current process for tracking bugs will be updated in the wiki: http://zenit.senecac.on.ca/wiki/index.php/Pidora_18_Bug_Tracking

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       I looked over the release material, and was distressed not to find any release notes

    saying which problem reports were fixed.  If there have been improvements in speed,

    I don't see any benchmarks to demonstrate that, either in comparison to the prior

    soft-float F18 or to the competing Raspian hard-float.

     

      I can't even find Pidora mentioned with the other releases at:

    http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/

     

    The F18 soft-float did have release notes, at:

    http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/18/images/RaspberryPi-Fedora-Remix-18-Release-Notes.txt

    but with sloppy mistakes:

      "Model A has been redesigned to have 512Mb RAM"

    but this should say 256, not 512, and MB, not Mb.

       "The Raspberry Pi Fedora Remix 17 will be the second version of the Remix released."

    but this should say 18, not 17, and third version, not second.

        "firmware version: raspberrypi-firmware-20120727git0d88fba-1"

    I don't really think it's quite that old.  I think it's dated Nov 23, 2012,

    rather than Jul 27, 2012.

       3 fixed problems are listed, but without problem tracking numbers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       Are you maintaining two separate wiki's now?

        

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix

    http://zenit.senecac.on.ca/wiki/index.php/Pidora

     

    There is a lot of obsolete information in the first wiki, and even some

    in the second, such as:

     

    "The Remix was produced at the Seneca Centre for Development of Open Technology, which hosts the Fedora ARM build system."

    I believe the Fedora ARM build system is hosted now in Phoenix, AZ, not Seneca.

     

    "For suggestions on packages to meet particular needs and which run well on the Raspberry Pi, see Raspberry Pi Fedora Remix 14 - Suggested Packages."

    I believe this Remix 14 link is no longer specifically applicable, since C is

    included now with Pidora.

     

    The FAQ at

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_FAQ#Why_is_the_Remix_slow.3F

    currently says:

     

    "The GUI in particular is slow, because the 2D graphics (the X Window System) are not yet connected to the 3D graphics processing unit on the SOC."

     

    Similarly, the Educational Pilot currently says:

    "At this time, regular 2D graphics do not use the 3D accelerator built into the Pi. Therefore, the regular graphical user interface is somewhat slow. The 2D graphics will be hooked up to the 3D accelerator at some point in the future."

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Educational_Pilot

     

    Are you still trying to accelerate X Windows using the 3D GPU? 

    Or have you given up on that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    >Are you maintaining two separate wiki's now?

    The Raspberry Pi Fedora Remix wiki is related to the soft-float version, while the pidora wiki is related to our new release.

     

    Checking out some of the errors you pointed out.

     

    Related to making windows faster using the GPU, you can check out http://en.wikipedia.org/wiki/Wayland_(display_server_protocol). I believe they have released support for the raspberry pi as well.

     

    Just to note, some stuff will be fixed and cleaned up regarding the wiki and other materials.

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       What are your plans with regard to the kernel?

     

    The kernel version is said to be 3.6.11.

    Do you have plans for 3.8.x?

     

    Do you know what is the date of the latest patch to 3.6.11

    that is included? 

    Does it include the recent USB fixes for keyboards

    missing and repeating keys?

     

    The wiki at

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_FAQ#What_are_the_Future_Plans_for_the_Raspberry_Pi_Fedora_Remix.3F

    currently says:

     

    "The number of packages in the Raspberry Pi-specific repositories is expected to diminish over time -- by the time that Fedora 19 is released (May 2012), the Raspberry Pi repositories should hopefully contain mot much more than the VideoCore libraries and headers. (If these were ever to become licensed these under an OSI-approved license then the need for a Remix will be eliminated, and the Raspberry Pi could be directly supported as a Fedora target)."

     

    Aside from the mistake in the date, May 2012 should be May 2013 (or later),

    has the number of Pi-specific packages diminished over time as expected?

    Do you still expect F19 to contain "mot [sic] much more than VideoCore libraries

    and headers"?

     

    With the opensourcing of the all the ARM-based libraries and headers,

    is there still a need for a Remix?

     

    The same wiki section also says:

     

    "The future of the Remix is closely tied to the plans of the Fedora ARM project. By the release of Fedora 20 in November 2013, the ARM architecture will hopefully be promoted to Primary Architecture status, meaning that the ARM release will be done in lock-step with the x86 PC release."

     

    How have the plans for the F19 RPi Remix been affected by Fedora ARM dropping

    support for pre-v7 versions of ARM?

    Are you still expecting Fedora 20 to include RPi as a primary architecture?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    > I looked over the release material, and was distressed not to find any release notes saying which problem reports were fixed. 

    Release notes can now be found: http://pidora.ca/pidora/releases/18/release-notes.txt or at http://pidora.ca/

     

    >If there have been improvements in speed,

     

    There are improvements to speed.

     

    >I don't see any benchmarks to demonstrate that, either in comparison to the prior

    >soft-float F18 or to the competing Raspian hard-float.

     

    Hopefully some will be up soon.

     

    > I can't even find Pidora mentioned with the other releases at:

    > http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/

     

    Should not be there. Should be found at http://pidora.ca/

     

    >The F18 soft-float did have release notes, at:

    >http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/18/images/RaspberryPi-Fedora-Remix-18-Release->Notes.txt

    >but with sloppy mistakes:

    >  "Model A has been redesigned to have 512Mb RAM"

    >but this should say 256, not 512, and MB, not Mb.

    >  "The Raspberry Pi Fedora Remix 17 will be the second version of the Remix released."

    >but this should say 18, not 17, and third version, not second.

    >   "firmware version: raspberrypi-firmware-20120727git0d88fba-1"

    >I don't really think it's quite that old.  I think it's dated Nov 23, 2012,

    >rather than Jul 27, 2012.

    >   3 fixed problems are listed, but without problem tracking numbers.

     

    Fixed.

     

    The Raspberry Pi Fedora Remix and Pidora are very different in a lot of ways. A lot has changed between them, these are noted in the release annoucements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       Yay, we're making some progress!

     

    You say

    >> I can't even find Pidora mentioned with the other releases at:

    >> http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/ Should not be there.

    >Should be found at http://pidora.ca/

     

    This isn't a big deal, but I don't see why Pidora should have less

    visibility than the other Fedora RPi Remixes.

     

    You say the F18 soft-float release notes are fixed at:

    http://scotland.proximity.on.ca/raspberrypi/raspberrypi-fedora-remix/18/images/RaspberryPi-Fedora-Remix-18-Release-Notes.txt

    but I don't see any corrections.

     

    The new Pidora release notes at:

      http://pidora.ca/pidora/releases/18/release-notes.txt

    still fail to say what problem reports have been fixed.

    The problem most anxiously awaited is the Hynix RAM

    problem:

    http://trac.proximity.on.ca/projects/rpfr/ticket/161

    https://fedorahosted.org/arm/ticket/65

    but I don't see any mention of it.

     

    Please add the kernel patch date to the release notes if possible.

    Edited to add: believed to be 3.6.11-5.20130415git197d15b

    http://japan.proximity.on.ca/koji/buildinfo?buildID=40348

     

    "Model A has been redesigned to have 256Mb RAM"

    This should be MB (bytes not bits) as indicated above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

    You wrote:

    >Related to making windows faster using the GPU, you can check out http://en.wikipedia.org/wiki/Wayland_(display_server_protocol). I believe they have released support for the raspberry pi as well.

     

    This doesn't address my question.  I was specifically asking about X11 acceleration using the GPU,

    which I don't think Wayland does.  Wayland isn't a direct replacement for X11, so an X11 application

    would be running on top of X11 which would be running on top of Wayland, which would be no faster

    than before at drawing the contents of windows, although moving windows around on the display

    would presumably be faster.

     

    Can you give us a clear statement about whether work or planned work on X11 acceleration using the

    GPU as described in the wiki has been abandoned?

     

     

    Edited to add:

     

    Today we saw examples of unclear statements on X11 GPU acceleration plans from RPF moderator Davespice,

    who wrote:

    "(ottd is a bit slow though since it runs under the X desktop for which there are no GPU drivers for the Pi yet)"

    and

    "Not all software on the Pi makes use of the GPU though, for example the X desktop. This is all being drawn by the main ARM CPU which is why web browsing is so slow. It is hoped that X GPU drivers for the Pi will be released at some point whereupon the X desktop responsiveness will be as good as one would expect."

     

    on this thread:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=44663

     

     

    On October 24, 2012 we were told by Alex Bradbury:

    "There’s still the problem of optimising client-side rendering of each window. Simon Hall has done some interesting work on XOrg that we’re working with him to package up."

    http://www.raspberrypi.org/archives/2221#comment-34969

     

    But on May 24, 2013 Eben told us:

    "We’ve made the decision to bypass X completely."

    http://www.raspberrypi.org/archives/4053

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    >This isn't a big deal, but I don't see why Pidora should have less

    >visibility than the other Fedora RPi Remixes.

     

    The idea is that by using pidora.ca, it will get more visibility image

     

    >The new Pidora release notes at:

    > http://pidora.ca/pidora/releases/18/release-notes.txt

    >still fail to say what problem reports have been fixed.

    >The problem most anxiously awaited is the Hynix RAM

    >problem:

     

    We will be looking into what is left to get working.

     

    More information and corrections are still to come. A lot of your questions might also be better directed in IRC freenode #seneca, some of the arm ones in #fedora-arm. Don't mean to turn you away, but unfortunately I cannot give answers to most of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

      I prefer to use this forum to ask RPi related questions, where the answers are

    visible to others here.  We have been carefully tracking Fedora's progress here

    and puzzling about its silence for an entire year:

     

    http://www.element14.com/community/thread/18095?tstart=0

     

    It's wonderful that someone finally has come to respond, even to a limited extent.

    This forum is wide open for Seneca to publicize what it's doing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       The Pidora installation instructions say:

    "Do not use a MicroSD card with an adapter -- it will not be recognized by the Raspberry Pi."

    http://zenit.senecac.on.ca/wiki/index.php/Pidora_Installation

     

    I think this bug has been fixed for a while now.

     

     

    The Pidora administration instructions at:

    http://zenit.senecac.on.ca/wiki/index.php/Pidora#System_Administration:_Managing_the_Raspberry_Pi_Fedora_Remix

    mistakenly refer to:

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_Administration

    rather than

    http://zenit.senecac.on.ca/wiki/index.php/Pidora_Administration

     

     

    The Pidora FAQ says:

    "It includes some software which cannot be included in Fedora because it is not licensed under any of the licenses approved by the Open Source Initiative."

    http://zenit.senecac.on.ca/wiki/index.php/Pidora_FAQ#What_is_Pidora.3F

     

    I don't think this is true.  The ARM-based code has been opensourced, and

    I believe Fedora policy allows the RPi's firmware to be proprietary.

    https://fedoraproject.org/wiki/Licensing:Main#Binary_Firmware

     

     

    The Pidora "getting help" instructions neglect to mention the active

    RPi community at element14, and also neglect to mention any OSTEP

    resources (blogs, mailing lists, meeting minutes).

    http://zenit.senecac.on.ca/wiki/index.php/Pidora#Getting_Help

     

     

    The main purpose of Pidora is to enable hard-float, in order to make floating point

    operations faster, but the word "float" or "floating point" does not appear

    anywhere in the Pidora Announcement nor Pidora Release Notes.

     

    The Pidora Release Notes should make clear that the firmware is actually

    dated May 15, even though is named "0415", which would be April 15.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

       The Pidora installation instructions say:

    "Do not use a MicroSD card with an adapter -- it will not be recognized by the Raspberry Pi."

    http://zenit.senecac.on.ca/wiki/index.php/Pidora_Installation

     

    I think this bug has been fixed for a while now.

     

     

    The Pidora administration instructions at:

    http://zenit.senecac.on.ca/wiki/index.php/Pidora#System_Administration:_Managing_the_Raspberry_Pi_Fedora_Remix

    mistakenly refer to:

    http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_Administration

    rather than

    http://zenit.senecac.on.ca/wiki/index.php/Pidora_Administration

     

     

    The Pidora FAQ says:

    "It includes some software which cannot be included in Fedora because it is not licensed under any of the licenses approved by the Open Source Initiative."

    http://zenit.senecac.on.ca/wiki/index.php/Pidora_FAQ#What_is_Pidora.3F

     

    I don't think this is true.  The ARM-based code has been opensourced, and

    I believe Fedora policy allows the RPi's firmware to be proprietary.

    https://fedoraproject.org/wiki/Licensing:Main#Binary_Firmware

     

     

    The Pidora "getting help" instructions neglect to mention the active

    RPi community at element14, and also neglect to mention any OSTEP

    resources (blogs, mailing lists, meeting minutes).

    http://zenit.senecac.on.ca/wiki/index.php/Pidora#Getting_Help

     

     

    The main purpose of Pidora is to enable hard-float, in order to make floating point

    operations faster, but the word "float" or "floating point" does not appear

    anywhere in the Pidora Announcement nor Pidora Release Notes.

     

    The Pidora Release Notes should make clear that the firmware is actually

    dated May 15, even though is named "0415", which would be April 15.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

      Are there plans to publicize OSTEP?

    I notice that it is not included by name in the "projects" panel on the

    left side of the CDOT main page at:

    http://zenit.senecac.on.ca/wiki/index.php/Main_Page

     

    The OSTEP page at:

    http://zenit.senecac.on.ca/wiki/index.php/Category:OSTEP

    neglects to include a link to the OSTEP meeting minutes at:

    http://zenit.senecac.on.ca/wiki/index.php/Category:OSTEP_Meeting

     

    And Chris Tyler's OSTEP blog post at

    http://blog.chris.tylers.info/index.php?/archives/268-The-OSTEP-Team.html

    doesn't link to the OSTEP page (or vice versa).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Coder27,

     

    >The Pidora installation instructions say:

    >"Do not use a MicroSD card with an adapter -- it will not be recognized by the Raspberry Pi."

    >http://zenit.senecac.on.ca/wiki/index.php/Pidora_Installation

    >

    >I think this bug has been fixed for a while now.

     

    You are correct, this bug is fixed. Changes made.

     

    >The Pidora administration instructions at:

    >http://zenit.senecac.on.ca/wiki/index.php/Pidora#System_Administration:_Managing_the_Raspberry_Pi_Fedora_Remix

    >mistakenly refer to:

    >http://zenit.senecac.on.ca/wiki/index.php/Raspberry_Pi_Fedora_Remix_Administration

    >rather than

    >http://zenit.senecac.on.ca/wiki/index.php/Pidora_Administration

     

    Fixed.

     

    >The Pidora FAQ says:

    >"It includes some software which cannot be included in Fedora because it is not licensed under any of the licenses >approved by the Open Source Initiative."

    >http://zenit.senecac.on.ca/wiki/index.php/Pidora_FAQ#What_is_Pidora.3F

     

    >I don't think this is true.  The ARM-based code has been opensourced, and

    >I believe Fedora policy allows the RPi's firmware to be proprietary.

    >https://fedoraproject.org/wiki/Licensing:Main#Binary_Firmware

     

    Yes, Fedora does allow the firmware. Changes made.

     

    >The Pidora "getting help" instructions neglect to mention the active

    >RPi community at element14, and also neglect to mention any OSTEP

    >resources (blogs, mailing lists, meeting minutes).

    >http://zenit.senecac.on.ca/wiki/index.php/Pidora#Getting_Help

     

    Looking into this. Will get some of this done soon.

     

    >The Pidora Release Notes should make clear that the firmware is actually

    >dated May 15, even though is named "0415", which would be April 15.

     

    Fixed in release notes.

     

    >Are there plans to publicize OSTEP?

    >I notice that it is not included by name in the "projects" panel on the

    >left side of the CDOT main page at:

    >http://zenit.senecac.on.ca/wiki/index.php/Main_Page

     

    Pidora was added to projects, will have to look into plans for OSTEP. Changes are taking place.

     

    >The OSTEP page at:

    >http://zenit.senecac.on.ca/wiki/index.php/Category:OSTEP

    >neglects to include a link to the OSTEP meeting minutes at:

    >http://zenit.senecac.on.ca/wiki/index.php/Category:OSTEP_Meeting

     

    Good point. Changed.

     

    >And Chris Tyler's OSTEP blog post at

    >http://blog.chris.tylers.info/index.php?/archives/268-The-OSTEP-Team.html

    >doesn't link to the OSTEP page (or vice versa).

     

    I'll look into this.

     

    Thanks again for the help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

      Good job!  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andrew,

        The Pidora FAQ still has an obsolete reference (that I didn't originally point out) to

    "proprietary" software that can't be included in Fedora:

     

    "In the case of the Raspberry Pi Fedora Remix, the proprietary software provided by the Raspberry Pi Foundation and the SOC vendor Broadcom cannot be included directly in Fedora."

    http://zenit.senecac.on.ca/wiki/index.php/Pidora_FAQ#What_does_the_term_.22Fedora_Remix.22_mean.3F

     

    I think the sticking point now is that the RPi software although no longer proprietary,

    is not suitable for inclusion in Fedora due to for example the nonstandard use of FIQ

    in the USB driver.

     

     

    Edited to add:

    The Pidora wiki at:

       http://zenit.senecac.on.ca/wiki/index.php/Pidora#Helping_with_the_Remix

    says: To learn why this is a Remix and not a direct Fedora release, please see the FAQ.

    but should say "see the Pidora FAQ" at:

       http://zenit.senecac.on.ca/wiki/index.php/Pidora_FAQ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    The Register has an article on Pidora at

       http://www.theregister.co.uk/2013/05/27/fedora_pidora_linux_for_raspberry_pi/

     

    Unfortunately, it quotes two of the misconceptions I've been suggesting be fixed:

     

         The use of the term “remix” is important because the Fedora folk point out it denotes the release includes “proprietary software provided by the Raspberry Pi Foundation and the SOC vendor Broadcom cannot be included directly in Fedora.”

     

         There's also a headless mode that may appeal because the FAQ for the new OS points out: “The GUI in particular is slow, because the 2D graphics (the X Window System) are not yet connected to the 3D graphics processing unit on the SOC.”