Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Hi there would love to know were to start
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 710 subscribers
  • Views 1814 views
  • Users 0 members are here
  • helpme
  • raspberry_pi
  • learning
  • raspberrypi
Related

Hi there would love to know were to start

sjea
sjea over 13 years ago

Hello all I am new to site but am eager to learn, I have done a bit of research and beleave this is the way I would like to go.  What I would like to do is make a media server from computer room to TV room, General set up is ethernet cat5e to TV room I could go wireless can get gigabit router it nessary I have compaired a few but down to:

Popcorn Hour A-400 http://www.cloudmedia.com/products/popcornhour/store-a-400

 

WD TV Live http://www.wdc.com/en/products/products.aspx?id=330

 

and finlly

 

BUNDLE, MODEL B + 8GB SDCard W/ NOOBS PRE-INSTALLED with Raspberry Pi Media Center 

 

Am I on the right track or am I missing something ? Would love imput, feedback etc.  Not sure if need the bundle I am great with windows PC's and know how to find software if I just got the new Raspberry pi with sd card, hdmi cable, and downloaded XBMC that would work ? 

 

I downloaded XBMC on my Note 2 and worked well

 

enough out of me time for your input

 

Thank you for your time !!!

  • Sign in to reply
  • Cancel
Parents
  • sjea
    sjea over 13 years ago

    Thank you !!!!!!! I also check the read /write tab on card image im up and running now I'm working on sound play in tv speaker not Bose yet but I will be getting an av cable and that should fix it for some reason hdmi does not connect in bose but tv works great !!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hughb
    hughb over 13 years ago in reply to sjea

    If your bose system is an older one and you use the VC-2 HDMI board then be aware that it doesnt support audio over HDMI. I recently discovered this myself after trying for a few days. Bose recomends using SPdif for the audio to go with the HDMI input. But this is only for the older lifestyle systems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sjea
    sjea over 13 years ago in reply to hughb

    Yes thank you !!!!

    I bought a audio cord single one end and double left right other I think I can plug that into the bord  finger crossed other then that Im up and running

     

    I do have another questiong HOW do I see other drives only see C: or main profile would love to get to E: F: so I do not have to drag and drop files to ssd

     

    THank you !1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sjea
    sjea over 13 years ago in reply to hughb

    HI agai I reread your post I look up SPdif  how diffrent is that to

    3.5mm Stereo Male to Two RCA Stereo Male Y-Cable M-M

    this cable will plug into the Raspberry in audio and the RCA look like it will plug into the Boise board ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hughb
    hughb over 13 years ago in reply to sjea

    Just realised that there is no spdif on the pi. No problem the 3.5mm audio jack to RCA will be fine. Just make sure you plug the RCA jacks into the correct input you are using on the lifestyle box itself. You may need to select the analog audio input under system settings on the Bose if I remember correctly but you should be good to go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sjea
    sjea over 13 years ago in reply to hughb

    yep just call Bose they said the say hope I do not have to chose Analog ? that would take away stereo right

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sjea
    sjea over 13 years ago in reply to hughb

    yep just call Bose they said the say hope I do not have to chose Analog ? that would take away stereo right

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hughb
    hughb over 13 years ago in reply to sjea

    You should get both left and right. At one end you have a stereo 3.5 and the other is two RCA a red and a white. Plug both of these RCA into the Bose (red and white sockets) and it should work great. If you are watching video's you may have to adjust the audio delay on the Bose too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to sjea

    Hi Richard,

     

    Stereo will work, but it will sound awful (just an opinion) or barely adequate. It's hard to connect up analog audio from a board and expect the sound to be hum-free and noise-free. Unfortunately, I think you may need a USB audio soundcard for any decent sound (some have digital outputs) or try to find a way with HDMI. I understand you may not want to use USB because you'll also be using the network, but in this case you may be ok (assuming the USB soundcard is compatible), because the audio file gets buffered locally (or it should) before playback occurs for media files on your LAN. If you're streaming from the Internet, the bitrate may be low so you'll be fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sjea
    sjea over 13 years ago in reply to shabaz

    I was thinking of a usb sound card right now I have it bypassing my Boise and going into my Tv with hdmi it works but would like to see it I can get better sound thank you for your input