Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiNoir & Santa Catcher Challenge Support
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 133 replies
  • Subscribers 712 subscribers
  • Views 16417 views
  • Users 0 members are here
  • santa_catcher
  • raspberry_pi
  • pi_noir
Related

PiNoir & Santa Catcher Challenge Support

doctorcdf
doctorcdf over 12 years ago

Please direct support questions in relation to the challenge here.  Many thanks.

  • Sign in to reply
  • Cancel
Parents
  • jwier92
    jwier92 over 12 years ago

    Okay, it has been too quiet around here.  Got my Pi NoIR camera today and decided to start playing.  Well, plugged it in and started it up and had the same problems others were having that it would not work.  Saying the camera was not installed.  Double checked everything, enabled, rebooted, seated on both ends of the ribbon cable, etc.  No luck.  Then I check the small ribbon connector at the top of the lens and found that if I pushed it in, it would pop and I am guess re-seat.  Tested it and it worked, then I put it back in the case and it did not work.  Seems that camera housing/case pops that little sucker off. 

     

    Here is the connector in question that I had a problem with

    image

     

     

    So now I just put on the case without getting it all the way in, no pushing, and here is my test.

     

     

    PiNoIRTest.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jwier92

    That connector popping off seems to be a common problem going by the number of reports of the same over on the RPF forums. Seem to be just your luck though, I have several cameras and haven't had any problems.

     

    I don't like the case much though. I got the white version a few months back and don't think the quality is at all good. One of the problems is getting the camera board to sit in the slots in the sides fully. It's a bit hard to tell from your photo, but I wonder if the camera board isn't seated fully ?  If the camera board sits too high then maybe something catches the connector when you close the case. Or I'd not be surprised if the force needed isn't causing the fairly thin PCB to flex and that's causing the connector to pop out.

     

    See here for my take on the case http://www.element14.com/community/message/83388/l/rpi-camera-cases#83388

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    The problem is that the case is essentially snap fit and since there are connectors on all sides it puts quite a bit of force on the connectors as you are assembling the case. not much you can do about that unfortunately?!!

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Problemchild

    True, case producers are very much at the mercy of the PCB designers and whether they give any thought to cases at all...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Not as much as we would like, that's why my cases are assembled the way they are so you don't need to worry about this . The only easy way of doing it with a moulded case would be to have half the connector on the bottom of the case and the top part of the connector apertures on the Top moulding so join was along the line of all the connectors so you can just pop the board in and then bolt it down.

    BTW notice that all these cases are probably a standard size with the apertures milled out so even here they didn't fancy making a tool to do the moulding in one piece!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jwier92
    jwier92 over 12 years ago in reply to Problemchild

    Thank you John and selsinork.  I am not too concerned about getting the little case to fit perfect.  It is together now, but just left it not pushed in tight at the top. After the road test, this will go in a different enclosure and be located outside.  I wanted to let people to know what to look for if they are having the same problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jwier92

    I'd be very interested to see what you come up with as a suitable case for outside use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fvan
    fvan over 12 years ago in reply to e14 Contributor

    Outside use sounds interesting: something compact and waterproof for pi and camera would be awesome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to fvan

    It's made somewhat more difficult by needing to have the Pi in the same case.  I've built a couple of weatherproof RPi cameras at laest one of which survived outside for 4-5 months.  As you can tell, I'm interested to see if others have any better ideas than mine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Problem with having all this in the same case is that you need some method of making all the connections and maintaining  some degree of weatherproofing also you'll need to have a nice place to mount the camera that is transparent....not beyond the means of man but obviously more than the case supplied is really designed for.

     

     

    one way is to start with a weather proof box then put the pi etc int he box then put a small window(Acrylic for example) in it siliconed in.

     

    Ideas from you guys ?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Problemchild

    John, have a look at the photos here https://picasaweb.google.com/selsinork/RPiCamera

    Having the camera inside the ~3mm thick clear lid has it's problems, you get distortions and reflections.  The last photo in that album shows the latest incarnation which has a sheet of OHP transparency sandwiched between the case and the plate on the front. Plenty of silicone image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Problemchild

    John, have a look at the photos here https://picasaweb.google.com/selsinork/RPiCamera

    Having the camera inside the ~3mm thick clear lid has it's problems, you get distortions and reflections.  The last photo in that album shows the latest incarnation which has a sheet of OHP transparency sandwiched between the case and the plate on the front. Plenty of silicone image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    selsinork

    How did the last image solution work out for distortion, etc.

     

    I'm about to tackle the 'inside a gutted floodlight' for another purpose, and hopefully the thin glass doesn't have distortion issues.

    The glare isn't a big problem as its intended to be mounted inside and for low light, but outside you may want to add a hood using a piece of pvc tubing.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to mcb1

    You shouldn't have any real problem as long as you keep the angle to the glass low and the illumination correct

    After all this is how all the security  cams are plumbed !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    Mark Beckett wrote:

     

    How did the last image solution work out for distortion, etc.

    It works well, partly because it's a very thin layer, and partly because unlike the clear-lid case it's a small opening and so doesn't suffer from light-pipe side effects.

    Camera as close to the glass as you can and as near parallel as possible and as John says you shouldn't have a problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Thanks for that.

    I searched around and found the lens depth dimension (5.2mm) so I now need to find a suitable thickness spacer plate to 'glue' to the glass.

     

     

    The good news is the rural mailman has delivered two UPS packages from Newark.

    According to the packing slips the second package contains the camera.

     

    Unfortunately I have a task that will take all day plus some, so they will need to wait.  (....maybe tonight)

     

     

    Laureen/Christian

    The standard packing note says 60 days for the review, which clearly is at odds with the challenge

    Testers are required to produce a full, comprehensive and well thought out review of the PiNoIR camera, we also expect a minimum of 1 blog posts about the "Santa Catcher" in the Raspberry Pi Projects area of element14 and a video as per the brief above. These elements are due by January 13, 2014.

    which was extended

    We will extend the deadlines as a result to Friday, January 31st.

    Possibly in the future just include the print of the Road Test page.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to mcb1

    Mark I was considering doing a mounting kit for this type of purpose where the mount is basically a set of 3mm sheets with the cut outs for the various bumps and notches for the camera it's self components and screw holes then a final sheet over the whole assembly with some screws to hold it all together that is then glued/siliconed to  the case

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to Problemchild

    John

    A few years back we manufactured an outdoor petrol/diesel pump controller that had an LCD on the front panel.

    We used an over-sized piece of acrylic with countersunk screws.

    This was then silicon'ed onto the inside of metal front panel with the screw threads sticking out.

    It worked very well with zero failures, and the silicon seemed to hold the screws very well.

     

    I think for this a 3mm thick piece with a notch for the camera, and a 2mm that had a little more clearance might work.

    You can use a piece of mylar for the last tenths of a millimeter, which could be cut larger and folded to provide protection to the back if the user desired.

     

    If you can't /didn't want to use 2mm screws, you could always make it wider with a third piece on the top that did the holding, and use 3mm screws.

    If you made the first piece longer then its easy to add a right angle bracket for a tripod or vertical mount.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to mcb1

    Yeah sounds like a goer... Since I'd be laser cutting it I would need to use  3mm Acrylic not least because that's all I've got at the moment image

     

    I'll have a go at that maybe at the weekend

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    I'm essentially using two 3mm bits of ABS to space mine.  For the clear lid version, I glued some pieces into the case, mounted the camera to a second, then bolted them together.  The current case uses the case itself as one of the 3mm parts with the clear sheet on the outside. I suspect the difference from 5.2mm to 6mm makes no difference and may possibly be taken up by the sticky pad holding the camera to the PCB anyway.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Thanks for that information ..Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • slopop27@gmail.com
    slopop27@gmail.com over 12 years ago in reply to mcb1

    Hey Mark (et all),

        I too received my final box today, the Carbon Fiber Pi+CAD enclosure, was going to snap some pics of my progress however, now I've run into a small hiccup I think.  It possibly is my fault but want to get a few other opinions before I go all hacker on it.  Before installing said Pi+CAD in the enclosure, i *thought things were grooving nicely, So a quick a quick catch up, I found some documentation that had me setup the Pi with Apache + some additional python scripts mix in a little php and voila, had on-demand snapshots, with a web browser that would display the newly snapped pic.  Configured that last night (late), then messed with that better part of the morning and just afternoon.  Then turned my attention to the snap-camera.  Found the article and documentation (forums stuff too about experience), got that up and configured and played a little with it this evening.    (reboot to enable and set newly installed snap-camera), seemed to be fine, left it alone for a few hours come back now that a cute little brown package arrives, unwrap the new CF-enclosure, ssh --  shutdown the Pi cleanly, put it all back together and power up the new good looking contraption and the Display text is now all garbled when it looks like it should be loading/starting up the snap-camera LCD screen txt.  Thought that was strange,  ssh - cleanly shutdown again, pull enclosure apart carefully and slowly to make sure nothing was disconnected or wonky, re-assemble, same thing.  Garbled txt when it finally is booted up.  SO, like any good *nix person, ssh -- restart the snap-camera service, display *rights itself, think it is fixed, only to have the characters start to *corrupt themselves after pushing the once working buttons.  I think this is a script/python level thing but this is where I default to everyone else for assistance.  I am not a programmer.  I can follow along and traceback things, but .....  SO, I'm leaning toward it's not a hardware issue, but python or a conflicting service or script.   About to disassemble the Pi, and run it again outside the enclosure jic.

    Thoughts anyone/everyone?

    Thanks in advance,

    Eric

     

    Updated, cover/enclosure removed, still doing it (garbled txt on display, however perhaps I just did not mess around long enough with it earlier to see that it was doing it.  A couple pictures I took showing the text *refresh maybe whats' going on, but maybe that the command that displays the sysinfo.py is somehow trying to update the display (as a service), where snap-camera is also interacting and updating the display?   So it feels like they are both running at the same time, only the snap-camera has more things being refreshed so it takes the lead, where if I left it on 1 of the modes while messing with the options in that mode, the IP address replaces the entire top line of txt.

    tired, crashing for the night,

    so,  nite!