Raspberry Pi Forum I'd be giving the patents away...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 691 subscribers
  • Views 2515 views
  • Users 0 members are here
  • raspberry_pi
  • patents
Related

I'd be giving the patents away...

packetgeek
packetgeek over 12 years ago

A recent discussion, which appears to have (thankfully) been removed, involved a technology which was doubted by many.  Ignoring that it was inappropriate to advertise the thing an off-topic post, the thing that made me think that the tool was just more snake oil was the vendor's statement: "If I tell you everything you want to know,'I'd be giving the patents away!! and I cannot afford to do that."  If the author of that statement has a patent, then the information is already publicly available.  His statement makes me believe there is no patent and no actual working technology.

  • Sign in to reply
  • Cancel
Parents
  • R_Phoenix
    R_Phoenix over 12 years ago

    Thanks e14 for pulling those articles.

    I was able to read it when it was first posted and I had a good chuckle. While we have yet to understand all forms of energy exchange and the efficiency of most applications can be much improved on - there is no such thing as "free energy".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to R_Phoenix

    I believed that the Sun and Wind are "Free Energy"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Guessing: the comparison involves different loads on the motor (i.e.,

    comparing one output to the other).  My statement applied to conversions

    between different forms of energy.  I'll withhold any further comment on

    the topic as we're just chasing each others tails with this discussion.

    I'd rather get back to experimenting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to packetgeek

    Sometimes it's hard to let the other guy have the last word image

     

    But motor efficiency (in the context of the link I provided) is mechanical power out/ electrical power in.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett

    But motor efficiency (in the context of the link I provided) is mechanical power out/ electrical power in.

    Funny I was thinking the same thing.

     

    In the case of this device, it isn't converting energy from its electrical state, and I do know of DC to DC converts in the high 90's% of efficiency.

     

    Test challenge

    I still haven't heard back, and obviously there would be no cost to the testers, otherwise its not fair.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to mcb1

    DC/DC is still from electrical to electrical; although applicable in the context of the product discussed, I think packetgeek meant conversion from one domain to the other.  Anyway, he's wrong as ThinGap claims 95% efficiency: http://www.thingap.com/efficiency-and-smoothness/ and the CSIRO motors have way more efficiency than 80%.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to mcb1

    mcb1 wrote:

    ... and I do know of DC to DC converts in the high 90's% of efficiency.

     

    Right. That's marketing-speak. In general DCDC converters convert at "around 80%" efficiency. Then when you sweep the output current along the whole range, at one point you may measure "above 90%" efficiency. The marketing guys jump on this number and prominently place it everywhere they can. In reality, count on 80% and let yourself be surprised if possible.

     

    The "80%" mentioned is a good ballpark figure. There are exceptions. Gas-powered central heating installations here in the Netherlands apparently achieve 107% efficiency according to the official efficiency-calculating-rules. If you WANT to go from electrical power to heat, that can easily be done with 100% efficiency.

     

    On the other hand, going from chemical (gas) to mechanical power (moving car), you are lucky if you hit the 30%.

     

    As another example of how "ballpark figures" work I use "0.8" as the density of "organic materials". Wood, gasonline, etc. I know there are woods that are so dense that they sink (i.e. >1.0). But as a ballpark figure this 0.8 still works quite well. (e.g. when they say an airplane had XXX kg of fuel on board).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to rew

    Gas-powered central heating installations here in the Netherlands apparently achieve 107% efficiency according to the official efficiency-calculating-rules. If you WANT to go from electrical power to heat, that can easily be done with 100% efficiency.

    That's because in the official rules (when efficinecy was much, much lower) they thought that the heat going through the chimney was neglectabe..... Now that that heat loss is reduced, you get more than 100% efficiency. It's more an calculation / definition error. 107% efficiency would mean you'd be generating energy more heat than is available in caloric energy in the gas...

     

    Then when you sweep the output current along the whole range, at one point you may measure "above 90%" efficiency

    Yes. And when your application permits, you can design to be in that sweet spot. So it's a marketing-overused, but not a lie.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to vsluiter

    It's not the "heat going through the chimney" that they neglected in the definition at first.

     

    It's the energy that is contained in the water-vapour that goes up the chimney that they neglected. That can be recovered if you make sure the water condenses and you can leave the resulting water somewhere (a drain).

     

    If you build a heat-pump, powered either by gas or by electricity, you can get even higher efficiency figures, well above 100%.

     

     

    P.S; I fully agree with you to call the 107% situation a "definition error".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to rew

    "I know there are woods that are so dense that they sink (i.e. >1.0). But as a ballpark figure this 0.8 still works quite well."

     

    More common than you might think - as is well known to my poor dog. In the woods where we walk about half the sticks I throw in the river for her to fetch turn out to be sinkers. I'm trying to improve my manual density measurement skills but so far to little avail.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Recommend doing the power conversion math using the cars specs

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Ouch.  Good thing the dog's density is a bit below 1.0,  Our dog would

    attempt to recover the stick anyways.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Ouch.  Good thing the dog's density is a bit below 1.0,  Our dog would

    attempt to recover the stick anyways.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 12 years ago in reply to packetgeek

    Re. Dog  - ours makes the attempts but isn't good underwater.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to michaelkellett

    just found a better source of free energy on the pic basic forum

    Électricité gratuite et infinie

     

    enjoy