Raspberry Pi Forum D-Link DWA-171 Wireless AC Dual Band Adapter with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 676 subscribers
  • Views 1092 views
  • Users 0 members are here
  • raspberry_pi
Related

D-Link DWA-171 Wireless AC Dual Band Adapter with Raspberry Pi

Former Member
Former Member over 11 years ago

Hi All,

          Has anyone here used the above adapter with RPi?  Seems only 2.4Ghz band is supported but not 5.0Ghz as when I tried using the 5.0Ghz band the RPi did not see my router at all.  Any help?

 

Thanks,

 

Clemzky

  • Sign in to reply
  • Cancel
  • rew
    rew over 11 years ago

    Dear Clemzky,

     

    Before buying did you see any advertisement stating that it would work with Linux?

     

     

    A device is more or less worthless without a driver. So manufacturers make sure they provide drivers for popular operating systems. For some manufacturers that's " the latest Microsoft Windows"  operating system. For others that includes Linux. If the manufacturer does not provide a driver, some smart guy may pop up somewhere and write a driver for Linux. If that doesn't happen, then there simply isn't a driver and your device is back to square one: mostly worthless.

     

    This MIGHT be the case with your wireless adapter. To be able to see if this might be the case we need the output of: "sudo lsusb -v"

     

    On the other hand, getting wireless to work is not always easy. I've managed a few times, but I'm not an expert of doing it properly. So I'll let this one to others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to rew

    Hi Roger,

                  Thanks again for the reply, yes I read that, my very first post here was about how to connect to internet with my very first RPi , I was using a D-Link 2.4Ghz wifi dongle and manage to run it, in fact it is with my other RPi running the Apache and a database now this unit was the one with the issue you solve for me yesterday.  The 5Ghz adapter is for my desktop actually and since I am playing with the other new RPi, I tried using the 5Ghz adapter and there you go, swapped it with the 2.4Ghz and works.

     

    Thanks,

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tobaccoman
    tobaccoman over 11 years ago in reply to Former Member

    Dear Clem,

     

    Did you manage with the DWA-171, because I didn't

     

    Kind regards

     

    Daniel

    Dubai UAE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to tobaccoman

    Hi Daniel,

                    No it is only on 2.4GHz.

     

    Thanks,

     

    Clemzky

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to tobaccoman

    Daniel I tried the D-Link DWA-171 with no success - I bought it as much for my PC in my Office since I have moved the router to the lounge room where pi is connected to TV.  I successfully had been using the DWA-131 which was picked up automatically.  So the 171 is back on the PC and the 131 is on the Pi again works quite adequately.

     

    For the record, I have lodged a submission to D-Link re Linux drivers for the 171.  There were none on the CD that came with the adapter.  They have acknowledged receipt of submission and have indicated they will get back to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago

    As mentioned some time ago, I wrote to DLink support regarding a Linux driver for this device.  After a month they got back to me and suggested I try using the driver found at this site.  I am yet to try it only got email today.

     

    Give it a go.  Cheers.

     

    . https://www.dropbox.com/s/evhnl71rdij91sm/rtl8812AU_8821AU_linux_v4.2.2_7502.20130517_addl_IDs_added.tar.bz2