Raspberry Pi Forum Raspberry pi USB dongle not getting IP address and keeps connecting and reconnecting.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 684 subscribers
  • Views 1296 views
  • Users 0 members are here
  • address
  • wi-fi
  • disconnect
  • usb
  • way
  • ip
  • shake
  • raspberrypi
  • dongle
  • connecting
  • hand
  • 4
Related

Raspberry pi USB dongle not getting IP address and keeps connecting and reconnecting.

Former Member
Former Member over 12 years ago

I Bought a raspberry pi model B that came with a usb dongle on amazon. The box says element 14 on it. Im using the GUI interface to connect to wifi but it will connect without a ip address then reconnect and repeat that process. It also says 4 way handshake. I don't think power is the issue as i have tried two different power adapters, and one had a 5 Mah output. Im completely new to the raspberry pi so explain things like i'm five.

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 12 years ago

    Sorry 1amp but 5 volts

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago

    Many RasPi problems have to do with getting 5V to the board.  Even if you have a good 5V power supply, many Micro USB cables have very thin conductors which give you enough of a voltage drop that TP1 drops below 4.75V.  Your WiFi dongle may be adding enough load that TP1 is dropping below 4.75V. The RasPi Troubleshooting Wiki has a good section on troubleshooting power problems: http://elinux.org/R-Pi_Troubleshooting#Troubleshooting_power_problems

     

    If you have an external USB hub with its own power supply, try using the WiFi dongle in that hub.  That way it's not affecting RasPi's 5V supply.

     

    The problem could easily be something else, but I recommend checking TP1 first to rule out power problems.