Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum py-spidev mod help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 692 views
  • Users 0 members are here
  • raspberry
  • python
  • spidev
  • raspberry_pi
  • mpc3002
  • gertboard
Related

py-spidev mod help

e14 Contributor
e14 Contributor over 11 years ago


Helllo community,

 

I want to use the ADC on the Gerdboard. I started with the example code, witch was mentioned in the book "Raspberry Pi - Das umfassende Handbuch"
The code looks like this:
import spidev

import time

spi = spidev.SpiDev()

spi.open(0,1)

while True:

     antwort = spi.xfer([1,128,0])

     if 0 <= antwort[1] <=3:

          wert = ((antwort[1] * 256) + antwort[2]) * 0.00322

          print wert, " V"

          time.sleep(1)

 

Pretty easy, but I got the ErrorMessage: typeError Argument must be a list of at least one, but not more than 4096 integers

 

I found an answer here: https://www.raspberrypi.org/forums/viewtopic.php?p=309582
My problem is now about to change the file. I have no writing-rights.

This problem could not be solved by the chmod "bufsiz" command.

I was allowed to change the file as I loged in with the sudo su superuser, but the change was removed after a reboot and a login with the normal user "pi-raspberry".

 

Do you think changing bufsiz is the right way and can you help me changing it permanently?

 

 

Thank you
Sebastian

 

 

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago

    For the file in question just do this:

    sudo chmod +777 myfile.xxx

    man chmod      for more help

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Command works but after a reboot it's like i never changed it.(4096)..
    Same Error with the gertboard "dad" example btw. ...

    Errors occurs even when the file is changed (so no reboot was done and the command cat "bufsiz" shows correctly "65536",
    i also addet options spidev bufsiz=65536 to etc/modprobe.d/local.conf but it has no effects

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I had a similar problem and I could solve it with help of SPI-Schnittstelle...HILFE.

    It seems to be of problem of different software versions. Perhaps these commands may help.

     

    sudo pip uninstall spidev

    sudo pip install spidev