Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Programming for an embedded app
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 37 replies
  • Subscribers 711 subscribers
  • Views 4786 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Programming for an embedded app

e14 Contributor
e14 Contributor over 11 years ago

Background: I need to convert a 200 kHz encoder pulse train to 47.5 kHz. I tried using the Arduino Nano but it topped out at 8 kHz. Is used an ISR triggered on the rising edge of the encoder pulse and did floating point addition to determine when I should output a pulse. I know FP math in an ISR is not a good idea in general but it was simple math and the Arduino couldn't output faster than 8 kHz even w/o any ISR processing. Someone suggest using the Raspberry so I am attempting it. I have the Raspberry Pi 2 900 MHz system.

 

Main Questions:

  1. Is it possible to booth the system and auto load an executable w/o having to login? I want it to run like an embedded system.
  2. I want to write the code in my MS Visual C environment. How do I compile it for running on the Raspberry. Do I copy the code on to the SD card and compile and run on the Raspberry?

 

These are my main questions. I am a newbie using this and don't know all the specific steps from start to finish. I do have the Raspberry up and running but somewhat stuck after that. My internet is slow and it take forever to surf and find stuff. Is there one or two locations that can show me how to write a program from scratch. The Arduino code is less than 30 lines.


  • Sign in to reply
  • Cancel
  • element14support
    0 element14support over 11 years ago

    Hello psh59

    Welcome to the element14 Community, I will move this over to the Raspberry Pi 2 area as it is a better fit.

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bobalexander
    0 bobalexander over 11 years ago

    The first is easy:

    How To Autorun A Python Script On Raspberry Pi Boot

    If it's not a Python script just substitute your compiled application for myscript.py.

     

    As for the second, you will probably have to install a C compiler such as gcc (sudo apt-get install gcc-4.9 g++-4.9) and compile your code locally on there from the SD card.

    I might even give this a try if I had MS Visual C: Tutorial: Developing a Raspberry PI app with Visual Studio

     

    This is a good resource https://www.raspberrypi.org/resources/learn/

    As is this site.

     

    Good luck and let us know how it goes!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    As to the first question, Bob Alexander answered this one and I agree. The second one depends where the MS Visual C environment is running. If on a PC, then you cannot because it relies on DLL's that are not compiled to run on ARM code for Raspberry Pi. If on the other hand, it is on Windows 10 2015 Visual C++ built for cross compiling for Raspberry Pi and the Pi runs Windows 10 (whew), the answer is yes. I agree that GCC (free as in beerimage) is a great alternative as stated above.

    C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • screamingtiger
    0 screamingtiger over 11 years ago

    You wont want to use a Raspberry Pi for this, its not a real time device.  I "heard" you can get a real time OS but never used it.  The overhead of the OS is going to cause issues with devices that need exact timed pulses.

     

    Feel free to post your code, I bet we can get it running faster.  if the arduino you are using is 8mhz perhaps a 16mhz version would work?  I am not so sure an ISR would be the way to go if this is the ONLY thing it is doing, it would be better to remove the ISR overhead IMO.  If you are using DigitalWrite etc you can get a major increase by simply using the pins IO ports instead.

     

    Finally, if that doesn't work you need a faster MCU, such as a chipkitP with a Pic 32 should do the trick.  Here is a quick vid I made of a speed comparison between the chipkit PI and the nano.  the same code you write for the nano should work directly on the ChipKit.  On top of that you can do the optimizations I mentioned above and have more than 10 fold increase in speed.

     

    ChipKit Pi Vs Arduinio Nano328 16mhz

    http://www.element14.com/community/videos/16140/l/chipkit-pi-vs-arduinio-nano328-16mhz

     

    You can also pick up a ChipKit UNO which is the same thing just a different layout.  Both are pretty cheap, I think the chipkit pi is cheaper.

     

    If you find this information helpful or correct, please may "helpful" and/or mark as "correct answer".

     

    Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Is it possible to booth the system and auto load an executable w/o having to login? I want it to run like an embedded system.

     

    As the Linux or Unix root (super user), edit /etc/rc.local (E.g. `su gedit /etc/rc.local`).  Just before the `exet` statement at the end of the file, this is where you will insert a command to launch whatever it is that you want launched soon after boot time.  Note that rc.local is launched just after all of the other /etc/rcN.d scripts are launched.  For more details about "rc", investigate how Linux boots and how the "init" process (pid 1) works.

     

    You probably do not want your stuff running as the root.  So, in /etc/rc.local, your command should be something like this:

     

         su -c 'COMMAND' MYUSERID

     

    where

     

         COMMAND = is the absolute path name to your shell script

         MYUSERID = the user name under which you want COMMAND to run

     

    When I do this, my shell script is always self contained i.e. I do not rely on any I/O redirection of environment variables setup for me.  Also, make sure that you check *every* exit code from any embedded executables or called scripts.

     

    Log to a directory that MYUSERID has write-access to and that will survive a reboot (E.g. do not log to /tmp).  Always include "evidence" with each log entry such process ID, date, time, and context (what was the goal?).  I would write to file names that included the date so that these log files could be aged (yes, you need to write a log-ager).

     

    I want to write the code in my MS Visual C environment. How do I compile it for running on the Raspberry. Do I copy the code on to the SD card and compile and run on the Raspberry?

     

    My understanding that Windows is not yet ready for general-purpose computing on the RPi, just "IoT".  I would stick to Linux and C/C++ programming for Raspbian or one of the Ubuntu flavors.  The Gnu C/C++ compiler works very well for this purpose.  Also, there are other language options such as Java and Python which can handle GPIO.

     

    Good luck and experiment with tools.  Report back!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Is there one or two locations that can show me how to write a program from scratch.

     

    From scratch, in a nutshell .....

     

    If you used Visual Studio C/C++ already, then you do not need a lesson in the C/C++ languages themselves.  For C/C++ programming, you'll need to get used to employing two basic tools:

    1. a GUI source code editor
    2. the gcc Compiler

     

    For #1, I prefer the `gedit` tool; for #2, I use the `gcc` tool.  Get them like this:

     

         sudo apt-get install gedit gcc

     

    Another good tool for C/C++ development is `make`.  If `which make` doesn't show you that you already have it, then do this:

     

         sudo apt-get install make

     

    The `make` utility, while quirky, allows you to automate compiling and perform maintenance tasks related to source code, libraries, and executables.  Actually, a "Makefile" can specify almost anything that you'd like.

     

    A simplistic example:

    • Establish a source repository.  E.g. I have one being a folder called "src" under my home directory.
    • Under $HOME/src, create a folder called "hello".
    • Open a terminal window and execute:

         cd $HOME/src/hello

         gedit hello.c

    • Enter the following lines, save, and then exit from gedit:

         #include <stdio.h>

     

         int main ( int argc, char **argv ) {

              printf ( "Howdy, y\'all\n" );

              return 0;

         }

    • Still in $HOME/src/hello, execute:

         gcc -o hello hello.c

    • Execute the compiled program:

         hello

     

    Some C/C++/gdb/make tutorials:

    http://www3.ntu.edu.sg/home/ehchua/programming/cpp/gcc_make.html

    http://pages.cs.wisc.edu/~beechung/ref/gcc-intro.html

    http://cseweb.ucsd.edu/classes/fa09/cse141/tutorial_gcc_gdb.html


    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    Why not use a PLL?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to D_Hersey

    What is a PLL and where do I find info on that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    https://en.wikipedia.org/wiki/Phase-locked_loop

    C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    Frequency-locked loops are a little slower but a little less tricky than phase-locked loops, but seem to get lumped in with PLLs and called "PLL' just the same.

     

    If you are really, really old, you remember TVs that rolled when they warmed up.  The PLL eliminated that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>