Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Copying my main.cpp from Raspberry onto any Editor.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 2047 views
  • Users 0 members are here
  • raspberry
  • raspberry_pi
Related

Copying my main.cpp from Raspberry onto any Editor.

e14 Contributor
e14 Contributor over 10 years ago

Hi, This is Asif, and I am new into the coding world. I have been working on a project, which requires me to optimize someone else's code As i am new to this, i have been facing some really basic problems. So, I got my raspberry pi connected. i can read all the files in the directory(in which the code is written), and also managed to read the main.cpp in the LX-Terminal. However i want to copy this code from raspberry pi(LX terminal) to some other kind of editor. which i can open and refer/read on any platform i am working on.(phone/desktop). Could you please let me know how could i possibly do this. and if its possible.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Asif,

     

    You could use a USB memory stick to do the transfer, but a popular way is to just use your network connection. For most computers (including Windows or Mac) there is software that performs something known as 'SSH' that is advisable to get familiar with using, and 'SFTP. Together they provide the ability to work remotely, and to transfer files. On windows, one popular version of SSH software is called 'PuTTY' and it is a free download. For the SFTP element (sometimes it is combined in the same piece of software) you could investigate WinSCP (I've not used it - but google for 'SFTP Raspberry Pi' to find tutorials).

    SFTP will allow you to transfer files back and forth between your PC and the

    Raspberry Pi. If you google for PuTTY, SFTP and Raspberry Pi you'll find tutorials to

    help you with all that.

    SSH and SFTP are ideal if your PC and the Raspberry Pi are on the same network - additional effort is needed to work across the internet, such as if your PC and Raspberry Pi are separated at different locations like school and home.

    Yet another method is to place your code on a cloud platform, e.g. github. Then you can

    download it from anywhere, on any device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    Hi Asif,

     

    You could use a USB memory stick to do the transfer, but a popular way is to just use your network connection. For most computers (including Windows or Mac) there is software that performs something known as 'SSH' that is advisable to get familiar with using, and 'SFTP. Together they provide the ability to work remotely, and to transfer files. On windows, one popular version of SSH software is called 'PuTTY' and it is a free download. For the SFTP element (sometimes it is combined in the same piece of software) you could investigate WinSCP (I've not used it - but google for 'SFTP Raspberry Pi' to find tutorials).

    SFTP will allow you to transfer files back and forth between your PC and the

    Raspberry Pi. If you google for PuTTY, SFTP and Raspberry Pi you'll find tutorials to

    help you with all that.

    SSH and SFTP are ideal if your PC and the Raspberry Pi are on the same network - additional effort is needed to work across the internet, such as if your PC and Raspberry Pi are separated at different locations like school and home.

    Yet another method is to place your code on a cloud platform, e.g. github. Then you can

    download it from anywhere, on any device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thanks. That was a really helpful answer, i would try transferring it using SFTP. Its just that, now I have to see what SFTP exactly is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    If you're on a Windows PC, you could try Notepad++ - I just tried it, and it seems quite easy to use, it uses the built-in SFTP functionality inside it.

     

    After I installed Notepad++, I then followed the instructions here:

    http://www.cssbakery.com/2012/04/using-notepad-to-edit-files-on-server.html

    (the only difference I did was to select the 'initial remote directory' to be /home/pi )

     

    When you run it, you can connect to the Raspberry Pi by clicking the icon that is called "(Dis)Connect" in the NppFTP pane, and you'll see the files on the Raspberry Pi listed.

    When you double-click any of them, they will open up in the editor. When you hit 'save' it will save them back onto the RPI, but you can do a local save to your PC by going to 'Save As'.

    Also, if you have any file already open in the editor (i.e. any file on your PC, you can transfer it by pressing the 'Upload' button in the NppFTP pane.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Sorry, i got the exact mistake, i actually cannot establish the connection between the two, after i click that Dis(Connect) pane on the window, it doesnt connect to my raspberry.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    The screenshot below shows my settings, yours needs to look something similar.

    You can confirm if your raspberry pi is reachable by typing 'ping xx.xx.xx.xx' in a

    Windows command prompt first (where xx.xx.xx.xx is the IP address of your

    Raspberry Pi). If the ping is not successful, then there is a network related issue.

    The ping should always be your first test to ensure that you have reachability.

     

    Bear in mind, this won't (usually) work if the only path between you and the Raspberry Pi is the public Internet. Where is your Raspberry Pi and PC located - in the same physical location?

    image

     

    This is what the ping output could look like, your addressing will be different:

    image

    (Type ipconfig /all if you're unsure what network connection is in use on your PC). You can see that my PC is on the same network (192.168.1.xx) as the Raspberry Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thanks for all the help. I finally got it. I was doing one stupid mistake, my laptop and my raspberry pi were not on same network. thats why it didnt connect