Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum very basic cable question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 1121 views
  • Users 0 members are here
  • raspberry_pi_getting_started
Related

very basic cable question

beaglejax
beaglejax over 10 years ago

Looking at building my own Ethernet cables. Reading a bunch of stuff about pairs and pins, it seems like if you just make sure that the wire at one end is wired to the same pin on the other end, everything will be OK no matter what color or stripe the wire has. I looked at several prewired cables I already have, and none seem to conform to the 568A or B standards. Am I missing something here or can I just wire the pairs through to the matching pinouts?

  • Sign in to reply
  • Cancel
Parents
  • uscdadnyc
    0 uscdadnyc over 10 years ago

    BTW there are Color Codes as to what color-wire to put on what "110" IDC (Insulation Displacement Connection). Again this is all USA TELCO Stuff. BUT if you are Consistent on which (color) wire goes on which termination, it will be like Hillary said at earlier US House (of Reps) Benghazi Hearings: "What Does It Matter? What Does it Matter?". Just be consistent. But in the Future when/if someone else will be supporting your Work, That person may curse you b/c you did NOT follow Standards. It is up to you. But my motto in situations like this is: "Go Along . Get Along"

    (from NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beaglejax
    0 beaglejax over 10 years ago in reply to uscdadnyc

    Thank you both, John and Edward.

     

    John, you're right; I should have realized it was a Telco compat thing. I have a microwave link for my ISP, but Gb network is probably overkill for me, too. But I have a box of Cat6, so that's what I'll be using. I'm such a NooB, I'm making cables with EZ-RJ45's. (Wiki says they should be called 8p8c's, looking into that, too.)

     

    Edward, I'm just doing a home installation of a few cameras right now. I have no Closet, although that may be a real consideration in the future. I have worked with 66 and 110 blocks before, but just as a wiring monkey. I certainly cursed when finding miswired blocks which usually caused the problem.

     

    My plan right now is to hook up a couple of weather cams, but as I learn more, I can see a Data Closet in the future... in the meantime, I just want to get the basic structure scalable as the project expands. Thank you both, again! ::thumbs::

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • uscdadnyc
    0 uscdadnyc over 10 years ago in reply to beaglejax

    WRT Cams/Cameras, I would go w/ a WiFi Cam/Camera(s) Rather than Hard-wired Cat# wiring. Reason being more flexibility. All you need is an 110V AC Source nearby. Check-out the "Cloud Cameras" at dlink.com(?). there are also other manufacturers.

    (NYC NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beaglejax
    0 beaglejax over 10 years ago in reply to uscdadnyc

    I'm not sure what "WRT Cams/Cameras" are, but I'm looking to install two very different cameras. They both will be outdoors, so 110ac ain't happening. Low volt will have to do, so PoE seems a good choice. I'm also not wanting to go cloud right now, just wanting to save locally. As you can see, this project has many tentacles to be considered, and I was looking to get data back to a server on clean lines that could also supply PoE to them. One camera is the RaspiCam because I like tinkering with stuff. The other is a Hikvision 2032-I. Yes, I had to tinker with it, too. lol

     

    I think the camera topic deserves a new thread. Sorry to wobble off........... image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • beaglejax
    0 beaglejax over 10 years ago in reply to uscdadnyc

    I'm not sure what "WRT Cams/Cameras" are, but I'm looking to install two very different cameras. They both will be outdoors, so 110ac ain't happening. Low volt will have to do, so PoE seems a good choice. I'm also not wanting to go cloud right now, just wanting to save locally. As you can see, this project has many tentacles to be considered, and I was looking to get data back to a server on clean lines that could also supply PoE to them. One camera is the RaspiCam because I like tinkering with stuff. The other is a Hikvision 2032-I. Yes, I had to tinker with it, too. lol

     

    I think the camera topic deserves a new thread. Sorry to wobble off........... image