Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace RTC on Raspberry Pi2: still losing time on reboot!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 1 answer
  • Subscribers 709 subscribers
  • Views 4516 views
  • Users 0 members are here
  • clock
  • pi
  • rtc
  • raspberry_pi
  • raspberrypi
  • date
  • settings
  • piface
Related

PiFace RTC on Raspberry Pi2: still losing time on reboot!

e14 Contributor
e14 Contributor over 10 years ago

Hi!

 

I bought a PiFace RTC and I'm trying it on a Raspberry Pi 2 Model B. I followed the many guides I found on the internet, but I'm still having problem with the date: when I reboot, the system time is always set to Jan 1, 1970! It seems to be in a reset condition.

The I2C detects well the device at the address 0x6F, and the battery is ok.

After the execution of the .sh script as written in the PiFace RTC user guide, I set the actual date with "sudo date -s "12 jan 2016 10:30:00",

set the i2c module from raspi-config.

I triyed in so many ways but I really can't understand what I'm doing wrong!

 

Any idea would be appreciated!
Thanks,

 

Andrea.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    You may have done this already but...

     

    without any script to talk to the RTC on power up

     

    set the RTC time manually using one of the above commands

    read the time back from the RTC... is it correct

     

    now without any automated scripts talking to the RTC reboot the PI, and remember... no scripts should be talking to the RTC during power up either

     

    once booted, again read (Only Read) the time back out of the RTC, it should be correct or very close as you have not powered off the device irrespective of the battery

     

    if this worked, shutdown the pi and dissconnect the power to the PI, wait a few seconds and power up again, now read the RTC again... again no other scripts should be going near the RTC

     

    If this also reads correctly or within a few seconds, then you issue is with your scripts in the auto start up.

     

    If this does not work then you probably have hardware issues

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Hi Peter,

     

    a strange thing happens.

    I set the date with

    sudo date -s ...

    I write the RTC with

    sudo hwclock -w

    Read the time with

    sudo hwclock -r

    And it gives me the correct time.

    Now I shoutdown and I wait for few minutes.

    I boot up, I read the RTC with

    sudo hwclock -r

    and the time is OK.

    Now I reboot (without shutting down) with

    sudo reboot

    Once booted, I read the RTC:

    sudo hwclock -r

    The correct time doesn't appears, it give me the error message:

    hwclock: The Hardware Clock registers contain values that are either  
    invalid (e.g. 50th day of month) or beyond the range we can handle (e.g. Year 2095).

     

    How can the RTC be correct after a shoutdown / powerup and not correct after a simple reboot? Who is that set the date to an invalid range value?? There should be somewhere some wrong stuff that is involved at the startup.. really cannot understand where!

    Many thanks!

    Andrea

     

    Added:

    I don't believe this can be the issue (because the i2c is well detected), but I noticed that in the /boot/config.txt I have a dtparam=i2c=on; shouldn't it be dtparam=i2c1=on?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I noticed one thing.

    When the RTC is not read well, during the boot I can read an error message on the screen, please see the image provided:

    image

    It seems to involve the /etc/rc.local. Perhaps is there an issue in such file?

    My /etc/rc.local is below. Is there something wrong inside it?

    !/bin/sh -e 
    # 
    # rc.local 
    # 
    # This script is executed at the end of each multiuser ru$ 
    # Make sure that the script will "" on success or any oth$ 
    # value on error. 
    # 
    # In order to enable or disable this script just change t$ 
    # bits. 
    # 
    # By default this script does nothing. 
    
    # Print the IP address 
    _IP=$(hostname -I) || true 
    if [ "$_IP" ]; then 
      printf "My IP address is %s\n" "$_IP" 
    fi 
    
    # Calibrate the clock (default: 0x47). See datasheet for $ 
    i2cset -y 1 0x6f 0x08 0x47 
    modprobe i2c:mcp7941x 
    echo mcp7941x 0x6f > /sys/class/i2c-dev/i2c-1/device/new_$ 
    hwclock -s

     

    Thanks again,

    Andrea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to e14 Contributor

    I would not be surprised if the driver takes a second before it has the chip up-and-running. So I would place a "sleep 1"  before the "hwclock -s".

     

    Does that help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rew

    Unfortunately it does not help image!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Does 'man hwclock' provide any insight, it appears to have various routes to accessing the RTC.  My Pi returns "Cannot access the hardware clock by any known method" but I'd expect this because I haven't added a system driver.  I do however have an off-board circuit to drive a DS1337 via I2C.  For this I have used Gordon's WiringPi but if the truth were known I haven't yet resolved the time discrepancy with that. Too many things to do...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • briangawenus
    0 briangawenus over 10 years ago in reply to e14 Contributor

    is there any way of pinging the time off the internet to reset? using the time.windows.com server ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to briangawenus

    yes, use the NTP... Network Time Protocol

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to e14 Contributor

    After reading this and a couple of similar posts, I decided to try hooking up a similar device, the DS 1307, in the same manner. I wrote a blog about it here

     

    Enabling RTC on the Raspberry Pi 2

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mconners

    Michael Conners ha scritto:

     

    After reading this and a couple of similar posts, I decided to try hooking up a similar device, the DS 1307, in the same manner. I wrote a blog about it here

     

    Enabling RTC on the Raspberry Pi 2

     

    Mike

    Thanks Mike, this is very interesting and well described! My rtc device has a MCP7940N onboard. Can I ask you which particular RTC commercial board with the DS1307 did you used in your guide?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to e14 Contributor

    laser srl wrote:

     

    Thanks Mike, this is very interesting and well described! My rtc device has a MCP7940N onboard. Can I ask you which particular RTC commercial board with the DS1307 did you used in your guide?

     

    I tried to figure out the manufacturer the other day and I can not remember where I purchased it. There is a good chance it's a Chinese board I bought from ebay. Adafruit sells a kit, but I'm not sure where the best source for you would be in Europe.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to e14 Contributor

    Looking at your post above, I noticed one of the lines in your rc.local has

     

    1. echo mcp7941x 0x6f > /sys/class/i2c-dev/i2c-1/device/new_$  

     

    does it really have a $ at the end? Is that valid? The examples I've seen, and a code snippet I found for the I2C driver, said new_device

     

    in fact in my example on my blog post, I had

     

    echo ds1307 0x68 > /sys/class/i2c-adapter/i2c-1/new_device

     

    notice, there is a difference

    /sys/class/i2c-adapter

    vs

    /sys/class/i2c-dev

     

    although I see that both exist on my pi

     

    I'd also consider commenting out the calibrate line in the rc.local

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mconners
    0 mconners over 10 years ago in reply to e14 Contributor

    Looking at your post above, I noticed one of the lines in your rc.local has

     

    1. echo mcp7941x 0x6f > /sys/class/i2c-dev/i2c-1/device/new_$  

     

    does it really have a $ at the end? Is that valid? The examples I've seen, and a code snippet I found for the I2C driver, said new_device

     

    in fact in my example on my blog post, I had

     

    echo ds1307 0x68 > /sys/class/i2c-adapter/i2c-1/new_device

     

    notice, there is a difference

    /sys/class/i2c-adapter

    vs

    /sys/class/i2c-dev

     

    although I see that both exist on my pi

     

    I'd also consider commenting out the calibrate line in the rc.local

     

    Mike