Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum inhibit buttons whilst running script?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 39 replies
  • Answers 7 answers
  • Subscribers 709 subscribers
  • Views 4764 views
  • Users 0 members are here
  • python
  • raspberry_pi
  • raspberry pi
  • piface
Related

inhibit buttons whilst running script?

brew
brew over 10 years ago

Hi there I'm trying to use my Raspberry Pi 1B and PiFace to run a little interactive museum exhibition.

 

Process is Pi is in standby, Standby.py runs from rc.local Relay 1 is closed as this is the main light in the room,

Button Press (SW1) initiates the show

GoShow.py runs, this closes a number of replays which change the lights in the space and trigger a media player for the video the Pi plays a audio file.

 

I want to inhibit the button when GoShow is active, I've tried to 'de-listen' under the GoShow.py but no luck.

 

https://github.com/Brewj/Event-Trigger

 

Anyone any ideas?

 

Cheers

Brew

  • Sign in to reply
  • Cancel
  • rew
    0 rew over 10 years ago in reply to mconners

    Premature optimization is the source of all evil!

     

    The idea of a "pi" is that you can easily do a lot of things "the easy way". So the file based semaphore is a great way to implement the locking that James wants.

     

    So, James, it is worth knowing that the computer-nerds call what you are asking a "semaphore". Feel free to forget that word if you want. This can be programmed efficiently with the system calls that are available. But another way, which is probably MUCH easier for you to implement is to simply us a file.  Remember to remove that file when the system boots. Otherwise, at one point in time someone may shut down the system with the presentation running and then the whole system would become unresponsive....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to rew

    LOL. I can appreciate your argument. As I mentioned the performance aspect is probably not a consideration as it was 40 years ago when computers were slow and resources were at a premium.

     

    I also don't have a problem with explaining to people what they are trying to accomplish and what the proper terms are for the processes and patterns they are implementing.

     

    Your point is taken, the pi is meant to be an easy platform.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brew
    0 brew over 10 years ago in reply to rew

    Is there not a simple way of when the GoShow python script is running to inhibit the input from the PiFace buttons?  Possibly changing the way my Standby script behaves?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to brew

    I don't have a piFace, but I have some suggestions.

     

    First, on the first line of the toggle_led0 , unlisten to the interrupt, whatever the proper piFace call is

    Second move all the stuff from goShow.py into standby.py in the toggle_led0 function, and get rid of the subprocess call

    Third Re-enable the interrupt when done

     

    at the end of the file do something like

     

    if __name__ == "__main__":

     

     

    put all your interrupt enabling stuff after that, with the proper indentations

    then call a while loop that does nothing

     

    that way you don't need your sh files, and you shouldn't need a semaphore

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jack.chaney56
    0 jack.chaney56 over 10 years ago in reply to brew

    I love this discussion, because it is offering a good cross section of solutions.  The wonderful part is they are all correct, and the problem is, they could also all be wrong.  It all goes back to clearly defining the requirements. Sadly, a step of the development process that often is minimal-ized. Michael did the right thing, by going to the information available (the provided code) and worked with the tools in use. Thank you.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to brew

    As mentioned, you could just check the process list. This worked, could be adapted to do what you want..

     

    import psutil
    p=psutil.pids()
    found=0
    for i, elem in enumerate(p):
      process=psutil.Process(elem)
      pname=process.name()
      print "process name %s " % pname
      if (pname=="vi"):
        found = 1
        break
    print "found = %d " % found

     

    Replace the text in line 8 with the name of your program (e.g. goshow). I tested it with 'vi'.

    I did this on a PC, not a Pi, so I've no idea if it will work. I needed to do 'pip install psutil' first.

     

    If that works, then in your toggle_led0 function, use a routine (perhaps call it goshow_found() similar to that.

    Pseudocode (because I'm not familiar enough with Python to do it properly):

     

    if goshow_found()==1:
    // do nothing
    else
    subprocess.call("/home/pi/goshow.sh", shell=True)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago

    Overlapped there with other responses from people simultaneously. But at least now you have a few options.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to mconners

    Something like this

     

    #!/usr/bin/python
    import pifacedigitalio
    import subprocess
    from time import sleep
    
    
    pfd = pifacedigitalio.PiFaceDigital()
    
    
    pfd.leds[5].turn_on() #Room light ON
    
    
    def toggle_led0(event):
      # unlisten
      pfd.leds[1].turn_on() #On Air and Cabinet ON
      sleep (2) #Delay for lights
      pfd.leds[0].turn_off() #Room light OFF
      sleep (1)
      os.system("aplay /home/pi/withy_edit.wav") #Audio GO
      sleep (3) #End Delay
      pfd.leds[0].turn_on() #Room light ON
      sleep (1)
      pfd.leds[1].turn_off() 
      #relisten
    
    
    
    if __name__ == "__main__":
      listener = pfd.InputEventListener(chip=pifacedigital)
      listener.register(0, pfd.IODIR_FALLING_EDGE, toggle_led0)
      listener.activate()
    
    
      while True:
      pass

     

     

    substituting the proper code for unlisten and listen

     

    EDIT: I noticed there were two copies of the pifacedigitalio.PiFaceDigital object

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brew
    0 brew over 10 years ago in reply to mconners

    Hi Michael, that's a great plan, I'm just struggling to find out what the correct code is for the listen and unlisted commands.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to brew

    Actually, doing a quick google it looks like

     

    listener.deactivate()

     

    will unlisten

     

    and listener.activate()

     

    will turn it back on

     

    move

    1.   listener = pfd.InputEventListener(chip=pifacedigital) 

     

    up just below

     

    1. pfd = pifacedigitalio.PiFaceDigital() 

     

    to make sure it's in scope, give that a try and let us know.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>