Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi3 B+ to 8 channel relay CODING HELP
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2470 views
  • Users 0 members are here
  • 8 channel relay
  • home automation
  • automated
  • raspberry_pi
  • pi3
  • rasberry pi 3
Related

Pi3 B+ to 8 channel relay CODING HELP

e14 Contributor
e14 Contributor over 10 years ago

Hello, I will be blunt and honest, This is my first time looking at a Linux system let alone trying to learn to code in python and I'm struggling big time trying to learn this all. I need a coding mentor who is willing to communicate with me and help me get this done. Ahead of time, I apologize for my lack of vocabulary and my unorthodox techniques and perspective and thank you for your everlasting patients and I really appreciate any and all time you invest into helping me!

 

Question: Will you look over my project (posted below) and help me get it coded? ideally, i would be able to have an interface that would allow ease of use programmable on//off cycle on each outlet (all 8) and also in addition to, a simple toggle on//off of all 8 as well.    ( example:    [OUTLET 1]  on=15 minutes   off=45 minutes * repeat*

                                                                                                                 [OUTLET 2]  on= 16 minutes   off=44 minutes *repeat*

                                                                                                                 [OUTLET 3]       on=2pm         off=11pm

                                                                                                                 [OUTLET 4]      ON

                                                                                                                 etc....etc......)

Here's where i am so far the best i can sum it up;

Pi3

Relay       Diagram of relay

CanaKit GPIO to Breadboard Interface Board

 

This is how i wired the relay to the main power source

 

 

image

 

Below is a how I wired the breadboard to the relay. (Picture is visual rep of it written out)

 

Relay       |      Gpio# 

JD=Vcc            5v                                           

GND                GND

 

Vcc                  5v

1n1                GPIO 17

1n2                GPIO 27

1n3               GPIO 22

1n4               GPIO 23

1n5              GPIO 24

1n6              GPIO 26

1n7              GPIO 12

1n8              GPIO 16

 


image

what do you think? Can you tailor some code for me? I'm sure the code is out there some where, I most likely just need some guidance on how to fine tune it to my wiring/setup. 

 

                                                  Anxiously and hopefully awaiting a response 

                                                                      ~Mathew

 

 

 

 

* WORKING WITH ELECTRICITY IS EXTREMELY DANGEROUS. DO NOT TRY THIS. THIS IS A HYPOTHETICAL PROJECT NOT MEANT TO BE DUPLICATED OR REPRODUCED BUT FOR EDUCATION PURPOSES ONLY. ALWAYS USE ALL SAFETY STANDARDS WHEN WORKING WITH ELECTRICITY PER YOUR AREAS LAWS AND REGULATIONS*

 

Message was edited by: Mathew Rawlings THANKS PETER

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Looking at what your doing with the GPIO etc and also the scheduling of the GPIO, I think using Node-Red would greatly simplify the design of the solution.

     

    Node-Red is a graphical Design environment and is fully supported on the Raspberry PI... And it is Free and with the latest versions of Raspbian, it is also part of the image.

     

    There are nodes designed to directly interact with the GPIO of the PI and you can also script in Java or call python if you want.


    This is what a design could look like

    ,image

    this produces a WEB UI like this (I took 3 pics as I scrolled down)

     

    imageimageimage

    and for output to GPIO there are design elements like this

    image

    Note the set of Raspberry PI nodes on the left and the great big BIGTIMER below that. BIGTimer is a node that can handle scheduling for you and was written by a good friend of mine.

     

    Also note the light blue node second in that is used to automatically handle a DS18B20 temperature sensor.

     

    So in summary... Node Red can provide the interface to the hardware for you in an easy to use way, it can provide a WEB based UI for you to interact with your project from any smart device, it can schedule tasks. It is free and runs on Linux.

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Looking at what your doing with the GPIO etc and also the scheduling of the GPIO, I think using Node-Red would greatly simplify the design of the solution.

     

    Node-Red is a graphical Design environment and is fully supported on the Raspberry PI... And it is Free and with the latest versions of Raspbian, it is also part of the image.

     

    There are nodes designed to directly interact with the GPIO of the PI and you can also script in Java or call python if you want.


    This is what a design could look like

    ,image

    this produces a WEB UI like this (I took 3 pics as I scrolled down)

     

    imageimageimage

    and for output to GPIO there are design elements like this

    image

    Note the set of Raspberry PI nodes on the left and the great big BIGTIMER below that. BIGTimer is a node that can handle scheduling for you and was written by a good friend of mine.

     

    Also note the light blue node second in that is used to automatically handle a DS18B20 temperature sensor.

     

    So in summary... Node Red can provide the interface to the hardware for you in an easy to use way, it can provide a WEB based UI for you to interact with your project from any smart device, it can schedule tasks. It is free and runs on Linux.

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    I think you hit the nail on the head peter. This looks way more up my alley. I did see the Node-red program on my pi, just knew nothing about it.

     

    I believe you just pushed me down the right road my friend. Now I know where to start putting my efforts into learning. based off of my ignorance and what i got from what you said i need to go research (forgive me for not using proper terminology) how to install nodes, so i can see my breadboard, then dl BIGTIMER, your friends code because it sound like the tailored code that i need. then start dinking around till everything is connected like i want it....

     

     

    while im here asking questions, any advise on where to dl the nodes from? How do i find your friends node?

     

    I have been on github a couple times trying to read some code for relays and Dht22 sensors but i get confused on what im looking at because my eyes are not tuned properly yet, so many different options and people updating files I couldn't even understand what was an update, an add on or the original file. any perspective tips anyone?  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Robert Peter Oakes

    Very quickly you will come across a program canned NPM, it is used to load the nodes into node red for you

     

    here are a few links you may find useful

    https://youtu.be/uyx2KZNxhe4?list=PL_atu5RtEPi7FbbB8yG__0eyztqYWFN5u

    https://youtu.be/5RdPFRs1cAc?list=PL_atu5RtEPi5I5YWx_wb_j9erZGCvnpvW

     

    https://www.youtube.com/watch?v=1p3OwICqQbc

     

    + the node-red site

     

    I will also be doing more videos on the subject in the coming weeks