Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Capacitor to smooth out Raspberry Pi power dips?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 48 replies
  • Answers 30 answers
  • Subscribers 710 subscribers
  • Views 22628 views
  • Users 0 members are here
  • usb power
  • power supply
  • raspberry_pi
  • pi3
  • raspberry pi
  • usb cable
Related

Capacitor to smooth out Raspberry Pi power dips?

ntewinkel
ntewinkel over 9 years ago

I recently was trying to do a few things with a Pi3, and it consistently hung when I tried to update the system (sudo apt-get update/upgrade). It did everything else well enough, so I wonder if that's power related, with the upgrade making the WiFi work extra hard - maybe not, but I thought I'd look into it.

 

I've also noticed that my older Pi1 will hang once in a while (every few months), and that's a bit of an issue now that I'm using it as my sprinkler controller - reliability has become much more important.

 

While searching for help online, I noticed Robert Peter Oakes did some research and made a nice blog entry explaining the role the USB cables have in the power issues. (Thanks Peter!)

 

In a nutshell, some cables cause a voltage drop that puts the supply too far below the ideal 5v voltage level for the Pi.

The problem is that once in a while the Pi draws enough power to make the voltage dip into the danger zone.

(Some places sell adapters with a higher voltage to compensate. AdaFruit, for example sells a 5.25v adapter for the RPi, and notes that 5.25v is still within the specifications for USB, so even with a perfect no-loss USB cable that should be safe.)

 

One notable item, to me, was that the Pi has some serious power dips on a regular basis, regardless of the cables - just that the better supplies+cables start with higher levels at the Pi and the dips don't take it down too far.

 

So here's my thought - capacitors are supposed to help against dips and spikes, right?

 

Is there a way to add some really big capacitor at the Pi side to help avoid such dips (and maybe spikes too) ?

 

I'm thinking VIN-GND with a 1,000+ uF cap? I have one rated 1,000 at 10v, also I see 1,800 at 16v, both should handle 5v-ish well.

 

Otherwise, maybe splice a USB cable to add the large cap near the micro-USB plug end?

 

Will that cause trouble? Will it help at all?

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • niteowl12
    0 niteowl12 over 9 years ago

    Wouldn't it be easier to use an O'Scope to measure the input voltage during the "hang" to make sure that voltage drop is the actual problem? This would be my first step because I would think it highly unlikely that an update would use enough extra current to drop the voltage enough to cause a micro to stop functioning.

     

    Is the Pi controlling the sprinkler system through logic control or is it actually providing the power to a valve?

     

     

     

    10uf Cap

    image

    image

     

    1000uf Cap

    image

     

     

    image

     

    Notice the drop in voltage is about the same with a 2A jump in current. R1 in the schematic represents the incoming wire resistance to the Pi. If all the power to the Pi and sprinkler run through that one wire then I would focus on fixing that. Use two separate wires or one large one. That resistance will be the primary driver for voltage drop.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to niteowl12

    Jason, that's a very good suggestion. Usually it is quite difficult to catch "occasional" problems. But for power supply sagging problems you can indeed put the scope in "normal" mode (as opposed to "single" or "auto") and set the trigger point at say 4.5V. Then you'd end up with a trace of "the event" when it eventually triggers. On the other hand, not everybody has an oscilloscope.

     

    The other part of your suggestion: Solenoids, relays and the likes will often generate strong EMI pulses. Those can also create havoc with the reliability of systems...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to rew

    >Solenoids, relays and the likes will often generate strong EMI pulses.

     

    True, and I've had issues with that in other projects in the past (aka "learning experiences" image), involving Arduino with LCD and relays resetting when the relays went on.

     

    In this case, it's a blank Pi3 (fresh Raspbian image) going through an update, sitting on my desk with nothing going on. I might try an older image also as part of my tests.

    (The Pi1 sprinkler controller is a separate thing)

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to rew

    >Solenoids, relays and the likes will often generate strong EMI pulses.

     

    True, and I've had issues with that in other projects in the past (aka "learning experiences" image), involving Arduino with LCD and relays resetting when the relays went on.

     

    In this case, it's a blank Pi3 (fresh Raspbian image) going through an update, sitting on my desk with nothing going on. I might try an older image also as part of my tests.

    (The Pi1 sprinkler controller is a separate thing)

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer