Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Capacitor to smooth out Raspberry Pi power dips?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 48 replies
  • Answers 30 answers
  • Subscribers 710 subscribers
  • Views 22628 views
  • Users 0 members are here
  • usb power
  • power supply
  • raspberry_pi
  • pi3
  • raspberry pi
  • usb cable
Related

Capacitor to smooth out Raspberry Pi power dips?

ntewinkel
ntewinkel over 9 years ago

I recently was trying to do a few things with a Pi3, and it consistently hung when I tried to update the system (sudo apt-get update/upgrade). It did everything else well enough, so I wonder if that's power related, with the upgrade making the WiFi work extra hard - maybe not, but I thought I'd look into it.

 

I've also noticed that my older Pi1 will hang once in a while (every few months), and that's a bit of an issue now that I'm using it as my sprinkler controller - reliability has become much more important.

 

While searching for help online, I noticed Robert Peter Oakes did some research and made a nice blog entry explaining the role the USB cables have in the power issues. (Thanks Peter!)

 

In a nutshell, some cables cause a voltage drop that puts the supply too far below the ideal 5v voltage level for the Pi.

The problem is that once in a while the Pi draws enough power to make the voltage dip into the danger zone.

(Some places sell adapters with a higher voltage to compensate. AdaFruit, for example sells a 5.25v adapter for the RPi, and notes that 5.25v is still within the specifications for USB, so even with a perfect no-loss USB cable that should be safe.)

 

One notable item, to me, was that the Pi has some serious power dips on a regular basis, regardless of the cables - just that the better supplies+cables start with higher levels at the Pi and the dips don't take it down too far.

 

So here's my thought - capacitors are supposed to help against dips and spikes, right?

 

Is there a way to add some really big capacitor at the Pi side to help avoid such dips (and maybe spikes too) ?

 

I'm thinking VIN-GND with a 1,000+ uF cap? I have one rated 1,000 at 10v, also I see 1,800 at 16v, both should handle 5v-ish well.

 

Otherwise, maybe splice a USB cable to add the large cap near the micro-USB plug end?

 

Will that cause trouble? Will it help at all?

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • niteowl12
    0 niteowl12 over 9 years ago

    Wouldn't it be easier to use an O'Scope to measure the input voltage during the "hang" to make sure that voltage drop is the actual problem? This would be my first step because I would think it highly unlikely that an update would use enough extra current to drop the voltage enough to cause a micro to stop functioning.

     

    Is the Pi controlling the sprinkler system through logic control or is it actually providing the power to a valve?

     

     

     

    10uf Cap

    image

    image

     

    1000uf Cap

    image

     

     

    image

     

    Notice the drop in voltage is about the same with a 2A jump in current. R1 in the schematic represents the incoming wire resistance to the Pi. If all the power to the Pi and sprinkler run through that one wire then I would focus on fixing that. Use two separate wires or one large one. That resistance will be the primary driver for voltage drop.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to niteowl12

    >Wouldn't it be easier to use an O'Scope

    Sadly I don't have one, but I do have a TI tester that can graph voltage, that may do the trick (not sure if it's fast enough).

     

    >Is the Pi controlling the sprinkler system through logic control or is it actually providing the power to a valve?

    The sprinkler Pi is my old Pi1, and it's mostly stable - it hangs every few months randomly, before sprinkling season had started (ie, just sitting there idling, with the sprinkler software on but not powering the valves). I just ran a full sprinkling round (3 hours) last night and the veggie gardens this morning, and it's still running properly.

    It uses the same methods as OpenSprinkler.com - the Pi provides logic to shift registers, which turn on Triacs that pass the 24VAC power to the valves.

     

    The issue of hanging was during update of a Pi3 that I was just trying to set up for a different project.

     

    Thanks for running those tests and the resulting graphs! From what I see, it looks like a capacitor wouldn't really make any difference - is that correct?

     

    And the conclusion being pretty much what everyone else was saying - upgrade the power supply.

     

    When I have a chance, I'll try that Pi3 update again while gathering some numbers, maybe through a wired Internet connection too as one of the tests.

     

    Thanks,

    -Nico

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to ntewinkel

    Hi Nico!

     

    I'm still not sure it is a supply issue since the power consumption shouldn't increase during an update/upgrade significantly, but if all you have is a 1000uF capacitor and no oscilloscope I don't think there is anything wrong with just trying it, if you suspect that a combination of your PSU and the USB cable are making things just marginal. It all depends on how marginal, and for how long you're getting high current spikes (if that is what is occurring, because it is speculation, but sometimes we have to speculate).

    If the spikes were short and infrequent (e.g. 1msec spikes) and the current demand was around 1A (I don't think the Pi ever consumes 2A unless you've got extra hardware attached; and 1.4A, i.e. around 7W, takes all cores to be performing a workload), and if the supply voltage can drop from 5V by a volt and still continue operation on the Pi 3, then a 1000uF capacitor may well help.

    Maybe an interesting project would be a low-voltage detector LED  that lights up for a second even on short drops in voltage : ) There are ICs that will approximately do this (ICs for handling brownouts).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago in reply to ntewinkel

    Hi Nico!

     

    I'm still not sure it is a supply issue since the power consumption shouldn't increase during an update/upgrade significantly, but if all you have is a 1000uF capacitor and no oscilloscope I don't think there is anything wrong with just trying it, if you suspect that a combination of your PSU and the USB cable are making things just marginal. It all depends on how marginal, and for how long you're getting high current spikes (if that is what is occurring, because it is speculation, but sometimes we have to speculate).

    If the spikes were short and infrequent (e.g. 1msec spikes) and the current demand was around 1A (I don't think the Pi ever consumes 2A unless you've got extra hardware attached; and 1.4A, i.e. around 7W, takes all cores to be performing a workload), and if the supply voltage can drop from 5V by a volt and still continue operation on the Pi 3, then a 1000uF capacitor may well help.

    Maybe an interesting project would be a low-voltage detector LED  that lights up for a second even on short drops in voltage : ) There are ICs that will approximately do this (ICs for handling brownouts).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to shabaz

    >I'm still not sure it is a supply issue...

     

    I'm starting to suspect that maybe I have a bad image or a difficult SD card for the Pi3.

     

    I might try a different image and/or SD card, coupled with the happiest power supply + USB cable I can find image

     

    I do want to try and see if I can get some voltage graphs too.

     

    Thanks,

    -Nico