Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Astrophotography With The 8MP Raspberry Pi Cameras
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Answers 11 answers
  • Subscribers 710 subscribers
  • Views 8397 views
  • Users 0 members are here
  • debian
  • python programming
  • raspberry pi compute
  • raspberry pi iot
  • astrophotography
  • debian jessie
  • python 3
  • astro-pi
  • beagle bone black
  • raspberrypiprojects
  • raspberry_pi
  • raspberry pi
  • python code
  • astronomy
  • beagleboneblackwireless
  • linux
Related

Astrophotography With The 8MP Raspberry Pi Cameras

ninjatrent
ninjatrent over 9 years ago

I will attempt to use the Raspberry Pi 8MP NoIR and standard v2 camera boards for capturing images of the night time sky, and also with specialized filters in the daytime.

 

My question for the E14 community,

 

Does anyone have experience in this application of the RPi 8MP v2 cameras?

  • Sign in to reply
  • Cancel
Parents
  • ninjatrent
    0 ninjatrent over 8 years ago

    Here is the Pi Camera with factory lense removed. This is my first attempt of constructing an adapter. I need a 3D printer or CNC to develop a better design.

    image

    image

    imageimageimageimageimageimageimage

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago in reply to ninjatrent

    I would get a T-adapter.

    You want to place the sensor in the middle of the field of view to get the flat field over the entire width of the sensor.

     

    You also want repeatability, so you want a robust mount for the camera.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to DAB

    Where might I find a T-Adapter? I found a perfect adapter but the the price of $155 is out of my range. They were $90 a few months ago before the solar eclipse. Here is a link to the website. The company is located in Florida.

     

    http://www.truetex.com/raspberry_pi_c-mount_lens_adapter.pdf

     

    Raspberry Pi

     

    Ordering page -- Raspberry Pi C-mount and M12 lens adapter

     

    I really wish the Raspberry Pi Foundation would release an official case for the Pi 3 and the Pi Zero W that has an adapter built in for C-Mount and M12 lens type applications. Even just a top piece designed to fit the official Pi Case similar to the official Pi Zero W case would be great. I tried the Zero's Top that has a camera mount.

     

    image

    One of three tops that come with the official Pi Zero Case

    image

    And the Official Raspberry 3 Case, with to my knowledge, no camera mount.

     

    There is a Black Edition of this case.

     

    The material needed to construct a perfect adapter would need to be completely black to prevent any unwanted light from entering the picture.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago in reply to ninjatrent

    If the telescope eyepiece is 1 1/4 inch, go down to the hardware store and buy some 1 1/4 inch PVC tubing and maybe a cap.

     

    You can glue the cap on the tube after you drill a hole large enough to get the light to the camera sensor.

     

    Then you just stick the tube in the eyepiece holder and adjust the focus.  QED!

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to DAB

    DAB,

    what you suggest is in correct in theory. But as a matter of fact I think there are implicit issues. I come from a past when photographers was makers and there was no Amazon selling ring adapters for any kind of lenses/cameras. In the case of the telescope the problem of the correct focal length probably is not relevant but there is  the big problem of parallax between the focal planes of the sensor and the telescope that has a very long focal. The result - especially if you think to make photos in a specific azimuth coordinate on the sky map all the planes should be absolutely parallel so I think that just pVC with almost centred holes does not solve the problem. Without considering the lens distortion if the plane of the sensor is not aligned. Same problems occur when photographing with microscope or bit tele.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to DAB

    DAB,

    what you suggest is in correct in theory. But as a matter of fact I think there are implicit issues. I come from a past when photographers was makers and there was no Amazon selling ring adapters for any kind of lenses/cameras. In the case of the telescope the problem of the correct focal length probably is not relevant but there is  the big problem of parallax between the focal planes of the sensor and the telescope that has a very long focal. The result - especially if you think to make photos in a specific azimuth coordinate on the sky map all the planes should be absolutely parallel so I think that just pVC with almost centred holes does not solve the problem. Without considering the lens distortion if the plane of the sensor is not aligned. Same problems occur when photographing with microscope or bit tele.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • DAB
    0 DAB over 8 years ago in reply to balearicdynamics

    Agreed, but for prime focus, my solution should work assuming you can get the chip perpendicular with the focus point.

     

    That is why my preferred solution is a T adaptor.  The PVC approach would be a quick and dirty solution.

     

    It all depends upon what you want to do and how good a picture you want to take.

     

    A good mounting bracket is best for high quality.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer