Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Astrophotography With The 8MP Raspberry Pi Cameras
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Answers 11 answers
  • Subscribers 710 subscribers
  • Views 8483 views
  • Users 0 members are here
  • debian
  • python programming
  • raspberry pi compute
  • raspberry pi iot
  • astrophotography
  • debian jessie
  • python 3
  • astro-pi
  • beagle bone black
  • raspberrypiprojects
  • raspberry_pi
  • raspberry pi
  • python code
  • astronomy
  • beagleboneblackwireless
  • linux
Related

Astrophotography With The 8MP Raspberry Pi Cameras

ninjatrent
ninjatrent over 9 years ago

I will attempt to use the Raspberry Pi 8MP NoIR and standard v2 camera boards for capturing images of the night time sky, and also with specialized filters in the daytime.

 

My question for the E14 community,

 

Does anyone have experience in this application of the RPi 8MP v2 cameras?

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to balearicdynamics

    Hi Enrico!

     

    I don't know the method Trent used, but since you have a 3D printer, there is some online design for a 'adjustment spanner', which partially helps: https://www.thingiverse.com/thing:1574661

    As I understand some of them are glued slightly too.

    The removal tool isn't great (I ordered one from thingiverse, since I didn't have a 3D printer) but it did kind-of work. I think with hindsight I would have just made my own from filing a shaped hole in a small sheet of aluminium, it would have been cheaper (and faster to arrive) than the thingiverse order.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to balearicdynamics

    It unscrews aparently quite easily.

    The blob of glue is simply to stop the ens moving from the focal point set at the factory.

     

    You try it and let me know, because I have one to do..... image

     

     

    Mark

    These might help

    https://blog.adafruit.com/2014/08/08/how-to-focus-the-raspberry-pi-camera-lens-without-breaking-it-piday-raspberrypi-ras…

    https://www.thingiverse.com/thing:1574661

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to shabaz

    Shabaz, thank you for the detail.

     

    I have 3D printers but you are true, it is not the worth to 3D print a "tool". Maybe easier to make one as you suggest. What I am not sure is if it is an advantage or not to sue the sensor alone without the lens in cases like this. I should investigate.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to balearicdynamics

    I used a razor blade and magnifying glass to carefully remove the glue. Then a pair of tweezers was used to unscrew the lens. The focus of the lens can also be adjusted this way.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago in reply to ninjatrent

    If the telescope eyepiece is 1 1/4 inch, go down to the hardware store and buy some 1 1/4 inch PVC tubing and maybe a cap.

     

    You can glue the cap on the tube after you drill a hole large enough to get the light to the camera sensor.

     

    Then you just stick the tube in the eyepiece holder and adjust the focus.  QED!

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to DAB

    DAB,

    what you suggest is in correct in theory. But as a matter of fact I think there are implicit issues. I come from a past when photographers was makers and there was no Amazon selling ring adapters for any kind of lenses/cameras. In the case of the telescope the problem of the correct focal length probably is not relevant but there is  the big problem of parallax between the focal planes of the sensor and the telescope that has a very long focal. The result - especially if you think to make photos in a specific azimuth coordinate on the sky map all the planes should be absolutely parallel so I think that just pVC with almost centred holes does not solve the problem. Without considering the lens distortion if the plane of the sensor is not aligned. Same problems occur when photographing with microscope or bit tele.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago in reply to balearicdynamics

    Agreed, but for prime focus, my solution should work assuming you can get the chip perpendicular with the focus point.

     

    That is why my preferred solution is a T adaptor.  The PVC approach would be a quick and dirty solution.

     

    It all depends upon what you want to do and how good a picture you want to take.

     

    A good mounting bracket is best for high quality.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • defied
    0 defied over 8 years ago in reply to rew

    I'm late to the show. Setting multiple 1 second exposures won't do much to collect light for and take pictures of Deep space objects. It will be a series of shots with 1 second light collection. Stacking the images won't give you any proper increase in exposure (ie: 5 images with 1-second exposures stacked will create 1 image with maybe a hair more than 1 second exposure (Due to atmosphere shifting allowing more or less light through). Using the method you recommend for sun or moon, or other bright objects in the sky works fantastic. Most Stacking programs will software de-rotate images (They do an outstanding job with video).

     

    Ideally, using the Rpi and a motor controller to create a Goto mount and (if necessary) a derotator for stabilizing and capturing a long-exposure image would be far superior.

     

    D

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rcpettengill
    0 rcpettengill over 8 years ago

    The following information on building a RaspberryPi camera with a T-ring adapter and example images of the moon and planets may be helpful.

    Astro RaspberryPi Camera @ not so bad Astrophotography

     

    image

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago in reply to rcpettengill

    Very nice.

     

    How long was your exposure?

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<