Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum GPIO & Video
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 705 subscribers
  • Views 488 views
  • Users 0 members are here
  • raspberry_pi
Related

GPIO & Video

pattycakez
pattycakez over 9 years ago

So I am really new at the whole Raspberry Pi scene and have only made one project thus far but am feeling rather brave. I just need one question answered to see how hard my plan may be.

 

When using the GPIO pins for video output, (IE a hat) is it still possible to attach other peripherals? If so, how? Any good tutorials / how to's on the subject?

 

Thanks!

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 9 years ago

    Hi Patrick,

     

    It is likely that the HAT uses just some pins (specifically, the SPI pins, and possibly the I2C pins), so you're free to use the remainder. (In fact you could also still use the I2C since it is a serial bus with spare capacity for adding on additional hardware). You have the physical challenge of connecting to the board if the display HAT doesn't have protruding pins to connect your additional hardware, but that can be resolved in various ways (e.g. just solder a few wires onto the HAT.

    I'm not sure there is a specific tutorial on using a video HAT with additional hardware, but the first step would be to examine your video HAT documentation to see what connections it uses. If you can post a link to the documentation, it will be a straightforward task hopefully to examine what connections can be used.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Williams, 

     

    better if you explain what do you have in mind image Some project design?

     

    In a general view the answer is yes - despite some hats does not have the second connector to transport the pins outside, for obvious reasons. But in this case you can solder your wires directly on top of the Hat. Every HAT is different as far as I know and you should see in the HAT technical description or datasheet etc. what are the used pins. Then, excluding these, if there are not some strange exceptions you can use all the remaining ones.

     

    Just consider the following: it is important not only the PINs your had (or shield or anything else) are used but what is their function. I list some examples below.

     

    1. If power pins are used you should take in account that adding other circuitry the power should not be higher than the maximum declared from the PI
    2. if the SPI protocol is used or I2C you should see what is the address of the chip select pin used by the HAT and you should not use the same address(es) to avoid conflicts in the buffer
    3. if the PWM signals are used you have not them available for other uses

     

    etc. Every project is almost a separate case and probably a solution can be found anyway.

     

    Enrico