Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Problem with Pi Desktop Case
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 1748 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Problem with Pi Desktop Case

joerg_reuter
joerg_reuter over 8 years ago

have the same problem as Robert (Pi Desktop very disappointing ). I have the Pi Desktop already a couple of weeks. At the beginning, everything went perfectly normal and suddenly I had no HDMI signal. Only through the tests of Robert I noticed that it really depends on the SD card. I have tried several SD cards with always the same result: If I start the device without extension everything works always problem-free. With extension, there is no HDMI signal when I press the normal power button. I turn off again (and do not pull the power supply!) And remove the SD card and insert it again, the system boots completely normal. I have a 128 GB Samsung SD card (the effect also occurs at 32 and 16 GB) and a Kingstion 120 GB SSD disk. The effect occurs with and without an SSD disk.

 

Video: https://youtu.be/Hv7WsLgQZJ8

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Jorg,

     

    I didn't check the entire video, but at the start (when the HDMI output is not available) it can be seen that the red light on the Pi is on, so it is getting power.

    This means one of these possibilities could exist (there may be more, but this should cover most of the possibilities):

     

    (a) The Pi has power, but insufficient power for some reason -> confirm you are using the official power supply, or

    (b) The Pi is deliberately being kept in a reset state -> connect up USB-UART device to the 40-way connector and see from the serial console output if the Pi boots up, or

    (c) The Pi has tried to boot, but failed for some reason -> connect up a USB-UART device to the 40-way connector and see from the serial console output how far the Pi got before a failure message occurs

     

    For (b) and (c), the procedure to use a USB-UART device is here:

    Accessing and Controlling the Pi

    Scroll down to the "Using a Serial Console" section.

     

    For (a), I couldn't immediately see from the video what power supply you are using. Could you let me know the model number/link to it? For fully debugging (a), you should consider removing the attached SSD and any other peripherals, to reduce the current consumption. You could also consider trying to measure the voltage at the Pi (the 5V and GND connections are on the 40-way connector, you'll need a multi-meter for this measurement).

     

    Anyway, that's how I would debug it. Without doing this, it is like flying blind. Some visibility is needed.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • joerg_reuter
    0 joerg_reuter over 8 years ago in reply to shabaz

    I have to disappoint you unfortunately: If I turn on the Raspberry Pi (after separation from the current) comes synonymous serially no output. First when I eject the SD card and plug again, the Raspberry Pi starts. However, I have found during experimenting that it is possible to install the Raspberry with a supply via the GPIO pins into the housing. But this is not a real solution either.

     

     

    Video: https://youtu.be/iJyIni_I7Q8

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to joerg_reuter

    Hi Jorg,

     

    That's interesting. So, it means that the Pi is either deliberately held in reset or has no power, or (perhaps) it is trying to boot from a different source. I don't have the Pi Desktop nor tried to boot from a different source, so I don't know if any console output is to be expected prior to boot from alternate source.

     

    Just to confirm, you're using a Pi 3, right? And do you have a disk/SSD connected? What happens if you don't have the disk drive/SSD connected? Does it then always power up correctly, or still have to remove micro SD after power-off?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago in reply to joerg_reuter

    Hi Jorg,

     

    That's interesting. So, it means that the Pi is either deliberately held in reset or has no power, or (perhaps) it is trying to boot from a different source. I don't have the Pi Desktop nor tried to boot from a different source, so I don't know if any console output is to be expected prior to boot from alternate source.

     

    Just to confirm, you're using a Pi 3, right? And do you have a disk/SSD connected? What happens if you don't have the disk drive/SSD connected? Does it then always power up correctly, or still have to remove micro SD after power-off?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • joerg_reuter
    0 joerg_reuter over 8 years ago in reply to shabaz

    Yes, I use a Raspberry 3. The behavior is independent of the SSD disk.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hanslegters
    0 hanslegters over 8 years ago in reply to joerg_reuter

    Hi Jorg,

     

    I had exactly the same problems and solved this by updating the PiDesktop package:

     

    Download de PiDesktop package (https://github.com/pi-desktop/deb-make/releases )

     

    # Remove the old package first

    $ sudo dpkg -r pidesktop-base

    # Then install the new one

    $ sudo dpkg -i pidesktop-base-1.1.0.deb

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • joerg_reuter
    0 joerg_reuter over 8 years ago in reply to hanslegters

    Thanks for the hint. I can not tell the difference between a system with installed PiDesktop package and without.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mechanicus
    0 mechanicus over 8 years ago in reply to joerg_reuter

    Hi everybody,

    just made an account because i have the same troubles as described here before.

     

    I bought the PiDesktop as well. Had to remove the pi computer out of the PiDesktop twice now. And still only working after taking out the SD-Card before 2nd boot attempt.

     

    When i transfered the system to the SSD and did a reboot there was no problem at all. But now i am stuck with the SD-Card. Take it out - put it in.

    Quote: Rawhide Cut em out (ride em in) Ride em in (cut em out) Cut em out (ride em in) Rawhide.

     

    Any solution?

     

    Greetings