Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Are pull-up resistors needed for a USB joystick controller?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 706 subscribers
  • Views 2127 views
  • Users 0 members are here
  • pull ups
  • joystick
  • tactile switch
  • usb
  • raspberry_pi
Related

Are pull-up resistors needed for a USB joystick controller?

andywest
andywest over 8 years ago

I recently purchased a USB encoder for arcade joysticks (https://www.amazon.com/gp/product/B00UUROWWK) to use with my Raspberry Pi 3 Model B.

 

The encoder is correctly recognized as a joystick in Raspbian, and by shorting button pins I can see the status change. Then it occurred to me that this might be a bad idea.

 

Since this will be used in a portable game system, I intend to use tactile button switches with the encoder (https://www.adafruit.com/product/367) instead of actual arcade buttons. My question is, do I need to use pull-up resistors with these switches? I think if I were to use the GPIO pins on the Pi, there are internal pull-up resistors that can be used. But as this is a separate, USB-based board, I wasn't sure.

 

I'm hoping there are enough GPIO pins to make using this board unnecessary anyway, but just in case...

  • Sign in to reply
  • Cancel
Parents
  • DAB
    0 DAB over 8 years ago

    Hi Andy,

     

    It all depends upon if your joystick is just a passive or active component.

    If they are passive, then the switch to ground or voltage should not impact it.

    On the other hand, if the output is from an active component like an integrated circuit or transistor, then you really should use pull up or pull down resistors.

     

    Either way, putting a 10K ohm resistor between the output and ground will ensure a safe transition and keep static electricity from getting into the electronics.

     

    That might be useful for a USB device.

     

    So I would go with caution until you get a full circuit diagram.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • DAB
    0 DAB over 8 years ago

    Hi Andy,

     

    It all depends upon if your joystick is just a passive or active component.

    If they are passive, then the switch to ground or voltage should not impact it.

    On the other hand, if the output is from an active component like an integrated circuit or transistor, then you really should use pull up or pull down resistors.

     

    Either way, putting a 10K ohm resistor between the output and ground will ensure a safe transition and keep static electricity from getting into the electronics.

     

    That might be useful for a USB device.

     

    So I would go with caution until you get a full circuit diagram.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • andywest
    0 andywest over 8 years ago in reply to DAB

    Thanks for your reply. The encoder is designed for a specific type of arcade joysticks and buttons and from what I can tell they are passive. I'm confident enough that I'm willing to risk frying these inexpensive boards if I'm wrong.