Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Are pull-up resistors needed for a USB joystick controller?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 706 subscribers
  • Views 2126 views
  • Users 0 members are here
  • pull ups
  • joystick
  • tactile switch
  • usb
  • raspberry_pi
Related

Are pull-up resistors needed for a USB joystick controller?

andywest
andywest over 8 years ago

I recently purchased a USB encoder for arcade joysticks (https://www.amazon.com/gp/product/B00UUROWWK) to use with my Raspberry Pi 3 Model B.

 

The encoder is correctly recognized as a joystick in Raspbian, and by shorting button pins I can see the status change. Then it occurred to me that this might be a bad idea.

 

Since this will be used in a portable game system, I intend to use tactile button switches with the encoder (https://www.adafruit.com/product/367) instead of actual arcade buttons. My question is, do I need to use pull-up resistors with these switches? I think if I were to use the GPIO pins on the Pi, there are internal pull-up resistors that can be used. But as this is a separate, USB-based board, I wasn't sure.

 

I'm hoping there are enough GPIO pins to make using this board unnecessary anyway, but just in case...

  • Sign in to reply
  • Cancel
  • andywest
    0 andywest over 8 years ago

    After a bit of research I'm going to answer my own question. It looks like arcade push buttons use micro switches. There are no resistors or anything special inside, and when closed the resistance should be close to zero.

     

    My conclusion is that the small tactile button switches can be wired directly to the encoder without any resistors. Feel free to correct me if this is wrong, and I apologize for the noise. This is all new to me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 8 years ago

    The encoder image shows a bunch of what look like 10K Ohm resistors, which are probably pull-ups.  Take a look at the back side of the circuit board with a multimeter and see where they go.  The usual scheme is that each 2-pin header has one side grounded and the other side connected to the USB chip, with an additional pull-up to +3.3V or +5V.  As you have discovered, micro-switches are usually just metal contacts with no resistors or other components.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago

    Hi Andy,

     

    It all depends upon if your joystick is just a passive or active component.

    If they are passive, then the switch to ground or voltage should not impact it.

    On the other hand, if the output is from an active component like an integrated circuit or transistor, then you really should use pull up or pull down resistors.

     

    Either way, putting a 10K ohm resistor between the output and ground will ensure a safe transition and keep static electricity from getting into the electronics.

     

    That might be useful for a USB device.

     

    So I would go with caution until you get a full circuit diagram.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • andywest
    0 andywest over 8 years ago in reply to DAB

    Thanks for your reply. The encoder is designed for a specific type of arcade joysticks and buttons and from what I can tell they are passive. I'm confident enough that I'm willing to risk frying these inexpensive boards if I'm wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andywest
    0 andywest over 8 years ago in reply to johnbeetem

    Thanks for the advice. I'm embarrassed to admit that I don't know enough yet to do this. I poked around a little with the resistance mode on my multimeter but I'm not sure where to put the leads, what settings to use, and what results to expect. I have a lot to learn. image At least this issue is no longer blocking me and I can continue working on my little project.