Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Are pull-up resistors needed for a USB joystick controller?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 706 subscribers
  • Views 2126 views
  • Users 0 members are here
  • pull ups
  • joystick
  • tactile switch
  • usb
  • raspberry_pi
Related

Are pull-up resistors needed for a USB joystick controller?

andywest
andywest over 8 years ago

I recently purchased a USB encoder for arcade joysticks (https://www.amazon.com/gp/product/B00UUROWWK) to use with my Raspberry Pi 3 Model B.

 

The encoder is correctly recognized as a joystick in Raspbian, and by shorting button pins I can see the status change. Then it occurred to me that this might be a bad idea.

 

Since this will be used in a portable game system, I intend to use tactile button switches with the encoder (https://www.adafruit.com/product/367) instead of actual arcade buttons. My question is, do I need to use pull-up resistors with these switches? I think if I were to use the GPIO pins on the Pi, there are internal pull-up resistors that can be used. But as this is a separate, USB-based board, I wasn't sure.

 

I'm hoping there are enough GPIO pins to make using this board unnecessary anyway, but just in case...

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 8 years ago

    The encoder image shows a bunch of what look like 10K Ohm resistors, which are probably pull-ups.  Take a look at the back side of the circuit board with a multimeter and see where they go.  The usual scheme is that each 2-pin header has one side grounded and the other side connected to the USB chip, with an additional pull-up to +3.3V or +5V.  As you have discovered, micro-switches are usually just metal contacts with no resistors or other components.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 8 years ago

    The encoder image shows a bunch of what look like 10K Ohm resistors, which are probably pull-ups.  Take a look at the back side of the circuit board with a multimeter and see where they go.  The usual scheme is that each 2-pin header has one side grounded and the other side connected to the USB chip, with an additional pull-up to +3.3V or +5V.  As you have discovered, micro-switches are usually just metal contacts with no resistors or other components.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • andywest
    0 andywest over 8 years ago in reply to johnbeetem

    Thanks for the advice. I'm embarrassed to admit that I don't know enough yet to do this. I poked around a little with the resistance mode on my multimeter but I'm not sure where to put the leads, what settings to use, and what results to expect. I have a lot to learn. image At least this issue is no longer blocking me and I can continue working on my little project.