Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How do I connect a car TFT screen to a raspberry pi 2b
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 705 subscribers
  • Views 3195 views
  • Users 0 members are here
  • raspberry_pi_space
Related

How do I connect a car TFT screen to a raspberry pi 2b

wayne.t.johnson
wayne.t.johnson over 8 years ago

Let me start off by saying I am a noob at this stuff but a fast leaner.  This is something I have been wanting to do for a while which is to make a portable gaming device with a raspberry pi.  Now I have the raspberry pi but can not for the life of me figure out how to connect a TFT screen to it because the cables do not fit the pi itself.  I have 8 lcd's with with 4 of them having a removable touchscreen, and one portable Blu-ray player.  I  have looked really hard to find someone using theses types of screens but almost all of them are using ones with a red, white, and yellow cables.  I really want to use the Blu-ray player  because I can also use the case and the rechargeable battery pack which is another issue because it pumps out 7.2v and I am afraid that it might short out the pi.  Can anyone please help me with this?imageimageimage

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Wayne,

     

    For some ideas and some info see here:

    Cheap portable LCD for Raspberry Pi

    and

    Small monitor options for R-Pi

    In short if the displays have an RCA connector style interface (also known as composite video) then they can likely be attached to the Pi. Another alternative is HDMI.

    There are other ways too, but they are more complicated and could require adaptors which are difficult to make, and may or may not function with the display drivers on the Pi today.

    If you're using RCA, then an adaptor cable is needed which might be available ready-made or see here for pin wiring information:

    Raspberry Pi 2 A/V output via RCA Question.

    As you say, 7.2V will damage the pi. A regulator is needed (called a DC-DC converter) if you want to operate from a 7.2V battery. The output needs to provide 5V and offer a minimum of 1.5A perhaps (2A or higher would be preferable).

    If you want a small display for the Pi that is better quality than via RCA, google for 'Pi SPI TFT'. Such displays attach to the large expansion connector on top of the Pi. There are various models from different manufacturers. For a bigger screen, see here: Raspberry Pi 7” Capacitive Touch Display: Assembly and Enclosure which attaches via a flat flex connector to the Pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago

    Hi Wayne,

     

    For some ideas and some info see here:

    Cheap portable LCD for Raspberry Pi

    and

    Small monitor options for R-Pi

    In short if the displays have an RCA connector style interface (also known as composite video) then they can likely be attached to the Pi. Another alternative is HDMI.

    There are other ways too, but they are more complicated and could require adaptors which are difficult to make, and may or may not function with the display drivers on the Pi today.

    If you're using RCA, then an adaptor cable is needed which might be available ready-made or see here for pin wiring information:

    Raspberry Pi 2 A/V output via RCA Question.

    As you say, 7.2V will damage the pi. A regulator is needed (called a DC-DC converter) if you want to operate from a 7.2V battery. The output needs to provide 5V and offer a minimum of 1.5A perhaps (2A or higher would be preferable).

    If you want a small display for the Pi that is better quality than via RCA, google for 'Pi SPI TFT'. Such displays attach to the large expansion connector on top of the Pi. There are various models from different manufacturers. For a bigger screen, see here: Raspberry Pi 7” Capacitive Touch Display: Assembly and Enclosure which attaches via a flat flex connector to the Pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer