Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Setting up 7" LCD TFT Display 1024*600 with RPi 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2662 views
  • Users 0 members are here
Related

Setting up 7" LCD TFT Display 1024*600 with RPi 3

afmishaq
afmishaq over 7 years ago

I just bought a 7" LCD TFT Display 1024*600 HDMI VGA Monitor Screen Kit for Raspberry Pi 3. It came with no documentation I generally know how to go about setting it up but I was wondering if someone has recently done it and could point me in th eright direction A picture of what I got is attached. I intend to use it with RPi 3 B+ and Rasbian Stretch.

 

The specs in the listing say it will require 12 V but the power cable supplied has USB connector at the other end! Guess, I can always try it with 5V. The other question is whether any edits are required to the config file?

Attachments:
image
  • Sign in to reply
  • Cancel
  • Gough Lui
    0 Gough Lui over 7 years ago

    The kit seems to be an LCD and a scaler-input board with a separate front-panel button PCB.

     

    For the Raspberry Pi, it will probably be best to use the HDMI output from the Pi into the scaler input for the clearest picture. The scaler board will need 5V - hence the USB to barrel jack provided. The screen's flexible flat cable connects to the scaler board directly. The front panel button PCB will connect via the included multi-way ribbon lead.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • afmishaq
    0 afmishaq over 7 years ago in reply to Gough Lui

    Hi Gough,

     

    Thank you for the response. Is there any documentation available for the scaler board and the use of the menu buttons board with remote?

     

    - Faiz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to afmishaq

    That you should ask your supplier about. I don't think this kit is an element14 or Raspberry Pi foundation product, but it should be intuitive enough that there shouldn't need to be any documentation. Most people don't read the manuals for a computer monitor - this is basically the same thing but in parts-form.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • afmishaq
    0 afmishaq over 7 years ago in reply to Gough Lui

    No, this is an unbranded product. You are right. Once I power it up, I should be able to figure out the functions of the buttons. Thanks for your help.

     

    - Faiz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • korn
    0 korn over 7 years ago

    Looks a lot like the one I got from Adafruit except they dont have the remote.

     

    worked fine with a windows 10PC. With the PI you may have to tweak the config a bit.

     

    One thing I found is make sure the screen is powered up Before the PI.

     

    If the Pi boots first it goes into the wrong resolution.

     

    You may just have to change the boot file options for HDMI to force what settings you want then boot order wont matter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • afmishaq
    0 afmishaq over 7 years ago in reply to korn

    Robert,

     

    Thank you. That is a very useful tip, having the screen powered up before the pi.

     

    - Faiz

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • korn
    0 korn over 7 years ago

    try their settings as a start.

     

    Adafruit puts a lot of effort into their docs...

     

    https://learn.adafruit.com/hdmi-uberguide/2299-display-no-touchscreen-1024x600-hdmi-slash-vga-slash-ntsc-slash-pal

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • korn
    0 korn over 7 years ago

    they also sell just the io board. and have the data sheet available.

     

    https://learn.adafruit.com/hdmi-uberguide/rtd2660-hdmi-vga-ntsc-pal-driver-board

     

    image

     

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago

    Hi Abul,

     

    I have something similar, although I don't really use it with the pi (because the display resolution was low for the one i had - but it was useful for non-Pi scenarios).

    It just works when connected, it likely sets itself up to match the resolution settings as best as it can manage, using the out-of-band channel that is over the HDMI connection. And the buttons could be used for tweaking settings or you may find no adjustment is needed at all. These displays should be handy for connecting to games systems (but regrettably my Nintendo doesn't have HDMI : ( or converting a Pi into a retro games system, there is a very huge thread on it here: PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • afmishaq
    0 afmishaq over 7 years ago in reply to korn

    Thank you. This is very similar to what I have.

     

    - Faiz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>