Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum SETI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 1940 views
  • Users 0 members are here
Related

SETI

philertman
philertman over 7 years ago

I got my Raspberry PI 3 today. I also received my 12" LCD monitor/television and the Miuzei case from Amazon. I spent some time today and put it all together. I inserted the memory card with NOOBS software and powered

everything up. After initial load I made the choice to load the Raspian OS. (Denbian Linux). I am a member of SETI@home. I run BOINC on my computer. I know I can run BOINC on the Raspberry. I am having a difficult time

of getting any answers. As I am new to Raspberry and LINUX I need everything done in kindergarten talk. I am learning folks, every journey begins with the first step. Do any of you know how to set up BOINC in a Raspberry?

    Second question is sort of strange. I would like to have multiple Raspberry PI running for analysis of signals. I have seen pictures of Raspberry PI's in clusters. But nobody is saying HOW to do it. Do you just use one Raspberry PI as a control of the stack and attach your keyboard, mouse and monitor to it? Is there any documentation so I don't have to keep bugging you folks.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Philip,

     

    There's no single location of documentation, but there's community-created content here: Raspberry Pi Projects (there are beginners articles and projects there) and beginners journal-like articles at http://www.raspberrypi.org/magpi

    The installation of boinc is discussed here: https://www.raspberrypi.org/magpi/share-boinc/

    Regarding clusters, unless software is specifically designed to run like this, the software needs to be run individually on each machine, there's no sharing of resources normally. You can log into one device and remotely access the others, using a few different techniques depending on needs.

    If you wish to view a full graphical desktop, then tools like rdesktop can be used. See the Remote Desktop section here to see how to do that: Accessing and Controlling the Pi

    If the software you're using is purely text-based and has no graphics and if you are happy with just command-line interaction (a bit like DOS) then it's possible to use a protocol called SSH. It is described at that link too.

    Just for reference, if you've already got a PC that you use for day-to-day stuff, then if you don't need graphics (or don't need intensive graphics) there's no need to attach a keyboard/monitor/mouse to a Pi, it can be accessed using the remote methods mentioned above, from your PC. My Pi is not connected to display/kb/mouse, just to the home network. I connect from the PC to do some work on it.

    I don't use the graphical view, so this is how it looks like from my Windows PC (red is Pi, blue is a different Linux machine.. but the same method can be used for many Pi's). So, for graphical method or not, it mainly depends on the end application and also on what you prefer, and desired mode of use - some prefer a separate keyboard/mouse/display).

    image

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • philertman
    0 philertman over 7 years ago in reply to shabaz

    I found a way to work with the Raspberry PI. It was intended for teacher/student inter action but it would work for me. It is call PiNet. Using a router, some network switched and just about as many PI's you can afford. You get an old X386 computer and it boots and download software to the PI's on the network. So I would have each PI running BOINC and they pretty much run on there own from there.

      SETI has "acquired" more data from a radio telescope in Ausralia. SETI has put together ANACONDA software free to download. It is a series of programs to sift through petrabytes of information from the new station. The radio files are huge and not in the same format that SETI uses. They want people to use the package to try and figure out a way to sift it for signals. SETI@Home is calling it Breakthrough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • philertman
    0 philertman over 7 years ago in reply to shabaz

    I found a way to work with the Raspberry PI. It was intended for teacher/student inter action but it would work for me. It is call PiNet. Using a router, some network switched and just about as many PI's you can afford. You get an old X386 computer and it boots and download software to the PI's on the network. So I would have each PI running BOINC and they pretty much run on there own from there.

      SETI has "acquired" more data from a radio telescope in Ausralia. SETI has put together ANACONDA software free to download. It is a series of programs to sift through petrabytes of information from the new station. The radio files are huge and not in the same format that SETI uses. They want people to use the package to try and figure out a way to sift it for signals. SETI@Home is calling it Breakthrough.