Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace not working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 703 subscribers
  • Views 1842 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
  • pifacerelayplus
Related

PiFace not working

arsaphes
arsaphes over 6 years ago

Hello,

 

I've just bought a PiFace Relay+ to extend my Raspberry Pi 3 B+, followed the starter guide, but le python blink test doesn't work. All I have is an error message saying that the card is not present. All switches are in correct position and power is supplied. (I checked the screw terminals).

I've upgraded Raspian as well.

 

My goal is to command the relays with node.

 

Any idea?

 

Thanks for your help!

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 6 years ago

    Hi Christophe,

     

    Possibly, the software is not compatible with Pi 3B+. The github site for the board has not been updated in 4 years.

    You'll possibly need to troubleshoot the code, or look for alternate software that may control the chip on the board, since probably they've used a popular chip on the board. Or, choose a different product.

    Basically, the manufacturer, PiFace, doesn't seem to have taken any effort to support this product on newer Pi's.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • arsaphes
    0 arsaphes over 6 years ago in reply to shabaz

    Thanks a lot. If the hardwares are not compatible, that will explain everything. I'll send the card back and try to find another one. Such a pity...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 6 years ago

    Are you sure that the necessary overlays have been configured to load (if I recall correctly, SPI is required)?

    Have you tried executing the program with sudo privileges due to the hardware access requirements?

     

    Perhaps you can try using other tools to access the port expander the device - e.g. wiringpi, although I don't know if it supports your version of the PiFace.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • arsaphes
    0 arsaphes over 6 years ago in reply to Gough Lui

    Unfortunately, yes... SPI is loaded. Sudo or not, same thing. I played with the 'GPIO' command, the pins are changing correctly, but no relay change. Even if I set all the GPIO pins to high, nothing appends...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 6 years ago in reply to arsaphes

    Are you sure JP4 is fitted (closed 1-2) as the 5V supply to the board depends on it if you're not using the power supply terminals at the bottom?

    Likewise, are you sure that JP1, JP2 and JP3 are at their default positions across the first two pins (1-2)?

     

    Other than that, I suppose you might give the relays a bit of a tap just in case they somehow got mechanically stuck ... but I can't think of anything else.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • arsaphes
    0 arsaphes over 6 years ago in reply to Gough Lui

    Yes, all JPs are correctly set. I even tried to move JP1..3 and with JP4 removed. Allways the same thing. What is surprising is that I've got some power on the screw terminals, even if JP4 is removed...

    I also tried the bit of tap, but still no luck...

     

    Thanks anyway for your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago

    Is it a PiFace 1 or 2? I have a #2 that works on Pi3 when addressing it via c and c++.  I can try if you point me to the exercise you’re trying out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Jan Cumps

    owla, I just found out that Relais+ is a different product. Excuses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • arsaphes
    0 arsaphes over 6 years ago in reply to Jan Cumps

    No problem, thanks anyway!