Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi gpio output doesn't work
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 704 subscribers
  • Views 6376 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi gpio output doesn't work

levpi
levpi over 6 years ago

I am trying to create a simple blinking led application using Pi 3 model A+.

 

 

After some experiments it turns out that for some reason I not able to bring any gpio pin to High state.

 

I have tried both C, Python and gpio script to turn pin to High, but it doesn't work. I have tested both with the led and with "gpio readall", but all output are always 0.

 

What I did managed to change is to change the mode of the pins from Input to Output. It always worked without any problem.

 

Any idea what can be a reason for the problems with outputs? I just started experimenting with gpio, so  I don't think I could burn it already and I did only resistance + led tests. Also constant 3v and 5v pins work properly, so I still hope that it gpio is functional.

 

Any ideas are very welcome,

Thanks

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Lev,

     

    There's not enough information to be sure (and a photo and code can help!), but if I had to guess, if you think the code is fine, then there's a chance it could be one of these things:

    * Incorrect pin is being connected to the LED (the GPIO numbering doesn't map 1:1 with the physical connector numbering)

    * If you're using jumper wires there's a possibility the wire could be faulty (some have been known to have the conductor cut and just hanging on by the plastic insulation being crimped).

    * Incorrect orientation of the LED (can be tested first by trying to connect it to the 3.3V output on the connector, via a resistor).

     

    There's a photo how to connect an LED and test the output, here:

    Raspberry Pi GPIO Explained

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • levpi
    0 levpi over 6 years ago in reply to shabaz

    Thanks a lot Shabaz,

     

    Right, the wiring is not trivial and for this reason I have mainly used output of gpio in hope to see that output will turn to 1. But while I was able to see it changing from Input to Output, I couldn't make Output to change to 1.

     

    Unfortunately, now the pi doesn't boot anymore. Only power led is on when I power it. I have tried to reformat the memory card, but it doesn't help image

     

    Not sure how it could happen as I used only led with a 300om resistance and played a bit with gpio setup.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • levpi
    0 levpi over 6 years ago in reply to shabaz

    Thanks a lot Shabaz,

     

    Right, the wiring is not trivial and for this reason I have mainly used output of gpio in hope to see that output will turn to 1. But while I was able to see it changing from Input to Output, I couldn't make Output to change to 1.

     

    Unfortunately, now the pi doesn't boot anymore. Only power led is on when I power it. I have tried to reformat the memory card, but it doesn't help image

     

    Not sure how it could happen as I used only led with a 300om resistance and played a bit with gpio setup.